<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Re: CW10.4 got problem after install update</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-4-got-problem-after-install-update/m-p/240826#M9327</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Any time I see a problem with a fresh install not running properly, my first thought is it could be a Windows permissions problems.&amp;nbsp; If you downloaded the install from the internet onto a Windows 7 machine, the default behavior is for Windows to set the properties of the exe file to Blocked.&amp;nbsp; If you do not edit the properties of the install file (CW_MCU_v10.4_SE_Offline.exe was mine) and unblock it before running it, it will look like it installed but will give you all kinds of errors.&amp;nbsp; Assuming you used the default folder, check the properties for C:\Freescale\CW MCU v10.4\eclipse\cwide.exe.&amp;nbsp; If the properties show the file is blocked, uninstall everything, unblock the install exe file and reinstall everything.&amp;nbsp; I hope this helps you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Sep 2013 14:30:30 GMT</pubDate>
    <dc:creator>kecart</dc:creator>
    <dc:date>2013-09-19T14:30:30Z</dc:date>
    <item>
      <title>CW10.4 got problem after install update</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-4-got-problem-after-install-update/m-p/240825#M9326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CW10.4 got problem after install update, does anyone have this problem?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="6334_6334.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119663i262A6808676BB544/image-size/large?v=v2&amp;amp;px=999" role="button" title="6334_6334.jpg" alt="6334_6334.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="CW10.4.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40021iE2F49F06A94BAE6F/image-size/large?v=v2&amp;amp;px=999" role="button" title="CW10.4.jpg" alt="CW10.4.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Sep 2013 12:59:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-4-got-problem-after-install-update/m-p/240825#M9326</guid>
      <dc:creator>changfuzhao</dc:creator>
      <dc:date>2013-09-19T12:59:35Z</dc:date>
    </item>
    <item>
      <title>Re: CW10.4 got problem after install update</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-4-got-problem-after-install-update/m-p/240826#M9327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Any time I see a problem with a fresh install not running properly, my first thought is it could be a Windows permissions problems.&amp;nbsp; If you downloaded the install from the internet onto a Windows 7 machine, the default behavior is for Windows to set the properties of the exe file to Blocked.&amp;nbsp; If you do not edit the properties of the install file (CW_MCU_v10.4_SE_Offline.exe was mine) and unblock it before running it, it will look like it installed but will give you all kinds of errors.&amp;nbsp; Assuming you used the default folder, check the properties for C:\Freescale\CW MCU v10.4\eclipse\cwide.exe.&amp;nbsp; If the properties show the file is blocked, uninstall everything, unblock the install exe file and reinstall everything.&amp;nbsp; I hope this helps you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Sep 2013 14:30:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-4-got-problem-after-install-update/m-p/240826#M9327</guid>
      <dc:creator>kecart</dc:creator>
      <dc:date>2013-09-19T14:30:30Z</dc:date>
    </item>
  </channel>
</rss>