<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Re: Breakpoints move while editing</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Breakpoints-move-while-editing/m-p/238570#M9312</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Larry:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Eclipse environment of CodeWarrior sets the breakpoints to editor line numbers and not "code lines". So I'm afraid you are correct, you need to update your breakpoints whenever you add something above. There is no option in Eclipse to change that behavior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Dec 2013 18:10:23 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2013-12-03T18:10:23Z</dc:date>
    <item>
      <title>Breakpoints move while editing</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Breakpoints-move-while-editing/m-p/238569#M9311</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using CodeWarrior and a Freedom board.&amp;nbsp; After setting a breakpoint, ANY edit of the source code above the line causes the breakpoint to stay with the editor line number and not stay with the source code line it was set on.&amp;nbsp; Thus I must delete all of my breakpoints and add new ones at the line I want to break when I go back into the debugger.&amp;nbsp; How do I get the breakpoints to stay with the source code line?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) The behavior is, set a breakpoint at a line of code.&amp;nbsp; All is well.&lt;/P&gt;&lt;P&gt;2) Add a extra blank line in the source code above the breakpoint and recompile.&lt;/P&gt;&lt;P&gt;3)&amp;nbsp; When I go back into the debugger, the breakpoint jumps to line of code above its previous position.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Dec 2013 19:35:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Breakpoints-move-while-editing/m-p/238569#M9311</guid>
      <dc:creator>larrycarter</dc:creator>
      <dc:date>2013-12-02T19:35:19Z</dc:date>
    </item>
    <item>
      <title>Re: Breakpoints move while editing</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Breakpoints-move-while-editing/m-p/238570#M9312</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Larry:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Eclipse environment of CodeWarrior sets the breakpoints to editor line numbers and not "code lines". So I'm afraid you are correct, you need to update your breakpoints whenever you add something above. There is no option in Eclipse to change that behavior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Dec 2013 18:10:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Breakpoints-move-while-editing/m-p/238570#M9312</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2013-12-03T18:10:23Z</dc:date>
    </item>
  </channel>
</rss>