<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックHow to add new processor at existing project ?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-add-new-processor-at-existing-project/m-p/237306#M9288</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a working project maked with cw6.3 build 9279 + 6.3.1 patch build 10105 and using the processor MC9S08AW32.&lt;/P&gt;&lt;P&gt;I want to add new processor MS9S08AW16, without loosing the old one.&lt;/P&gt;&lt;P&gt;I have create a new Target with "create new target" and clone from existing target, but when attempt to change the processor type i have the error message "The change MCU feature is not available for project with more that one build target".&lt;/P&gt;&lt;P&gt;There is a solution ?&lt;/P&gt;&lt;P&gt;Thanx&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 Jan 2013 10:46:33 GMT</pubDate>
    <dc:creator>enzobruno</dc:creator>
    <dc:date>2013-01-25T10:46:33Z</dc:date>
    <item>
      <title>How to add new processor at existing project ?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-add-new-processor-at-existing-project/m-p/237306#M9288</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a working project maked with cw6.3 build 9279 + 6.3.1 patch build 10105 and using the processor MC9S08AW32.&lt;/P&gt;&lt;P&gt;I want to add new processor MS9S08AW16, without loosing the old one.&lt;/P&gt;&lt;P&gt;I have create a new Target with "create new target" and clone from existing target, but when attempt to change the processor type i have the error message "The change MCU feature is not available for project with more that one build target".&lt;/P&gt;&lt;P&gt;There is a solution ?&lt;/P&gt;&lt;P&gt;Thanx&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jan 2013 10:46:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-add-new-processor-at-existing-project/m-p/237306#M9288</guid>
      <dc:creator>enzobruno</dc:creator>
      <dc:date>2013-01-25T10:46:33Z</dc:date>
    </item>
  </channel>
</rss>