<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K60 MMA7760 Accelerometer with  I2C Protocol in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/K60-MMA7760-Accelerometer-with-I2C-Protocol/m-p/237028#M9285</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dao,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;do you refer to the example&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; \CW MCU v10.5\MCU\CodeWarrior_Examples\Processor_Expert\Kinetis\TWR-K60N512\I2C&lt;/P&gt;&lt;P&gt;I will check with colleague but I don't think we've other example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Keep you informed.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Pascal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Feb 2014 14:00:55 GMT</pubDate>
    <dc:creator>trytohelp</dc:creator>
    <dc:date>2014-02-25T14:00:55Z</dc:date>
    <item>
      <title>K60 MMA7760 Accelerometer with  I2C Protocol</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/K60-MMA7760-Accelerometer-with-I2C-Protocol/m-p/237027#M9284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does anybody know how to output the K60 tower board's accelerometer measurements via I2C Protocol and ProcessorExpert? I tried the example in codewarrior, debugged it, but it only returns descriptions, not measurements:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="9678_9678.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119719i1AC6E19DBCE21CFE/image-size/large?v=v2&amp;amp;px=999" role="button" title="9678_9678.jpg" alt="9678_9678.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="K60_MMA7660.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41484i8EDE5F27317D578E/image-size/large?v=v2&amp;amp;px=999" role="button" title="K60_MMA7660.jpg" alt="K60_MMA7660.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Any help, suggestions, guides on how to program this in codewarrior would be very much appreciated This is work related and time-sensitive. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Dao.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Feb 2014 18:01:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/K60-MMA7760-Accelerometer-with-I2C-Protocol/m-p/237027#M9284</guid>
      <dc:creator>broccolee</dc:creator>
      <dc:date>2014-02-14T18:01:39Z</dc:date>
    </item>
    <item>
      <title>Re: K60 MMA7760 Accelerometer with  I2C Protocol</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/K60-MMA7760-Accelerometer-with-I2C-Protocol/m-p/237028#M9285</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dao,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;do you refer to the example&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; \CW MCU v10.5\MCU\CodeWarrior_Examples\Processor_Expert\Kinetis\TWR-K60N512\I2C&lt;/P&gt;&lt;P&gt;I will check with colleague but I don't think we've other example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Keep you informed.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Pascal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Feb 2014 14:00:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/K60-MMA7760-Accelerometer-with-I2C-Protocol/m-p/237028#M9285</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2014-02-25T14:00:55Z</dc:date>
    </item>
    <item>
      <title>Re: K60 MMA7760 Accelerometer with  I2C Protocol</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/K60-MMA7760-Accelerometer-with-I2C-Protocol/m-p/237029#M9286</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pascal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for responding! I most certainly did try all the examples available. Since I have no prior experience with microcontrollers and very very little programming knowledge, I am clueless on how to change the example program above to print out the accelerometer measurements for example measurements X, Y and Z. The reason this is important is that I have to eventually try to talk to an external IMU sensor that has an I2C protocol.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Again, any help, suggestions, guides on how to program this in codewarrior would be very much appreciated as this is work related and time-sensitive.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Thanks,&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Dao.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Feb 2014 15:18:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/K60-MMA7760-Accelerometer-with-I2C-Protocol/m-p/237029#M9286</guid>
      <dc:creator>broccolee</dc:creator>
      <dc:date>2014-02-25T15:18:50Z</dc:date>
    </item>
    <item>
      <title>Re: K60 MMA7760 Accelerometer with  I2C Protocol</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/K60-MMA7760-Accelerometer-with-I2C-Protocol/m-p/237030#M9287</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dao,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are some information associated to the example.&lt;/P&gt;&lt;P&gt;Extract of the readme.txt file:&lt;/P&gt;&lt;P&gt;++++++++++++++&lt;/P&gt;&lt;P&gt;====================&lt;/P&gt;&lt;P&gt;This project demonstrates the use of the I2C component. An external&lt;/P&gt;&lt;P&gt;accelerometer is switched into a test mode in which the user can write&lt;/P&gt;&lt;P&gt;into the X, Y, Z data registers and then read the written values. For setting&lt;/P&gt;&lt;P&gt;up the mode register a one byte write/read operation is used, for write/read&lt;/P&gt;&lt;P&gt;the data registers a multibyte write/read operation is used. Comments and test&lt;/P&gt;&lt;P&gt;results are sent to ConsoleUART (Serial component) via a Tower Serial module&lt;/P&gt;&lt;P&gt;(TWR-SER). RS232 settings: 38400baud rate, 8-bit, 1-stop bit, no parity.&lt;/P&gt;&lt;P&gt;++++++++++++++&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can get help of each bean.&lt;/P&gt;&lt;P&gt;By this way you will have all information associated to a bean: how to configure it&lt;/P&gt;&lt;P&gt;&lt;IMG alt="" class="jiveImage" height="459" style="max-width: 1200px; max-height: 900px; width: 857px; height: 459.209px;" width="857" /&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;IMG style="height: 511px; width: 953.269px;" /&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Click on &lt;A _jive_internal="true" href="https://community.nxp.com/thread/I2C_LDDTypical Usage.html"&gt;Typical Usage&lt;/A&gt; to have more example of bean usage.&lt;/P&gt;&lt;P&gt;Hope this will help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pascal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Feb 2014 09:35:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/K60-MMA7760-Accelerometer-with-I2C-Protocol/m-p/237030#M9287</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2014-02-26T09:35:58Z</dc:date>
    </item>
  </channel>
</rss>