<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Re: How to setup the CodeWarrior in the CodeWright IDE completly?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-setup-the-CodeWarrior-in-the-CodeWright-IDE-completly/m-p/234968#M9238</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;now there are enough informations trough activating the "verbose format" with -WmsgFbv. But at the moment when I am executing CodeWarrior from CodeWright with the following line:&lt;/P&gt;&lt;P&gt;C:\Freescale\CodeWarrior for Microcontrollers V6.3\bin\ide.exe c:\.....{PROJECTNAME}.mcp /t "{TARGETNAME}" /r /b /q&amp;nbsp;&amp;nbsp;&amp;nbsp; with the Options "No cmd shell" and "Save all files".&lt;/P&gt;&lt;P&gt;After the execution the content of the Errorfile is deleted.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And even if this would be fixed I would still have problem with the parser. Do I have to write a new parser in this case or can I use one of the predefined parsers of CodeWright?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thx a lot for the support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Jan 2013 16:06:25 GMT</pubDate>
    <dc:creator>elsalvadore</dc:creator>
    <dc:date>2013-01-28T16:06:25Z</dc:date>
    <item>
      <title>How to setup the CodeWarrior in the CodeWright IDE completly?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-setup-the-CodeWarrior-in-the-CodeWright-IDE-completly/m-p/234962#M9232</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the CodeWarrior Ver. 5.9 and the CodeWright Ver. 7.5.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Does someone knows how to set the CodeWarrior or the CodeWright IDE, to get the "Warning Error Msgs" directly into the CodeWright IDE?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I am so far that I can start the CodeWarrior from the CodeWright, trough the settings in Project-&amp;gt;Project Properties-&amp;gt;Tools and the CodeWarrior generates a file, but only with the messages e. g.:&lt;/P&gt;&lt;P&gt;1 warning&lt;/P&gt;&lt;P&gt;1 error&lt;/P&gt;&lt;P&gt;It is to less information. I am expecting infos like the type of warnings or error and also the line number.&lt;/P&gt;&lt;P&gt;Thx for help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Jan 2013 15:17:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-setup-the-CodeWarrior-in-the-CodeWright-IDE-completly/m-p/234962#M9232</guid>
      <dc:creator>elsalvadore</dc:creator>
      <dc:date>2013-01-23T15:17:38Z</dc:date>
    </item>
    <item>
      <title>Re: How to setup the CodeWarrior in the CodeWright IDE completly?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-setup-the-CodeWarrior-in-the-CodeWright-IDE-completly/m-p/234963#M9233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Not sure which MCU you are targeting here.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are targeting a HCS12, HCS12X or a HCS08, the attached Technical note might be of interest.&lt;/P&gt;&lt;P&gt;It was created a couple of years back for an earlier version of CodeWright.&lt;/P&gt;&lt;P&gt;May be the same mechanism is still working with the new release of CodeWright.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2013 06:56:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-setup-the-CodeWarrior-in-the-CodeWright-IDE-completly/m-p/234963#M9233</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2013-01-24T06:56:04Z</dc:date>
    </item>
    <item>
      <title>Re: How to setup the CodeWarrior in the CodeWright IDE completly?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-setup-the-CodeWarrior-in-the-CodeWright-IDE-completly/m-p/234964#M9234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello CrasyCat,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;thx a lot for such fast answering.&lt;/P&gt;&lt;P&gt;I have already found this doc. in one previos discciussion...&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/42878#42878"&gt;https://community.freescale.com/message/42878#42878&lt;/A&gt;&lt;/P&gt;&lt;P&gt;This is quit helpful, but still written for some tools from Metroworks. And my tools are from CodeWarrior. So it still a question which file you have to type in the tab "errors" in the field "Error Filename" and also the format of the output file in the field "Error Parser 1".&lt;/P&gt;&lt;P&gt;The result is that the found errors and warnings in CodeWarrior are not transfered to CodeWright.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But, found out yesterday that this messages are transferred directly from the CHC08.exe (the compiler from CodeWarrior) into CodeWright.&lt;/P&gt;&lt;P&gt;Still to do is the settings for the compiler. For the CodeWarrior &lt;EM&gt;IDE &lt;/EM&gt;the settings are already finished :smileysad:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2013 09:04:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-setup-the-CodeWarrior-in-the-CodeWright-IDE-completly/m-p/234964#M9234</guid>
      <dc:creator>elsalvadore</dc:creator>
      <dc:date>2013-01-24T09:04:02Z</dc:date>
    </item>
    <item>
      <title>Re: How to setup the CodeWarrior in the CodeWright IDE completly?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-setup-the-CodeWarrior-in-the-CodeWright-IDE-completly/m-p/234965#M9235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Which MCU are you targeting?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2013 14:45:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-setup-the-CodeWarrior-in-the-CodeWright-IDE-completly/m-p/234965#M9235</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2013-01-24T14:45:56Z</dc:date>
    </item>
    <item>
      <title>Re: How to setup the CodeWarrior in the CodeWright IDE completly?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-setup-the-CodeWarrior-in-the-CodeWright-IDE-completly/m-p/234966#M9236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The MCU is: MC9S0BGT32.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have found an answer two my previous question in the doc. Compiler_HC08.chm:....&lt;/P&gt;&lt;P&gt;If you start the Compiler from an IDE (with &lt;CODE class="cCode"&gt;'%f'&lt;/CODE&gt; given on the command line) or CodeWright (with &lt;CODE class="cCode"&gt;'%b%e'&lt;/CODE&gt; given on the command line), the Compiler does not produce the &lt;CODE class="cCode"&gt;&lt;SPAN style="background-color: #0a246a; color: #ffffff;"&gt;err.txt&lt;/SPAN&gt;&lt;/CODE&gt; error file. Instead, the Compiler writes the error messages in a special format in a file called &lt;CODE class="cCode"&gt;EDOUT&lt;/CODE&gt; using the default..... Microsoft format.&lt;/P&gt;&lt;P&gt;Nevertheless I the msgs don not pop up in the CWright.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried to generate a msg output file with the msgs, therefore I set the param:&lt;/P&gt;&lt;P&gt;-Env"ERRORFILE=MyErrors.txt"&lt;/P&gt;&lt;P&gt;in the Command Line Arguments from the Compiler for HC08. But the file was not generated sadly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2013 15:17:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-setup-the-CodeWarrior-in-the-CodeWright-IDE-completly/m-p/234966#M9236</guid>
      <dc:creator>elsalvadore</dc:creator>
      <dc:date>2013-01-24T15:17:33Z</dc:date>
    </item>
    <item>
      <title>Re: How to setup the CodeWarrior in the CodeWright IDE completly?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-setup-the-CodeWarrior-in-the-CodeWright-IDE-completly/m-p/234967#M9237</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want the compiler to generate a custom error file, you need to add the options -EnvERRORFILE=&amp;lt;fileName&amp;gt; and -WOutFileOn.&lt;/P&gt;&lt;P&gt;For example to generate a file called MyErrors.txt use -EnvERRORFILE=MyErrors.txt and -WOutFileOn&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding the format of the generated error message, there is an option -WmsgFb allowing to modify the generated error message format.&lt;/P&gt;&lt;P&gt;Using it you might be able to adjust the message format to what CodeWright expects.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Take a look at the MCU_HCS08_compiler.pdf for information about this option.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jan 2013 07:05:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-setup-the-CodeWarrior-in-the-CodeWright-IDE-completly/m-p/234967#M9237</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2013-01-25T07:05:12Z</dc:date>
    </item>
    <item>
      <title>Re: How to setup the CodeWarrior in the CodeWright IDE completly?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-setup-the-CodeWarrior-in-the-CodeWright-IDE-completly/m-p/234968#M9238</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;now there are enough informations trough activating the "verbose format" with -WmsgFbv. But at the moment when I am executing CodeWarrior from CodeWright with the following line:&lt;/P&gt;&lt;P&gt;C:\Freescale\CodeWarrior for Microcontrollers V6.3\bin\ide.exe c:\.....{PROJECTNAME}.mcp /t "{TARGETNAME}" /r /b /q&amp;nbsp;&amp;nbsp;&amp;nbsp; with the Options "No cmd shell" and "Save all files".&lt;/P&gt;&lt;P&gt;After the execution the content of the Errorfile is deleted.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And even if this would be fixed I would still have problem with the parser. Do I have to write a new parser in this case or can I use one of the predefined parsers of CodeWright?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thx a lot for the support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Jan 2013 16:06:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-setup-the-CodeWarrior-in-the-CodeWright-IDE-completly/m-p/234968#M9238</guid>
      <dc:creator>elsalvadore</dc:creator>
      <dc:date>2013-01-28T16:06:25Z</dc:date>
    </item>
  </channel>
</rss>