<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Create a new CW project for TWR-Wifi-AR4100P in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Create-a-new-CW-project-for-TWR-Wifi-AR4100P/m-p/234800#M9223</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The way I solved this issue is easy but time consuming. Basically I created a new project using New MQX project Wizard. In the wizard I added rtcs library by right click on source folder and click on "add file". After that I added all AR4100-wifi library files from Qualcomm. The library is huge but after adding all files the project up and running. right now, I am able to debug the code and use MQX tool for task monitoring in my project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 Jan 2014 17:49:21 GMT</pubDate>
    <dc:creator>amleng</dc:creator>
    <dc:date>2014-01-20T17:49:21Z</dc:date>
    <item>
      <title>Create a new CW project for TWR-Wifi-AR4100P</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Create-a-new-CW-project-for-TWR-Wifi-AR4100P/m-p/234798#M9221</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Right now, I'm working on a wifi project. I use MQX 4.0.2 and installed Patch for TWR-WIFI-AR4100P. I run some demos in "atheros_wifi" folder and they work well. As I understand, all the original demo projects are linked to the wifi library files and use the functions in those files but if I create my own MQX project in CW it doesn't link to those wifi library. I tried to copy the compiler and assembler input from the demo project to my project but still I get some errors. I tried to copy one of the demos in another location and customized it but that causes the link broken to the wifi library!&amp;nbsp; So my question is how can I create a project and link to the wifi library? &lt;/P&gt;&lt;P&gt;The MQX tools (plugin) doesn't work with any of the demo projects.&lt;/P&gt;&lt;P&gt;I import web_hvac demo by drag and drop “.project” file of the project in CW 10.5 projects window and built it. Do I need to try another import approach? I appreciare you feedback.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #222222; font-family: arial, sans-serif;"&gt;Cheers!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jan 2014 20:54:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Create-a-new-CW-project-for-TWR-Wifi-AR4100P/m-p/234798#M9221</guid>
      <dc:creator>amleng</dc:creator>
      <dc:date>2014-01-14T20:54:06Z</dc:date>
    </item>
    <item>
      <title>Re: Create a new CW project for TWR-Wifi-AR4100P</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Create-a-new-CW-project-for-TWR-Wifi-AR4100P/m-p/234799#M9222</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As far as I know there are no wifi libraries (or you mean the atheros source/header files?). The code for the TWR-WIFI is merged with the default MQX libraries.&lt;/P&gt;&lt;P&gt;So, to use that code you just need to include the required libraries for your new project. If you open the web_hvac demo from the atheros_wifi folder, you can see the linked libraries by going to Project -&amp;gt; Properties -&amp;gt; C/C++ Build -&amp;gt; Settings. In the next 2 example pictures you can see the settings for the TWR-K60D100 project:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1-&lt;/STRONG&gt; If using Freescale build tools you would see this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Libraries_FSL.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41665iF07996AA1DCE213A/image-size/large?v=v2&amp;amp;px=999" role="button" title="Libraries_FSL.png" alt="Libraries_FSL.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2-&lt;/STRONG&gt; If using GCC build tools:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Libraries_GCC.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41667iAD1FB84014187B69/image-size/large?v=v2&amp;amp;px=999" role="button" title="Libraries_GCC.png" alt="Libraries_GCC.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this is useful!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jan 2014 03:58:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Create-a-new-CW-project-for-TWR-Wifi-AR4100P/m-p/234799#M9222</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-01-15T03:58:55Z</dc:date>
    </item>
    <item>
      <title>Re: Create a new CW project for TWR-Wifi-AR4100P</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Create-a-new-CW-project-for-TWR-Wifi-AR4100P/m-p/234800#M9223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The way I solved this issue is easy but time consuming. Basically I created a new project using New MQX project Wizard. In the wizard I added rtcs library by right click on source folder and click on "add file". After that I added all AR4100-wifi library files from Qualcomm. The library is huge but after adding all files the project up and running. right now, I am able to debug the code and use MQX tool for task monitoring in my project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jan 2014 17:49:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Create-a-new-CW-project-for-TWR-Wifi-AR4100P/m-p/234800#M9223</guid>
      <dc:creator>amleng</dc:creator>
      <dc:date>2014-01-20T17:49:21Z</dc:date>
    </item>
  </channel>
</rss>