<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Re: CW 10.3 Compilation Latency on Network drive</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-3-Compilation-Latency-on-Network-drive/m-p/231044#M9111</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Erich for your answer. Unfortunately I have disable all security process (FW, antivirus,...) and dit not see any benefit.&lt;/P&gt;&lt;P&gt;I would imagine it is a bad spliting of the file stored locally and those one related to user data which have to be store on the NAS server. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Jan 2013 18:11:20 GMT</pubDate>
    <dc:creator>philippeborghin</dc:creator>
    <dc:date>2013-01-23T18:11:20Z</dc:date>
    <item>
      <title>CW 10.3 Compilation Latency on Network drive</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-3-Compilation-Latency-on-Network-drive/m-p/231042#M9109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have just installed the CW 10.3 on Windows 7 64bits. Works fine execpt the following point which I can not understand perfectly.&lt;/P&gt;&lt;P&gt;When the project (for ex. the attached project) is installed on local drive it is compiles in around 9s...not so fast but ok I can live with that&lt;/P&gt;&lt;P&gt;When same project is installed on my Network drive attached to LAN running at 100Mbps effective troughput is compiled in more than 40s which is just unacceptable in development phase.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried to stop Antivirus, and Firewall -&amp;gt; no change&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any configuration I have to do to optimized such bahaviour ?&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance for your help&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Philippe&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-339048"&gt;TEST_1.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 20 Jan 2013 09:25:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-3-Compilation-Latency-on-Network-drive/m-p/231042#M9109</guid>
      <dc:creator>philippeborghin</dc:creator>
      <dc:date>2013-01-20T09:25:18Z</dc:date>
    </item>
    <item>
      <title>Re: CW 10.3 Compilation Latency on Network drive</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-3-Compilation-Latency-on-Network-drive/m-p/231043#M9110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;For ARM gcc, there is a tip available on &lt;A href="http://mcuoneclipse.com/2013/01/09/reducing-the-build-time-with-gcc-for-arm-and-codewarrior/" title="http://mcuoneclipse.com/2013/01/09/reducing-the-build-time-with-gcc-for-arm-and-codewarrior/"&gt;Reducing the build time with gcc for ARM and CodeWarrior | MCU on Eclipse.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;But then I realized that this if for ColdFire and that you do not generate a listing file.&lt;/P&gt;&lt;P&gt;From the past I know that a virus scanner might be impacting file I/O especially over network a lot. Can you try if you see a difference if you temporarily disable the firewall/virus scanner?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 20 Jan 2013 10:39:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-3-Compilation-Latency-on-Network-drive/m-p/231043#M9110</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2013-01-20T10:39:17Z</dc:date>
    </item>
    <item>
      <title>Re: CW 10.3 Compilation Latency on Network drive</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-3-Compilation-Latency-on-Network-drive/m-p/231044#M9111</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Erich for your answer. Unfortunately I have disable all security process (FW, antivirus,...) and dit not see any benefit.&lt;/P&gt;&lt;P&gt;I would imagine it is a bad spliting of the file stored locally and those one related to user data which have to be store on the NAS server. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Jan 2013 18:11:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-3-Compilation-Latency-on-Network-drive/m-p/231044#M9111</guid>
      <dc:creator>philippeborghin</dc:creator>
      <dc:date>2013-01-23T18:11:20Z</dc:date>
    </item>
    <item>
      <title>Re: CW 10.3 Compilation Latency on Network drive</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-3-Compilation-Latency-on-Network-drive/m-p/231045#M9112</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Philippe,&lt;/P&gt;&lt;P&gt;to bad. Do you have only the project on the NAS, or is your workspace on the NAS too? Eclipse stores information into the .metadata&amp;nbsp; inside the workspace folder, so this might have an impact.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Jan 2013 18:29:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-3-Compilation-Latency-on-Network-drive/m-p/231045#M9112</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2013-01-23T18:29:55Z</dc:date>
    </item>
  </channel>
</rss>