<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Ignore interrupts when stepping the debugger in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Ignore-interrupts-when-stepping-the-debugger/m-p/228937#M9034</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm sorry, I'm not using PowerPC, and do not have a workaround. Only that you might disable the interrupts with a script (Debugger shell) maybe?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Nov 2013 16:15:40 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2013-11-26T16:15:40Z</dc:date>
    <item>
      <title>Ignore interrupts when stepping the debugger</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Ignore-interrupts-when-stepping-the-debugger/m-p/228932#M9029</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using CW 10.5 is it possible to configure the debugger to ignore interrupts while stepping?&amp;nbsp; I see this is possible using the classic IDE from the following post:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" data-containerid="2031" data-containertype="14" data-objectid="302141" data-objecttype="1" href="https://community.nxp.com/thread/302141#307587"&gt;https://community.freescale.com/message/307587#307587&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2013 14:44:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Ignore-interrupts-when-stepping-the-debugger/m-p/228932#M9029</guid>
      <dc:creator>twp</dc:creator>
      <dc:date>2013-11-26T14:44:21Z</dc:date>
    </item>
    <item>
      <title>Re: Ignore interrupts when stepping the debugger</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Ignore-interrupts-when-stepping-the-debugger/m-p/228933#M9030</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it is there since MCU10.2 (&lt;A href="http://mcuoneclipse.com/2012/02/06/mcu10-2-is-here-or-4-t-shirts-in-13-weeks/" title="http://mcuoneclipse.com/2012/02/06/mcu10-2-is-here-or-4-t-shirts-in-13-weeks/"&gt;MCU10.2 is here! Or: 4 t-shirts in 13 weeks… | MCU on Eclipse&lt;/A&gt;):&lt;/P&gt;&lt;P&gt;see attached screenshot: it is in the debug/launch configuration under 'interrupts'.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2013 14:54:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Ignore-interrupts-when-stepping-the-debugger/m-p/228933#M9030</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2013-11-26T14:54:18Z</dc:date>
    </item>
    <item>
      <title>Re: Ignore interrupts when stepping the debugger</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Ignore-interrupts-when-stepping-the-debugger/m-p/228934#M9031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That's where I would expect it to be, but I don't have that tab:&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41317i9CAD80354650A71D/image-size/large?v=v2&amp;amp;px=999" title="no_interrupt_tab.png" alt="no_interrupt_tab.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Is this due to using a PnE MultiLink or is this due to the processor type MPC5643L?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2013 15:43:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Ignore-interrupts-when-stepping-the-debugger/m-p/228934#M9031</guid>
      <dc:creator>twp</dc:creator>
      <dc:date>2013-11-26T15:43:18Z</dc:date>
    </item>
    <item>
      <title>Re: Ignore interrupts when stepping the debugger</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Ignore-interrupts-when-stepping-the-debugger/m-p/228935#M9032</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That setting is specific to each architecture. Looks like it is not implemented for PowerPC.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2013 15:45:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Ignore-interrupts-when-stepping-the-debugger/m-p/228935#M9032</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2013-11-26T15:45:16Z</dc:date>
    </item>
    <item>
      <title>Re: Ignore interrupts when stepping the debugger</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Ignore-interrupts-when-stepping-the-debugger/m-p/228936#M9033</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Any suggestions for a work around?&amp;nbsp; It makes it very difficult to debug without that setting as the thread stack looses the last code position when jumping in to an interrupt, Codewarrior also seems to close the file containing the code at the deepest point of the call stack.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2013 15:53:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Ignore-interrupts-when-stepping-the-debugger/m-p/228936#M9033</guid>
      <dc:creator>twp</dc:creator>
      <dc:date>2013-11-26T15:53:30Z</dc:date>
    </item>
    <item>
      <title>Re: Ignore interrupts when stepping the debugger</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Ignore-interrupts-when-stepping-the-debugger/m-p/228937#M9034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm sorry, I'm not using PowerPC, and do not have a workaround. Only that you might disable the interrupts with a script (Debugger shell) maybe?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2013 16:15:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Ignore-interrupts-when-stepping-the-debugger/m-p/228937#M9034</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2013-11-26T16:15:40Z</dc:date>
    </item>
    <item>
      <title>Re: Ignore interrupts when stepping the debugger</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Ignore-interrupts-when-stepping-the-debugger/m-p/228938#M9035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Twp,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately there is no option to disable interrupts when stepping available in CW MCUs v10.5 for e200.&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt; This request has been already logged a feature request under the number ENGR00229357.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;You can e.g. manually control EE bit in MSR register in the Register View to enable/disable interrupts as a workaround.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41929i1A064C1398619ADC/image-size/large?v=v2&amp;amp;px=999" title="CW10_5_Register_View_Disable_Enable_External_interrrupts.png" alt="CW10_5_Register_View_Disable_Enable_External_interrrupts.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you need the interrupt handlers running on the background while stepping you can use "Run To Line" (Ctrl+R) and manually move line (cursor) at next code line as a workaround&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jan 2014 17:54:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Ignore-interrupts-when-stepping-the-debugger/m-p/228938#M9035</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2014-01-20T17:54:44Z</dc:date>
    </item>
  </channel>
</rss>