<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックCW 10.3 Code analysis with command line defines</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-3-Code-analysis-with-command-line-defines/m-p/227449#M9014</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If types/code or whatever are switched in or out via a command line define (-d XXX in the project Properties-&amp;gt;C/C++ Build-&amp;gt;Settings-&amp;gt;Language settitngs-&amp;gt;Other flags) the IDE does not seem to recognize that that they are set.&amp;nbsp; It seems to assume they are not defined.&amp;nbsp; It works fine if they are set in an include file. Is there any way to get this to work correctly?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Mar 2013 14:22:14 GMT</pubDate>
    <dc:creator>mikestich</dc:creator>
    <dc:date>2013-03-15T14:22:14Z</dc:date>
    <item>
      <title>CW 10.3 Code analysis with command line defines</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-3-Code-analysis-with-command-line-defines/m-p/227449#M9014</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If types/code or whatever are switched in or out via a command line define (-d XXX in the project Properties-&amp;gt;C/C++ Build-&amp;gt;Settings-&amp;gt;Language settitngs-&amp;gt;Other flags) the IDE does not seem to recognize that that they are set.&amp;nbsp; It seems to assume they are not defined.&amp;nbsp; It works fine if they are set in an include file. Is there any way to get this to work correctly?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Mar 2013 14:22:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-3-Code-analysis-with-command-line-defines/m-p/227449#M9014</guid>
      <dc:creator>mikestich</dc:creator>
      <dc:date>2013-03-15T14:22:14Z</dc:date>
    </item>
    <item>
      <title>Re: CW 10.3 Code analysis with command line defines</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-3-Code-analysis-with-command-line-defines/m-p/227450#M9015</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You need to define it throught the compiler &amp;gt; Preprocessor settings.&lt;/P&gt;&lt;P&gt;See&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2012/10/05/compiler-defines-and-eclipse-editor-highlighting/" title="http://mcuoneclipse.com/2012/10/05/compiler-defines-and-eclipse-editor-highlighting/"&gt;Compiler Defines and Eclipse Editor Highlighting | MCU on Eclipse&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Mar 2013 14:59:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-3-Code-analysis-with-command-line-defines/m-p/227450#M9015</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2013-03-15T14:59:06Z</dc:date>
    </item>
    <item>
      <title>Re: CW 10.3 Code analysis with command line defines</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-3-Code-analysis-with-command-line-defines/m-p/227451#M9016</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unfortunately I'm using the Freescale Coldfire. I have my defines set up exactly how the link you reference says I should. However, it says that the solution that works in other cases does not exist for that compiler.&amp;nbsp; Looks like I'm stuck with the Editor not knowing about the defines.&amp;nbsp; Thanks for the pointer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Mar 2013 18:27:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-3-Code-analysis-with-command-line-defines/m-p/227451#M9016</guid>
      <dc:creator>mikestich</dc:creator>
      <dc:date>2013-03-15T18:27:04Z</dc:date>
    </item>
    <item>
      <title>Re: CW 10.3 Code analysis with command line defines</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-3-Code-analysis-with-command-line-defines/m-p/227452#M9017</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;But wait!&amp;nbsp; I went and actually looked in my project and there is a "Symbols" tab under the Paths and Symbols resource.&amp;nbsp; Moved all my -d defines there and all works great now, complete with appropriate highlighting in the editor.&amp;nbsp; Thanks much!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Mar 2013 18:36:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-3-Code-analysis-with-command-line-defines/m-p/227452#M9017</guid>
      <dc:creator>mikestich</dc:creator>
      <dc:date>2013-03-15T18:36:33Z</dc:date>
    </item>
  </channel>
</rss>