<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: CW10.2 .s19 files</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-2-s19-files/m-p/221788#M8802</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a project which we changed the .bbl file directly to 32 bit address and when I compile the S19 output changes accordingly from 0x0000 to 0x00000000. You will see how it works when you open the bbl file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you try this and can not work it out let me know and I will track the project down, open it all up and find the change I made.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Oct 2012 22:09:07 GMT</pubDate>
    <dc:creator>CarlFST60L</dc:creator>
    <dc:date>2012-10-22T22:09:07Z</dc:date>
    <item>
      <title>CW10.2 .s19 files</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-2-s19-files/m-p/221786#M8800</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone figured out how to format the line length in .s19 files?&lt;/P&gt;&lt;P&gt;I need lines of 32 bytes of data max. The Linker Settings have no options for this. Furthermore, the file created has a .sx suffix.&lt;/P&gt;&lt;P&gt;Where are the .s19 options for file creation?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have gone through the Burner document and see that those options are there. Do I need the Burner to read the .abs file, process it&lt;/P&gt;&lt;P&gt;and send it to a .s19 file? One would think that these features SHOULD be set up in the Linker Settings.....&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 20 Oct 2012 20:13:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-2-s19-files/m-p/221786#M8800</guid>
      <dc:creator>bob_walker</dc:creator>
      <dc:date>2012-10-20T20:13:51Z</dc:date>
    </item>
    <item>
      <title>Re: CW10.2 .s19 files</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-2-s19-files/m-p/221787#M8801</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;the linker usually only offers the minimal settings. I use the burner as postlinker to do the more advanced stuff (see &lt;A href="http://mcuoneclipse.wordpress.com/2012/09/27/s-record-intel-hex-and-binary-files/" title="http://mcuoneclipse.wordpress.com/2012/09/27/s-record-intel-hex-and-binary-files/"&gt;S-Record, Intel Hex and Binary Files | MCU on Eclipse&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS: which microcontroller/compiler are you using, btw? Things are always a little bit different for each toolchain, e.g. gcc is different from the Freescale compilers, etc.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 21 Oct 2012 07:01:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-2-s19-files/m-p/221787#M8801</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2012-10-21T07:01:30Z</dc:date>
    </item>
    <item>
      <title>Re: CW10.2 .s19 files</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-2-s19-files/m-p/221788#M8802</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a project which we changed the .bbl file directly to 32 bit address and when I compile the S19 output changes accordingly from 0x0000 to 0x00000000. You will see how it works when you open the bbl file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you try this and can not work it out let me know and I will track the project down, open it all up and find the change I made.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Oct 2012 22:09:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-2-s19-files/m-p/221788#M8802</guid>
      <dc:creator>CarlFST60L</dc:creator>
      <dc:date>2012-10-22T22:09:07Z</dc:date>
    </item>
    <item>
      <title>Re: CW10.2 .s19 files</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-2-s19-files/m-p/221789#M8803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just what I needed. Thanks Erich and Carl.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Oct 2012 19:59:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-2-s19-files/m-p/221789#M8803</guid>
      <dc:creator>bob_walker</dc:creator>
      <dc:date>2012-10-26T19:59:50Z</dc:date>
    </item>
  </channel>
</rss>