<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックInstall CW 5.9.0 in WinXP available for ALL users</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Install-CW-5-9-0-in-WinXP-available-for-ALL-users/m-p/216994#M8560</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I've installed the Special Edition CW 5.9.0 as administrator.&amp;nbsp; It never asks if you want this to be just for the administrator or for everyone.&amp;nbsp; When a non-administrator logs in, it is in the list of programs, but is not recognized as installed.&amp;nbsp; If the user navigates down to the correct location, he can start it and run it, so it is not an issue of files not being open to the regular user.&amp;nbsp;&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 18 Sep 2009 01:17:56 GMT</pubDate>
    <dc:creator>r490</dc:creator>
    <dc:date>2009-09-18T01:17:56Z</dc:date>
    <item>
      <title>Install CW 5.9.0 in WinXP available for ALL users</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Install-CW-5-9-0-in-WinXP-available-for-ALL-users/m-p/216994#M8560</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I've installed the Special Edition CW 5.9.0 as administrator.&amp;nbsp; It never asks if you want this to be just for the administrator or for everyone.&amp;nbsp; When a non-administrator logs in, it is in the list of programs, but is not recognized as installed.&amp;nbsp; If the user navigates down to the correct location, he can start it and run it, so it is not an issue of files not being open to the regular user.&amp;nbsp;&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Sep 2009 01:17:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Install-CW-5-9-0-in-WinXP-available-for-ALL-users/m-p/216994#M8560</guid>
      <dc:creator>r490</dc:creator>
      <dc:date>2009-09-18T01:17:56Z</dc:date>
    </item>
    <item>
      <title>Re: Install CW 5.9.0 in WinXP available for ALL users</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Install-CW-5-9-0-in-WinXP-available-for-ALL-users/m-p/216995#M8561</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;it seems this was in issue in the InstallShield (the installation program) used in CW 5.9. To my understanding this has been resolved in CW 6.1 as this uses the new InstallShield which has resolved this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Sep 2009 15:57:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Install-CW-5-9-0-in-WinXP-available-for-ALL-users/m-p/216995#M8561</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2009-09-18T15:57:51Z</dc:date>
    </item>
    <item>
      <title>Re: Install CW 5.9.0 in WinXP available for ALL users</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Install-CW-5-9-0-in-WinXP-available-for-ALL-users/m-p/216996#M8562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Perhaps I've overlooked something, but the only edition I see for HCS12 family is 5.9; &amp;nbsp;the version 6.1 is for other chips, not the HCS12 family. &amp;nbsp;Someone please correct me if I'm wrong on this. &amp;nbsp;Also, is there a patch to fix this problem in 5.9 if it is a known issue?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-- RAM&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Sep 2009 19:45:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Install-CW-5-9-0-in-WinXP-available-for-ALL-users/m-p/216996#M8562</guid>
      <dc:creator>r490</dc:creator>
      <dc:date>2009-09-18T19:45:05Z</dc:date>
    </item>
    <item>
      <title>Re: Install CW 5.9.0 in WinXP available for ALL users</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Install-CW-5-9-0-in-WinXP-available-for-ALL-users/m-p/216997#M8563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Version 5.9 is the IDE version, not the actual version of the tools. To get the tools version number, select Help &amp;gt; About Freescale CodeWarrior &amp;gt; Installed Products. If you downloaded the Special Edition of the HC12 tools recently, it has to be version 5. You might file a service request to have this installer feature fixed or added.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, when posting a question, remember to include the &lt;FONT color="#ff0000"&gt;hardware target name (such as HC(S)08 or HCS12(C))&lt;/FONT&gt; along with the version number.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by J2MEJediMaster on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-09-18&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;09:06 AM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Sep 2009 20:05:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Install-CW-5-9-0-in-WinXP-available-for-ALL-users/m-p/216997#M8563</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2009-09-18T20:05:05Z</dc:date>
    </item>
    <item>
      <title>Re: Install CW 5.9.0 in WinXP available for ALL users</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Install-CW-5-9-0-in-WinXP-available-for-ALL-users/m-p/216998#M8564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi RAM,&lt;/P&gt;&lt;P&gt;I (wrongly) assumed you are using CW for MCU/HCS08. My reply was targeting to that product line, and not the S12 one.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Sep 2009 20:09:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Install-CW-5-9-0-in-WinXP-available-for-ALL-users/m-p/216998#M8564</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2009-09-18T20:09:04Z</dc:date>
    </item>
    <item>
      <title>Re: Install CW 5.9.0 in WinXP available for ALL users</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Install-CW-5-9-0-in-WinXP-available-for-ALL-users/m-p/216999#M8565</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So, I have solved this (a bit of a kludge).&amp;nbsp; I temporarily made the non-administrative user an admin.&amp;nbsp; Then installed for him, and changed him back to a member of PowerUsers group.&amp;nbsp; Seems to work for now.&lt;/P&gt;&lt;P&gt;--- RAM&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 20 Sep 2009 03:37:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Install-CW-5-9-0-in-WinXP-available-for-ALL-users/m-p/216999#M8565</guid>
      <dc:creator>r490</dc:creator>
      <dc:date>2009-09-20T03:37:01Z</dc:date>
    </item>
  </channel>
</rss>