<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Processor Expert adding 2 of the same CPU's to a project in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC08-Processor-Expert-adding-2-of-the-same-CPU-s-to-a-project/m-p/129046#M852</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;OK&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I have tried to create a project for HC08JL3 with CW HC08 V5.1.&lt;/DIV&gt;&lt;DIV&gt;I get the attached dialog opened.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;This seems to indicate that there will be 2 CPUs created in Debug configuration. One for Mon08 debug (in Clock settings -&amp;gt; CPU Mode = Monitor Mode) and one for BDM debug (in Clock settings -&amp;gt; CPU Mode =&amp;nbsp;User Mode).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;According to Processor Expert on line Help property "CPU Mode Selection" is necessary for the correct CPU's internal timing.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;CrasyCat&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Sep 2006 19:01:52 GMT</pubDate>
    <dc:creator>CrasyCat</dc:creator>
    <dc:date>2006-09-15T19:01:52Z</dc:date>
    <item>
      <title>HC08: Processor Expert adding 2 of the same CPU's to a project</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC08-Processor-Expert-adding-2-of-the-same-CPU-s-to-a-project/m-p/129042#M848</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I am just curious if anyone knows why when I select a processor to add to my project, processor expert adds 2 of them. One with a check beside it indicating it is the active processor and another one with the same exact name that has an X beside it? Every project I have created with Processor Expert has done this.&lt;/SPAN&gt;&lt;P&gt;Message Edited by CrasyCat on &lt;SPAN class="date_text"&gt;2007-04-13&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;02:16 PM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Sep 2006 08:29:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC08-Processor-Expert-adding-2-of-the-same-CPU-s-to-a-project/m-p/129042#M848</guid>
      <dc:creator>bespenschied</dc:creator>
      <dc:date>2006-09-04T08:29:16Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert adding 2 of the same CPU's to a project</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC08-Processor-Expert-adding-2-of-the-same-CPU-s-to-a-project/m-p/129043#M849</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello&lt;/DIV&gt;&lt;DIV&gt;Each HCS12 MCU may be available in different package (pinouts).&lt;/DIV&gt;&lt;DIV&gt;For example HCS12C32 is available in 80 pinout or 52 pinout or 48 pinouts.&lt;/DIV&gt;&lt;DIV&gt;Just point with the mouse to the listed CPU. The tooltips will show you the different pinouts.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;As ProcessorExpert displays port assignment, it adds the different pinouts version to your project.&lt;/DIV&gt;&lt;DIV&gt;The one&amp;nbsp; with a V in front is the current one. The one with the X are the other available variants.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If you know you will be using a 52 pinout chip, you can change the active configuration as follows:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; - Click with the right mouse button on the configuration you will be using.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; - In the pop up menu select "Select CPU as Target".&lt;/DIV&gt;&lt;DIV&gt;This will change the Configuration in ProcessorExpert to the 52-pinout one.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;CrasyCat&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Sep 2006 15:36:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC08-Processor-Expert-adding-2-of-the-same-CPU-s-to-a-project/m-p/129043#M849</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2006-09-04T15:36:30Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert adding 2 of the same CPU's to a project</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC08-Processor-Expert-adding-2-of-the-same-CPU-s-to-a-project/m-p/129044#M850</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I understand about the different pin CPU's but these cpu's show the exact number of pins and the help popup shows the same information. The chip that is showing 2 right now is the MC68HC908GT16CFB. When I selected it from the CPU list 2 of them appeared and they are both the same part. I recently updated to the new CodeWarrior V5.1 and most of my code is in V3.? and I have not converted them so I can't look to see if this has happened in the past. If It shows up again I will let you know. It may even be I double clicked the CPU. I was just curious if there was any reason it happened. &lt;BR /&gt;&lt;BR /&gt;Brian&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Sep 2006 12:57:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC08-Processor-Expert-adding-2-of-the-same-CPU-s-to-a-project/m-p/129044#M850</guid>
      <dc:creator>bespenschied</dc:creator>
      <dc:date>2006-09-14T12:57:41Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert adding 2 of the same CPU's to a project</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC08-Processor-Expert-adding-2-of-the-same-CPU-s-to-a-project/m-p/129045#M851</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I have included 2 jpg images to show you what I am talking about. I just started a new project for a new PCB I just finished designing. It uses the MC68HC908JL3CP chip. I captured an image of the display that shows each processor and the popup help text that appears when you put your mouse over the item. They are both the same.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Sep 2006 01:32:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC08-Processor-Expert-adding-2-of-the-same-CPU-s-to-a-project/m-p/129045#M851</guid>
      <dc:creator>bespenschied</dc:creator>
      <dc:date>2006-09-15T01:32:20Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert adding 2 of the same CPU's to a project</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC08-Processor-Expert-adding-2-of-the-same-CPU-s-to-a-project/m-p/129046#M852</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;OK&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I have tried to create a project for HC08JL3 with CW HC08 V5.1.&lt;/DIV&gt;&lt;DIV&gt;I get the attached dialog opened.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;This seems to indicate that there will be 2 CPUs created in Debug configuration. One for Mon08 debug (in Clock settings -&amp;gt; CPU Mode = Monitor Mode) and one for BDM debug (in Clock settings -&amp;gt; CPU Mode =&amp;nbsp;User Mode).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;According to Processor Expert on line Help property "CPU Mode Selection" is necessary for the correct CPU's internal timing.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;CrasyCat&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Sep 2006 19:01:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC08-Processor-Expert-adding-2-of-the-same-CPU-s-to-a-project/m-p/129046#M852</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2006-09-15T19:01:52Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert adding 2 of the same CPU's to a project</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC08-Processor-Expert-adding-2-of-the-same-CPU-s-to-a-project/m-p/129047#M853</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;That makes sense. I remember that selection window and I did select both of them. I did not realize that is why. I have always just changed the settings in the active device CPU mode Selection to match whatever mode I needed. When you select the other CPU the settings are not available until you make it the active part. I am not sure how usefull this is since it so easy to just change the one CPU mode setting and compile it. &lt;BR /&gt;&lt;BR /&gt;Thanks!&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 16 Sep 2006 11:03:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC08-Processor-Expert-adding-2-of-the-same-CPU-s-to-a-project/m-p/129047#M853</guid>
      <dc:creator>bespenschied</dc:creator>
      <dc:date>2006-09-16T11:03:09Z</dc:date>
    </item>
  </channel>
</rss>