<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: AEFSKIPERASING</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/AEFSKIPERASING/m-p/210062#M8231</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the response, Tom.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've already researched this in the forums, and in the help documentation, and in the app-notes, etc., etc., etc...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The flash setup in the debugger has these 5 blocks which can be protected from erasure by using AEFSKIPERASING.&lt;/P&gt;&lt;P&gt;0DFLASH&lt;/P&gt;&lt;P&gt;1FLASH_4000&lt;/P&gt;&lt;P&gt;2FLASH_8000&lt;/P&gt;&lt;P&gt;3FLASH_C000&lt;/P&gt;&lt;P&gt;4ALL_PPAGES&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What I am requesting, is to break the PFLASH into it's 3 (seperately erasable) blocks so that I can protect one of the PFLASH blocks from being erased while loading the debug code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So I would have something like this&lt;/P&gt;&lt;P&gt;0DFLASH&lt;/P&gt;&lt;P&gt;1FLASH_4000&lt;/P&gt;&lt;P&gt;2FLASH_8000&lt;/P&gt;&lt;P&gt;3FLASH_C000&lt;/P&gt;&lt;P&gt;4PFLASH_780000&lt;/P&gt;&lt;P&gt;5PFLASH_7A0000&lt;/P&gt;&lt;P&gt;6PFLASH_7C0000&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I believe this setup is controlled by the processor-specific MCU02DA.fpp file.&lt;/P&gt;&lt;P&gt;I would mess with this file if I could but it appears to be undocumented.&lt;/P&gt;&lt;P&gt;I've spoken with P&amp;amp;E Microsystems because I thought that might be something they controlled but they referred me to Freescale.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a service request opened, but, after three days with no repsonse, I decided to try the forums.&lt;/P&gt;&lt;P&gt;This morning... I finally received a response from the service request I opened last Tuesday.... (they are working on it...)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Feb 2012 22:43:57 GMT</pubDate>
    <dc:creator>kbatke</dc:creator>
    <dc:date>2012-02-27T22:43:57Z</dc:date>
    <item>
      <title>AEFSKIPERASING</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/AEFSKIPERASING/m-p/210060#M8229</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using CodeWarrior v5.1 with 9S12XEQ512 processsor.&amp;nbsp;&lt;BR /&gt;This processor has 3 blocks of P-FLASH but when I try to use AEFSKIPERASING, I&amp;nbsp;&lt;BR /&gt;can only select ALL of P-FLASH to be skipped.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Would it be possible to create the .fpp or whatever files need to be created&amp;nbsp;&lt;BR /&gt;that would split the P-FLASH into it's 3 blocks (for this processor... more or&amp;nbsp;&lt;BR /&gt;less for others).&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I would like finer control using AEFSKIPERASING. Specifically, I would like to&amp;nbsp;&lt;BR /&gt;skip erasing one of the P-FLASH blocks as I am programming an array that I&amp;nbsp;&lt;BR /&gt;don't want erased every time load the debugger from CodeWarrior.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 25 Feb 2012 04:03:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/AEFSKIPERASING/m-p/210060#M8229</guid>
      <dc:creator>kbatke</dc:creator>
      <dc:date>2012-02-25T04:03:59Z</dc:date>
    </item>
    <item>
      <title>Re: AEFSKIPERASING</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/AEFSKIPERASING/m-p/210061#M8230</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You might want to check out this &lt;A href="https://community.freescale.com/message/44136#44136" title="https://community.freescale.com/message/44136#44136"&gt;https://community.freescale.com/message/44136#44136&lt;/A&gt;. Also, use the forum search function to look for any occurences of "AEFSKIPERASING".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Feb 2012 22:10:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/AEFSKIPERASING/m-p/210061#M8230</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2012-02-27T22:10:30Z</dc:date>
    </item>
    <item>
      <title>Re: AEFSKIPERASING</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/AEFSKIPERASING/m-p/210062#M8231</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the response, Tom.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've already researched this in the forums, and in the help documentation, and in the app-notes, etc., etc., etc...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The flash setup in the debugger has these 5 blocks which can be protected from erasure by using AEFSKIPERASING.&lt;/P&gt;&lt;P&gt;0DFLASH&lt;/P&gt;&lt;P&gt;1FLASH_4000&lt;/P&gt;&lt;P&gt;2FLASH_8000&lt;/P&gt;&lt;P&gt;3FLASH_C000&lt;/P&gt;&lt;P&gt;4ALL_PPAGES&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What I am requesting, is to break the PFLASH into it's 3 (seperately erasable) blocks so that I can protect one of the PFLASH blocks from being erased while loading the debug code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So I would have something like this&lt;/P&gt;&lt;P&gt;0DFLASH&lt;/P&gt;&lt;P&gt;1FLASH_4000&lt;/P&gt;&lt;P&gt;2FLASH_8000&lt;/P&gt;&lt;P&gt;3FLASH_C000&lt;/P&gt;&lt;P&gt;4PFLASH_780000&lt;/P&gt;&lt;P&gt;5PFLASH_7A0000&lt;/P&gt;&lt;P&gt;6PFLASH_7C0000&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I believe this setup is controlled by the processor-specific MCU02DA.fpp file.&lt;/P&gt;&lt;P&gt;I would mess with this file if I could but it appears to be undocumented.&lt;/P&gt;&lt;P&gt;I've spoken with P&amp;amp;E Microsystems because I thought that might be something they controlled but they referred me to Freescale.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a service request opened, but, after three days with no repsonse, I decided to try the forums.&lt;/P&gt;&lt;P&gt;This morning... I finally received a response from the service request I opened last Tuesday.... (they are working on it...)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Feb 2012 22:43:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/AEFSKIPERASING/m-p/210062#M8231</guid>
      <dc:creator>kbatke</dc:creator>
      <dc:date>2012-02-27T22:43:57Z</dc:date>
    </item>
    <item>
      <title>Re: AEFSKIPERASING</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/AEFSKIPERASING/m-p/210063#M8232</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The forum editor deleted my tabs&amp;nbsp;&lt;IMG alt=":smileyfrustrated:" class="emoticon emoticon-smileyfrustrated" id="smileyfrustrated" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-frustrated.gif" title="Smiley Frustrated" /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is what I have:&lt;/P&gt;&lt;P&gt;0-DFLASH&lt;/P&gt;&lt;P&gt;1-FLASH_4000&lt;/P&gt;&lt;P&gt;2-FLASH_8000&lt;/P&gt;&lt;P&gt;3-FLASH_C000&lt;/P&gt;&lt;P&gt;4-ALL_PPAGES&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is what I want:&lt;/P&gt;&lt;P&gt;0-DFLASH&lt;/P&gt;&lt;P&gt;1-FLASH_4000&lt;/P&gt;&lt;P&gt;2-FLASH_8000&lt;/P&gt;&lt;P&gt;3-FLASH_C000&lt;/P&gt;&lt;P&gt;4-PFLASH_780000&lt;/P&gt;&lt;P&gt;5-PFLASH_7A0000&lt;/P&gt;&lt;P&gt;6-PFLASH_7C0000&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Keith Batke&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Feb 2012 22:46:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/AEFSKIPERASING/m-p/210063#M8232</guid>
      <dc:creator>kbatke</dc:creator>
      <dc:date>2012-02-27T22:46:57Z</dc:date>
    </item>
    <item>
      <title>Re: AEFSKIPERASING</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/AEFSKIPERASING/m-p/210064#M8233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Keith,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am looking to be able to do the same as you - and have also drawn a blank.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I know that the mcu03cd.fpp file defines the list of 'FLASH' that you get to see, and this is inherited from hcs12_common.fpp.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The documentation shows a screenshot with seperate flash pages listed, but there is mention that due to some devices having a large number of pages, they have been 'shrunk' to speed things up !&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I wish there was an 'unshrink' option !&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Did you get a reponse from freescale at all ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Andy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Apr 2012 22:34:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/AEFSKIPERASING/m-p/210064#M8233</guid>
      <dc:creator>AndyUK</dc:creator>
      <dc:date>2012-04-06T22:34:07Z</dc:date>
    </item>
  </channel>
</rss>