<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックPower Cycle Dialog</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Power-Cycle-Dialog/m-p/209269#M8181</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Processor: MC9S08EL32CTL&lt;/P&gt;&lt;P&gt;Emulator:&amp;nbsp; PE Microlink USB Interface&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was debugging my device in Code Warrior.&amp;nbsp; Everything was running fine. I was stepping through an analog conversion -- I had done several channels already when a probe slipped and the processor reset. After that the debugging session locked up and I couldn't run or step. I exited the simulator and restarted the debug session, but every time I would get the Power Cycle Dialog that tells me to recycle power to the MCU and then hit okay. I did this several times, and reinserted cables etc. but it always came up with the Power Cycle dialog. over and over. I tried a new board and it does the same thing. The processor seems fine since it runs fine on a power up not in debug mode. I'm thinking something is wrong with the emulator. How can I tell?&amp;nbsp; Both blue and amber LEDs are on. The BGND line is at 0.28V when the dialog comes up, then it goes to 2.78 when I hit okay. I have 4.98V on the 5V line.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Thanks for any help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Feb 2012 12:04:41 GMT</pubDate>
    <dc:creator>jam_petersen</dc:creator>
    <dc:date>2012-02-23T12:04:41Z</dc:date>
    <item>
      <title>Power Cycle Dialog</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Power-Cycle-Dialog/m-p/209269#M8181</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Processor: MC9S08EL32CTL&lt;/P&gt;&lt;P&gt;Emulator:&amp;nbsp; PE Microlink USB Interface&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was debugging my device in Code Warrior.&amp;nbsp; Everything was running fine. I was stepping through an analog conversion -- I had done several channels already when a probe slipped and the processor reset. After that the debugging session locked up and I couldn't run or step. I exited the simulator and restarted the debug session, but every time I would get the Power Cycle Dialog that tells me to recycle power to the MCU and then hit okay. I did this several times, and reinserted cables etc. but it always came up with the Power Cycle dialog. over and over. I tried a new board and it does the same thing. The processor seems fine since it runs fine on a power up not in debug mode. I'm thinking something is wrong with the emulator. How can I tell?&amp;nbsp; Both blue and amber LEDs are on. The BGND line is at 0.28V when the dialog comes up, then it goes to 2.78 when I hit okay. I have 4.98V on the 5V line.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Thanks for any help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Feb 2012 12:04:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Power-Cycle-Dialog/m-p/209269#M8181</guid>
      <dc:creator>jam_petersen</dc:creator>
      <dc:date>2012-02-23T12:04:41Z</dc:date>
    </item>
    <item>
      <title>Re: Power Cycle Dialog</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Power-Cycle-Dialog/m-p/209270#M8182</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What voltage you see on BGND when BDM is disconnected? Maybe EL32 internal&amp;nbsp;weak BGND pullup got damaged. If you don't have any pull up resistor on BGND,&amp;nbsp;then try soldering something like 4.7kOhm between BGND and Vdd. You need that voltage to rise above Vih=0.65*Vdd, which is&amp;nbsp;3.25V in your case&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Feb 2012 16:07:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Power-Cycle-Dialog/m-p/209270#M8182</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2012-02-23T16:07:22Z</dc:date>
    </item>
  </channel>
</rss>