<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: A hardware reset might have occurred</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/A-hardware-reset-might-have-occurred/m-p/208588#M8136</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;The message means that the BDM lost contact with the CPU. There could be several causes. HW reset, changing the bus clock through the PLL, self-clock mode (external oscillator malfunctioning), noise on the BDM signal line (no pull-up or too long cable), buggy code jumping to wrong addresses etc etc.&lt;BR /&gt;&lt;BR /&gt;So this may or may not be an issue, depending on the cause of the lost connection.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Dec 2008 23:25:28 GMT</pubDate>
    <dc:creator>Lundin</dc:creator>
    <dc:date>2008-12-10T23:25:28Z</dc:date>
    <item>
      <title>A hardware reset might have occurred</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/A-hardware-reset-might-have-occurred/m-p/208587#M8135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;HCS12NE64 with PE Micro USB Multilink in Codewarrior often (but not always) produces the message, "A hardware reset might have occurred".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In the past have had code which always produced that message but was never sure what I did that put an end to it. Never could narrow it down to a single line of code, only a general region.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Am pretty sure my CPU is *not* executing a RESET as my variables are not being cleared by Init().&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is this message something for concern? The "might" choice of words suggests the PE Micro developers gave up on trying to absolutely state a RESET has occurred.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Dec 2008 06:38:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/A-hardware-reset-might-have-occurred/m-p/208587#M8135</guid>
      <dc:creator>dkelly</dc:creator>
      <dc:date>2008-12-10T06:38:23Z</dc:date>
    </item>
    <item>
      <title>Re: A hardware reset might have occurred</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/A-hardware-reset-might-have-occurred/m-p/208588#M8136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;The message means that the BDM lost contact with the CPU. There could be several causes. HW reset, changing the bus clock through the PLL, self-clock mode (external oscillator malfunctioning), noise on the BDM signal line (no pull-up or too long cable), buggy code jumping to wrong addresses etc etc.&lt;BR /&gt;&lt;BR /&gt;So this may or may not be an issue, depending on the cause of the lost connection.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Dec 2008 23:25:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/A-hardware-reset-might-have-occurred/m-p/208588#M8136</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2008-12-10T23:25:28Z</dc:date>
    </item>
  </channel>
</rss>