<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: S19 and phy files</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/S19-and-phy-files/m-p/204435#M7826</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kef,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your clarification.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Normally I am using&amp;nbsp;Codewarrior Hiwave debugger and P&amp;amp;E Multilink hardware but in one case I have only s19 file which I need to program to MC9S12A128 using BDM multilink. Here I have to use the conversion utility to get phy file and use with BDM. Am I correct?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Jun 2010 22:01:01 GMT</pubDate>
    <dc:creator>SSK</dc:creator>
    <dc:date>2010-06-02T22:01:01Z</dc:date>
    <item>
      <title>S19 and phy files</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/S19-and-phy-files/m-p/204431#M7822</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Forum members,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using CodeWarrior 5.7 with MC9S12A128 processor. When I build my project I find two output files in the bin folder - s19 and phy alongwith abs and map files. Can anyone tell the difference between the two s19 and phy files? When to use s19 and when to use phy file?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using P &amp;amp; E BDM multilink debugger to download the out file to target. When I use s19 file with BDM multilink, it gives some memory error but works fine with phy file. What is the reason for this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have an old s19 file but not the phy file and want to use this s19 to download to target using BDM multilink but as s19 is not accepted by BDM, I am unable to download the same? How should I proceed?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Your earliest help in this regard will be highly appreciated. Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Jun 2010 22:09:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/S19-and-phy-files/m-p/204431#M7822</guid>
      <dc:creator>SSK</dc:creator>
      <dc:date>2010-06-01T22:09:50Z</dc:date>
    </item>
    <item>
      <title>Re: S19 and phy files</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/S19-and-phy-files/m-p/204432#M7823</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;S19 file contains S records with "logical" or "banked" addresses. S2 record&amp;nbsp;address in such format is PPAGE * 0x10000 + 16bits CPU address.&lt;/P&gt;&lt;P&gt;Phy&amp;nbsp; file contains S records with "physical" or "linear" addresses. Linear S2 address is PPAGE * 0x4000 + CPU address mod 0x4000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can convert S records from one format to another. You may look at Freescale web for SRecCvt utility or at &lt;A href="http://www.pemicro.com" rel="nofollow" target="_blank"&gt;www.pemicro.com&lt;/A&gt; for Log2Phy utility.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jun 2010 01:18:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/S19-and-phy-files/m-p/204432#M7823</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2010-06-02T01:18:26Z</dc:date>
    </item>
    <item>
      <title>Re: S19 and phy files</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/S19-and-phy-files/m-p/204433#M7824</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks kef for your reply.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I will use the log2phy utility to convert s19 file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can I use s19 directly with BDM multilink? or BDM only accepts phy format?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What&amp;nbsp;setup is needed if s19 is to be used without converting to another format?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jun 2010 12:37:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/S19-and-phy-files/m-p/204433#M7824</guid>
      <dc:creator>SSK</dc:creator>
      <dc:date>2010-06-02T12:37:50Z</dc:date>
    </item>
    <item>
      <title>Re: S19 and phy files</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/S19-and-phy-files/m-p/204434#M7825</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;BDM multilink can't download S records, it's just a hardware&amp;nbsp;that is often used&amp;nbsp;to connect PC to target MCU.&amp;nbsp;&amp;nbsp;In you starting post by "P &amp;amp; E BDM multilink debugger" did you mean Codewarrior Hiwave debugger and P&amp;amp;E Multilink hardware? Because it depends what debugger software you are using. You could use NoICE debugger (&lt;A href="http://www.noicedebugger.com" rel="nofollow" target="_blank"&gt;www.noicedebugger.com&lt;/A&gt;) with Multilink.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;NoICE simply allows you to check/uncheck in load file&amp;nbsp;dialog "S2 records have linear addresses" checkbox.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In Hiwave it is more difficult.&amp;nbsp;FAQ-27684 is for S12X MCU's. It is almost the same for non-X S12, but you should use in step 3 different ini file string&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;SRECISHCS12LINEARADR=1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;instead of&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;SRECISS12XGLOBALADR=1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;A href="http://www.freescale.com/webapp/sps/utils/SingleFaq.jsp?FAQ-27684.xml" rel="nofollow" target="_blank"&gt;http://www.freescale.com/webapp/sps/utils/SingleFaq.jsp?FAQ-27684.xml&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jun 2010 13:41:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/S19-and-phy-files/m-p/204434#M7825</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2010-06-02T13:41:07Z</dc:date>
    </item>
    <item>
      <title>Re: S19 and phy files</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/S19-and-phy-files/m-p/204435#M7826</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kef,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your clarification.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Normally I am using&amp;nbsp;Codewarrior Hiwave debugger and P&amp;amp;E Multilink hardware but in one case I have only s19 file which I need to program to MC9S12A128 using BDM multilink. Here I have to use the conversion utility to get phy file and use with BDM. Am I correct?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jun 2010 22:01:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/S19-and-phy-files/m-p/204435#M7826</guid>
      <dc:creator>SSK</dc:creator>
      <dc:date>2010-06-02T22:01:01Z</dc:date>
    </item>
    <item>
      <title>Re: S19 and phy files</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/S19-and-phy-files/m-p/204436#M7827</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hiwave debugger uses banked/paged S records by default. To load linear/physical S records you need either to 1) convert from linear to banked format or to 2) follow FAQ from above, of course using SRECISHCS12LINEARADR=1 string instead of specified in the FAQ.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jun 2010 22:24:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/S19-and-phy-files/m-p/204436#M7827</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2010-06-02T22:24:51Z</dc:date>
    </item>
  </channel>
</rss>