<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Link in files not found problem</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Link-in-files-not-found-problem/m-p/203763#M7780</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is driving me up the wall,&amp;nbsp; I am using CW10.1, Windows 7 64 bit&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a commom monitor that is used in many projects.&lt;/P&gt;&lt;P&gt;so want to reference the Monitor files in a commom refereced directory.&lt;/P&gt;&lt;P&gt;So when I add the files to the project, I select the option to link the files to the project&lt;/P&gt;&lt;P&gt;thus if I need to enhance or correct something in the monitor the changes will flow across all projects&lt;/P&gt;&lt;P&gt;This seems to work just fine with the C files.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;but linking in the header files for the related C files - - - I can open and edit the file but&lt;/P&gt;&lt;P&gt;when compiling, these header files are not found.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This seems to only be a problem with linked C files&lt;/P&gt;&lt;P&gt;Help this is driving me up the wall.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jim P&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 May 2011 01:44:06 GMT</pubDate>
    <dc:creator>Jim_P</dc:creator>
    <dc:date>2011-05-06T01:44:06Z</dc:date>
    <item>
      <title>Link in files not found problem</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Link-in-files-not-found-problem/m-p/203763#M7780</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is driving me up the wall,&amp;nbsp; I am using CW10.1, Windows 7 64 bit&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a commom monitor that is used in many projects.&lt;/P&gt;&lt;P&gt;so want to reference the Monitor files in a commom refereced directory.&lt;/P&gt;&lt;P&gt;So when I add the files to the project, I select the option to link the files to the project&lt;/P&gt;&lt;P&gt;thus if I need to enhance or correct something in the monitor the changes will flow across all projects&lt;/P&gt;&lt;P&gt;This seems to work just fine with the C files.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;but linking in the header files for the related C files - - - I can open and edit the file but&lt;/P&gt;&lt;P&gt;when compiling, these header files are not found.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This seems to only be a problem with linked C files&lt;/P&gt;&lt;P&gt;Help this is driving me up the wall.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jim P&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 May 2011 01:44:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Link-in-files-not-found-problem/m-p/203763#M7780</guid>
      <dc:creator>Jim_P</dc:creator>
      <dc:date>2011-05-06T01:44:06Z</dc:date>
    </item>
    <item>
      <title>Re: Link in files not found problem</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Link-in-files-not-found-problem/m-p/203764#M7781</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In order to allow the compiler to find the header files, the paths to the header files needs to be added to the include file paths.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you are building for HCS08 MCU, these are specified in C/C++ Build &amp;gt; Settings &amp;gt; HC08 Compiler &amp;gt; Input &amp;gt; Include File Path edit box.&lt;/P&gt;&lt;P&gt;If you are building for Coldfire MCU these are specified in C/C++ Build &amp;gt; Settings &amp;gt; ColdFilre Compiler &amp;gt; Input &amp;gt; User Path&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 May 2011 18:44:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Link-in-files-not-found-problem/m-p/203764#M7781</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2011-05-09T18:44:36Z</dc:date>
    </item>
  </channel>
</rss>