<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: version 10, change s19 file name?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/version-10-change-s19-file-name/m-p/203074#M7696</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;if you are using in your project the Burner to create the S19 file, then have a look at the burner.bbl inside the Project_Settings/Linker_Files/burner.bbl:&lt;/P&gt;&lt;P&gt;there is&lt;/P&gt;&lt;P&gt;OPENFILE "%ABS_FILE%.s19"&lt;BR /&gt;format=motorola&lt;BR /&gt;busWidth=1&lt;BR /&gt;origin=0&lt;BR /&gt;len=0x1000000&lt;BR /&gt;destination=0&lt;BR /&gt;SRECORD=Sx&lt;BR /&gt;SENDBYTE 1 "%ABS_FILE%"&lt;BR /&gt;CLOSE&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;So you can change the OPENFILE line to whatever you like.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 May 2011 22:05:36 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2011-05-03T22:05:36Z</dc:date>
    <item>
      <title>version 10, change s19 file name?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/version-10-change-s19-file-name/m-p/203073#M7695</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm liking the new Eclipse IDE, but wow so many options! &amp;nbsp;I can't seem to find where I can change the S19 file name output after a build. &amp;nbsp;I see the project properties (right click on the root project folder, click on Properties) dialog with its build options, but nothing specific about output file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also see the Run Configurations (go to the Run menu, click&amp;nbsp;Run Configurations). &amp;nbsp;In that tree, under the BDM_PandE_Multilink_CyclonePro branch, in the Main tab, there are options for C/C++ application. &amp;nbsp;These are by default "Project" and "Standard/Project.abs"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried changing these both to my new name, but the S19 file that is created remains "Project.s19". &amp;nbsp;Anyone?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 May 2011 21:43:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/version-10-change-s19-file-name/m-p/203073#M7695</guid>
      <dc:creator>irob</dc:creator>
      <dc:date>2011-05-03T21:43:00Z</dc:date>
    </item>
    <item>
      <title>Re: version 10, change s19 file name?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/version-10-change-s19-file-name/m-p/203074#M7696</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;if you are using in your project the Burner to create the S19 file, then have a look at the burner.bbl inside the Project_Settings/Linker_Files/burner.bbl:&lt;/P&gt;&lt;P&gt;there is&lt;/P&gt;&lt;P&gt;OPENFILE "%ABS_FILE%.s19"&lt;BR /&gt;format=motorola&lt;BR /&gt;busWidth=1&lt;BR /&gt;origin=0&lt;BR /&gt;len=0x1000000&lt;BR /&gt;destination=0&lt;BR /&gt;SRECORD=Sx&lt;BR /&gt;SENDBYTE 1 "%ABS_FILE%"&lt;BR /&gt;CLOSE&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;So you can change the OPENFILE line to whatever you like.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 May 2011 22:05:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/version-10-change-s19-file-name/m-p/203074#M7696</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2011-05-03T22:05:36Z</dc:date>
    </item>
    <item>
      <title>Re: version 10, change s19 file name?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/version-10-change-s19-file-name/m-p/203075#M7697</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, BlackNight. &amp;nbsp;I settled on manually (outside of CW10 / Eclipse) renaming the *.abs, *.args, *.map files. &amp;nbsp;I also had to update the reference to the old name in the .cproject config file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Works fine now.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 May 2011 02:47:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/version-10-change-s19-file-name/m-p/203075#M7697</guid>
      <dc:creator>irob</dc:creator>
      <dc:date>2011-05-04T02:47:19Z</dc:date>
    </item>
    <item>
      <title>Re: version 10, change s19 file name?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/version-10-change-s19-file-name/m-p/203076#M7698</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Nov 2011 05:02:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/version-10-change-s19-file-name/m-p/203076#M7698</guid>
      <dc:creator>bob_walker</dc:creator>
      <dc:date>2011-11-25T05:02:47Z</dc:date>
    </item>
    <item>
      <title>Re: version 10, change s19 file name?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/version-10-change-s19-file-name/m-p/203077#M7699</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Proper way:&lt;/P&gt;&lt;P&gt;properties-&amp;gt;C/C++ Build/Built Artifacts&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Aug 2012 00:57:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/version-10-change-s19-file-name/m-p/203077#M7699</guid>
      <dc:creator>Nik</dc:creator>
      <dc:date>2012-08-24T00:57:33Z</dc:date>
    </item>
  </channel>
</rss>