<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: License error when using command line linker in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/License-error-when-using-command-line-linker/m-p/201646#M7602</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Correction: It wasn't the environment variable. It was the license file. I used the CodeWarrior for Coldfire Architecture license file instead of the Microcontrollers one. Apparently some features necessary to compile for V1 ColdFires are only defined the V2-4 license file.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 May 2010 22:25:07 GMT</pubDate>
    <dc:creator>stbohne</dc:creator>
    <dc:date>2010-05-26T22:25:07Z</dc:date>
    <item>
      <title>License error when using command line linker</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/License-error-when-using-command-line-linker/m-p/201643#M7599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I get the following message when linking a simple c (void main() {}) file:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;### mwldmcf Driver Error:#&amp;nbsp;&amp;nbsp; License check failed: No such feature exists#&amp;nbsp;&amp;nbsp; Feature:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Win32_ColdFire_Special_512#&amp;nbsp;&amp;nbsp; License path:&amp;nbsp; C:\Programme\Freescale\CodeWarrior for Microcontrollers -#&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; V6.3\Bin\..\license.dat
#&amp;nbsp;&amp;nbsp; FLEXlm error:&amp;nbsp; -5,357#&amp;nbsp;&amp;nbsp; For further information, refer to the FLEXlm End User Manual,#&amp;nbsp;&amp;nbsp; available at "&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.macrovision.com" rel="nofollow noopener noreferrer" target="_blank"&gt;www.macrovision.com&lt;/A&gt;".Errors caused tool to abort.&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The path to the license file is correct. I can compile using mwccmcf -c, but using mwccmcf without -c causes the same message. I'm also using the same installation via CodeWarrior GUI without problems.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any ideas what I'm doing wrong?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Stefan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 May 2010 21:20:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/License-error-when-using-command-line-linker/m-p/201643#M7599</guid>
      <dc:creator>stbohne</dc:creator>
      <dc:date>2010-05-18T21:20:05Z</dc:date>
    </item>
    <item>
      <title>Re: License error when using command line linker</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/License-error-when-using-command-line-linker/m-p/201644#M7600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It would probably help if you posted the batch/make file that you are using.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 May 2010 19:55:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/License-error-when-using-command-line-linker/m-p/201644#M7600</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2010-05-19T19:55:26Z</dc:date>
    </item>
    <item>
      <title>Re: License error when using command line linker</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/License-error-when-using-command-line-linker/m-p/201645#M7601</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found the solution. I had to set the LM_LICENSE_FILE environment variable. The --use-license-file option did not help. And I only found this documented on the installation CD. The CodeWarrior help files I looked into did not mention this variable.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I should add, I'm using CodeWarrior for Microcontrollers V6.3.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 May 2010 20:58:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/License-error-when-using-command-line-linker/m-p/201645#M7601</guid>
      <dc:creator>stbohne</dc:creator>
      <dc:date>2010-05-26T20:58:49Z</dc:date>
    </item>
    <item>
      <title>Re: License error when using command line linker</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/License-error-when-using-command-line-linker/m-p/201646#M7602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Correction: It wasn't the environment variable. It was the license file. I used the CodeWarrior for Coldfire Architecture license file instead of the Microcontrollers one. Apparently some features necessary to compile for V1 ColdFires are only defined the V2-4 license file.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 May 2010 22:25:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/License-error-when-using-command-line-linker/m-p/201646#M7602</guid>
      <dc:creator>stbohne</dc:creator>
      <dc:date>2010-05-26T22:25:07Z</dc:date>
    </item>
    <item>
      <title>Re: License error when using command line linker</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/License-error-when-using-command-line-linker/m-p/201647#M7603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That sure does not sound right. I would suggest submitting a service request to see if we have a license problem. Click &lt;A href="https://www.freescale.com/webapp/servicerequest.create_SR.framework" rel="nofollow" target="_self"&gt;here&lt;/A&gt; to submit a service request.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 May 2010 19:14:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/License-error-when-using-command-line-linker/m-p/201647#M7603</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2010-05-27T19:14:37Z</dc:date>
    </item>
  </channel>
</rss>