<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックWhat does CW put into S0 record?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/What-does-CW-put-into-S0-record/m-p/128540#M759</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I would like to know what information CW puts into the S0 record in&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;.S19 files. It seems to change when the project is recompiled in a different&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;directory, but not at different times in the same directory. My goal is to&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;make it so that others can compile the project and get exactly the same .s19&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;file.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using CW for the HC12 version 3.0&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Jim&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Mar 2007 01:04:21 GMT</pubDate>
    <dc:creator>kb3kj</dc:creator>
    <dc:date>2007-03-29T01:04:21Z</dc:date>
    <item>
      <title>What does CW put into S0 record?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/What-does-CW-put-into-S0-record/m-p/128540#M759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I would like to know what information CW puts into the S0 record in&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;.S19 files. It seems to change when the project is recompiled in a different&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;directory, but not at different times in the same directory. My goal is to&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;make it so that others can compile the project and get exactly the same .s19&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;file.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using CW for the HC12 version 3.0&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Jim&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Mar 2007 01:04:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/What-does-CW-put-into-S0-record/m-p/128540#M759</guid>
      <dc:creator>kb3kj</dc:creator>
      <dc:date>2007-03-29T01:04:21Z</dc:date>
    </item>
    <item>
      <title>Re: What does CW put into S0 record?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/What-does-CW-put-into-S0-record/m-p/128541#M760</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;It's the filename of the elf file, I think.&lt;BR /&gt;&lt;BR /&gt;For srecords creates with the burner, there is an option -Ns to configure if the full path or just the filename should be written to the s0, or if no s0 should be emitted at all.&lt;BR /&gt;However I don't know if this option is already in the V3.0 version you are using. Also srecords can be generated by other tools too (assembler/linker).&lt;BR /&gt;&lt;BR /&gt;Daniel&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Mar 2007 02:38:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/What-does-CW-put-into-S0-record/m-p/128541#M760</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2007-03-29T02:38:39Z</dc:date>
    </item>
  </channel>
</rss>