<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Re-Allocate _Startup in PRM file? in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Re-Allocate-Startup-in-PRM-file/m-p/199580#M7473</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; The command VECTOR ADDRESS can be used to write a 2 byte value at a specified address.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; It is mainly used to initialize vector table entries. This is the reason the command has been called VECTOR ADDRESS.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; You can use it to relocate the vector table to another location.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Do not attempt to use the VECTOR command.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; This command&amp;nbsp;uses a vector number to determine which memory cell to initialize. It works only for the real&amp;nbsp;vector table&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; as it expect vector 0 to be at 0xFFFE.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; This command cannot be used to allocated a function at a specific address as it initialize on;y 2 bytes (the size of en entry in the vector table).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;In order to allocate a function at a specific address, place it in a user defined section and allocate the section at the desired address.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Jan 2012 14:44:17 GMT</pubDate>
    <dc:creator>CrasyCat</dc:creator>
    <dc:date>2012-01-23T14:44:17Z</dc:date>
    <item>
      <title>Re-Allocate _Startup in PRM file?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Re-Allocate-Startup-in-PRM-file/m-p/199578#M7471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using CW 4.6.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've got and application merged with bootloader using the HEXFILE instruction. Also have PRM pre-process enable, so I define a label __INCLUDE_BOOTLOADER__ to include it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When including the bootloader _Startup cannot be @0xFFFE because the bootloader reset vector is there; and it must be place @0xEFFE... So I try doing this:&lt;/P&gt;&lt;PRE&gt;#ifndef __INCLUDE_BOOTLOADER__&amp;nbsp; VECTOR ADDRESS 0xFFFE&amp;nbsp; _Startup#else&amp;nbsp; VECTOR ADDRESS 0xEFFE&amp;nbsp; _Startup#endif&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;BR /&gt;And it works.... but I've got some questions:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) First of all... Is that correct? Because I&amp;nbsp;thoguht that it will trow me and error because 0xEFFE is no a "VECTOR ADDRESS"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) And that leads me to wonder... What does&amp;nbsp;&lt;STRONG&gt;VECTOR ADDRESS&lt;/STRONG&gt;&amp;nbsp;mean or do?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;3) And finally... Can I re-locate any function to be wherever I want in .prm file? I mean, can I put&amp;nbsp;&lt;STRONG&gt;&lt;EM&gt;my_func&lt;/EM&gt;&amp;nbsp;&lt;/STRONG&gt;at address&amp;nbsp;&lt;STRONG&gt;&lt;EM&gt;0xC582&lt;/EM&gt;&lt;/STRONG&gt;&amp;nbsp;be doing:&lt;STRONG&gt;VECTOR ADDRESS&amp;nbsp;&lt;/STRONG&gt;&lt;STRONG&gt;0xC582&amp;nbsp;&lt;EM&gt;my_func&lt;/EM&gt;&lt;/STRONG&gt;?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for reading, I hope you can "feed" my&amp;nbsp;curiousity!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Jan 2012 02:52:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Re-Allocate-Startup-in-PRM-file/m-p/199578#M7471</guid>
      <dc:creator>sebasira</dc:creator>
      <dc:date>2012-01-21T02:52:08Z</dc:date>
    </item>
    <item>
      <title>Re: Re-Allocate _Startup in PRM file?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Re-Allocate-Startup-in-PRM-file/m-p/199579#M7472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sebastian,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The following is an excerpt from the Build Tools Utilities manual, and shows the VECTOR command alternatives available.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P align="left"&gt;&lt;FONT color="#0000ff"&gt;&lt;EM&gt;&lt;STRONG&gt;VECTOR Command&lt;/STRONG&gt;&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P align="left"&gt;&amp;nbsp;&lt;/P&gt;&lt;P align="left"&gt;&lt;FONT color="#0000ff"&gt;&lt;EM&gt;This command is specially defined to initialize the vector table.&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P align="left"&gt;&lt;FONT color="#0000ff"&gt;&lt;EM&gt;Use the syntax &lt;FONT face="courier new,courier" size="2"&gt;VECTOR &amp;lt;Number&amp;gt;&lt;/FONT&gt;&lt;FONT face="Times-Roman" size="1"&gt;&lt;FONT face="Times-Roman" size="1"&gt;&lt;FONT face="Times-Roman" size="1"&gt;&lt;FONT face="courier new,courier" size="2"&gt;.&lt;/FONT&gt;&amp;nbsp; &lt;FONT size="2"&gt;In this case, the linker allocates the vector&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt; depending on the target CPU.&amp;nbsp; The vector number zero is usually the reset vector, but depends on the target.&amp;nbsp; The Linker knows the default start location of the vector table for each target supported.&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P align="left"&gt;&amp;nbsp;&lt;/P&gt;&lt;P align="left"&gt;&lt;FONT color="#0000ff"&gt;&lt;EM&gt;You can use the syntax &lt;FONT face="courier new,courier" size="2"&gt;VECTOR ADDRESS&lt;/FONT&gt; &lt;FONT face="Times-Roman" size="2"&gt;&lt;FONT face="Times-Roman"&gt;&lt;FONT face="Times-Roman"&gt;as well. The size of the entries in the vector&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt; table depend on the target processor.&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P align="left"&gt;&amp;nbsp;&lt;/P&gt;&lt;P align="left"&gt;&lt;FONT color="#0000ff"&gt;&lt;EM&gt;&lt;STRONG&gt;Table 3.4 &amp;nbsp;VECTOR Command Syntax and Descriptions&lt;/STRONG&gt;&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P align="left"&gt;&lt;FONT color="#0000ff"&gt;&lt;EM&gt;&lt;FONT face="courier new,courier"&gt;VECTOR ADDRESS 0xFFFE 0x1000&lt;/FONT&gt;&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P align="left"&gt;&lt;FONT color="#0000ff"&gt;&lt;EM&gt;Indicates that the value 0x1000 must be stored at address 0xFFFE&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P align="left"&gt;&lt;FONT color="#0000ff"&gt;&lt;EM&gt;&lt;FONT face="courier new,courier"&gt;VECTOR ADDRESS 0xFFFE FName&lt;/FONT&gt;&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P align="left"&gt;&lt;FONT color="#0000ff"&gt;&lt;EM&gt;Indicates that the address of the function &lt;FONT face="courier new,courier" size="2"&gt;FName&lt;/FONT&gt; must be stored at address 0xFFFE.&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P align="left"&gt;&lt;FONT color="#0000ff"&gt;&lt;EM&gt;&lt;FONT face="courier new,courier"&gt;VECTOR ADDRESS 0xFFFE FName OFFSET 2&lt;/FONT&gt;&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P align="left"&gt;&lt;FONT color="#0000ff"&gt;&lt;EM&gt;Indicates that the address of the function &lt;FONT face="Courier" size="1"&gt;&lt;FONT face="Courier" size="1"&gt;FName,&lt;/FONT&gt;&lt;/FONT&gt;incremented by 2, must be stored at address 0xFFFE&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P align="left"&gt;&lt;FONT color="#0000ff"&gt;&lt;EM&gt;The last syntax may be very useful when working with a common interrupt service routine.&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;An alternative method for handling this situation would be to compile and link the code in the normal manner, as if the bootloader were not present.&amp;nbsp; This will generate a S19 file for the code.&amp;nbsp; Of course, the code will need to avoid using the area occupied by the bootloader, but the vectors will be at their normal location.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then, for the cases where this file is&amp;nbsp;handled by a bootloader, the bootloader itself can determine when it encounters a vector address, and automatically relocate the vector data to an alternative address location, known to itself.&amp;nbsp; This would apply whether automatic vector redirection is applicable (for other than the reset vector), or vector&amp;nbsp;redirection is via code within the bootloader.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Jan 2012 14:02:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Re-Allocate-Startup-in-PRM-file/m-p/199579#M7472</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2012-01-21T14:02:39Z</dc:date>
    </item>
    <item>
      <title>Re: Re-Allocate _Startup in PRM file?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Re-Allocate-Startup-in-PRM-file/m-p/199580#M7473</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; The command VECTOR ADDRESS can be used to write a 2 byte value at a specified address.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; It is mainly used to initialize vector table entries. This is the reason the command has been called VECTOR ADDRESS.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; You can use it to relocate the vector table to another location.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Do not attempt to use the VECTOR command.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; This command&amp;nbsp;uses a vector number to determine which memory cell to initialize. It works only for the real&amp;nbsp;vector table&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; as it expect vector 0 to be at 0xFFFE.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; This command cannot be used to allocated a function at a specific address as it initialize on;y 2 bytes (the size of en entry in the vector table).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;In order to allocate a function at a specific address, place it in a user defined section and allocate the section at the desired address.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jan 2012 14:44:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Re-Allocate-Startup-in-PRM-file/m-p/199580#M7473</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2012-01-23T14:44:17Z</dc:date>
    </item>
    <item>
      <title>Re: Re-Allocate _Startup in PRM file?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Re-Allocate-Startup-in-PRM-file/m-p/199581#M7474</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you both for clarifying that! I'll keep it in mind.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jan 2012 20:19:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Re-Allocate-Startup-in-PRM-file/m-p/199581#M7474</guid>
      <dc:creator>sebasira</dc:creator>
      <dc:date>2012-01-27T20:19:32Z</dc:date>
    </item>
    <item>
      <title>Re: Re-Allocate _Startup in PRM file?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Re-Allocate-Startup-in-PRM-file/m-p/199582#M7475</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi again crasycat!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've got a doubt about what you said. You said:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;&amp;gt;You can use it to relocate the vector table to another location.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't understand how to do that....Did you mean that I can change the vector location? I mean, let's take reset vector. It address is 0xFFFE, can I change that address so the reset vector is at, for example, 0xFF00?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How could I do that?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance, and forgive my misunderstanding&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Feb 2012 03:00:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Re-Allocate-Startup-in-PRM-file/m-p/199582#M7475</guid>
      <dc:creator>sebasira</dc:creator>
      <dc:date>2012-02-01T03:00:28Z</dc:date>
    </item>
    <item>
      <title>Re: Re-Allocate _Startup in PRM file?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Re-Allocate-Startup-in-PRM-file/m-p/199583#M7476</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What I meant here is that you can use the comamnd VECTOR ADDRESS to initialize a mirror of the vector table.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Which is what you are looking for when you are using your bootloader.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Feb 2012 18:36:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Re-Allocate-Startup-in-PRM-file/m-p/199583#M7476</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2012-02-01T18:36:26Z</dc:date>
    </item>
    <item>
      <title>Re: Re-Allocate _Startup in PRM file?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Re-Allocate-Startup-in-PRM-file/m-p/199584#M7477</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Oh, ok.... Now I understand! Thanks for your quick reply&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Feb 2012 21:07:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Re-Allocate-Startup-in-PRM-file/m-p/199584#M7477</guid>
      <dc:creator>sebasira</dc:creator>
      <dc:date>2012-02-01T21:07:28Z</dc:date>
    </item>
  </channel>
</rss>