<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic headers not found in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/headers-not-found/m-p/199359#M7462</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;using the S08JM16 for a project with CW 10.1 running on Windows 7 64 bit&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have different directories setup in the project file.&amp;nbsp; one for the application with the code in this directory.&lt;/P&gt;&lt;P&gt;a different directory for the real time monitor that I have developed and use as starting code for many projects.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;this code in in the monitor_Lib directory.&amp;nbsp; and was drag and dropped into the monitor_lib directory and option to have the code linked into the project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The headers for the different files are in the Standard CW header folder.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;the problem is that while I can select and open the header files, the compiler can not seem to find the header files.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;any suggestion&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;Jim P&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Apr 2011 05:00:34 GMT</pubDate>
    <dc:creator>Jim_P</dc:creator>
    <dc:date>2011-04-19T05:00:34Z</dc:date>
    <item>
      <title>headers not found</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/headers-not-found/m-p/199359#M7462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;using the S08JM16 for a project with CW 10.1 running on Windows 7 64 bit&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have different directories setup in the project file.&amp;nbsp; one for the application with the code in this directory.&lt;/P&gt;&lt;P&gt;a different directory for the real time monitor that I have developed and use as starting code for many projects.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;this code in in the monitor_Lib directory.&amp;nbsp; and was drag and dropped into the monitor_lib directory and option to have the code linked into the project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The headers for the different files are in the Standard CW header folder.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;the problem is that while I can select and open the header files, the compiler can not seem to find the header files.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;any suggestion&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;Jim P&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Apr 2011 05:00:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/headers-not-found/m-p/199359#M7462</guid>
      <dc:creator>Jim_P</dc:creator>
      <dc:date>2011-04-19T05:00:34Z</dc:date>
    </item>
    <item>
      <title>Re: headers not found</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/headers-not-found/m-p/199360#M7463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Did you add the path to the include files to your project?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Apr 2011 13:22:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/headers-not-found/m-p/199360#M7463</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2011-04-19T13:22:10Z</dc:date>
    </item>
  </channel>
</rss>