<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: Pushbutton switch stimulation using the special edition version</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Pushbutton-switch-stimulation-using-the-special-edition-version/m-p/196095#M7244</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Special edition only limits the number of instruments you can add in a visualization tool window.&lt;/P&gt;&lt;P&gt;It does not limit the functionality&amp;nbsp;of the instruments.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I did try on a simple project&amp;nbsp;and I can toggle a bit on POTA through a Switch Instrument.&lt;/P&gt;&lt;P&gt;Did you initialize the port direction register appropriately to allow input on that bit?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As you did not specify which version of CodeWarrior you are using I assumed you are using CodeWarrior for MCU V6.2.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Jul 2009 20:16:48 GMT</pubDate>
    <dc:creator>CrasyCat</dc:creator>
    <dc:date>2009-07-09T20:16:48Z</dc:date>
    <item>
      <title>Pushbutton switch stimulation using the special edition version</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Pushbutton-switch-stimulation-using-the-special-edition-version/m-p/196093#M7242</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Just want to confirm that the special edition does not allow&amp;nbsp;stimulation of a pushbutton or any switch connected to an I\O port.&amp;nbsp; I can toggle an LED using the graphical tools, but not a switch input.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a way to stimulate an input using the special edition version?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;FC&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jul 2009 06:05:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Pushbutton-switch-stimulation-using-the-special-edition-version/m-p/196093#M7242</guid>
      <dc:creator>FC</dc:creator>
      <dc:date>2009-07-03T06:05:27Z</dc:date>
    </item>
    <item>
      <title>Re: Pushbutton switch stimulation using the special edition version</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Pushbutton-switch-stimulation-using-the-special-edition-version/m-p/196094#M7243</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello again,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have the read the posts similiar to this topic, but they discuss simulating KBI interrupts.&amp;nbsp; For a polling application, can a switch component change the input value on a pin?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Jul 2009 02:34:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Pushbutton-switch-stimulation-using-the-special-edition-version/m-p/196094#M7243</guid>
      <dc:creator>FC</dc:creator>
      <dc:date>2009-07-04T02:34:54Z</dc:date>
    </item>
    <item>
      <title>Re: Pushbutton switch stimulation using the special edition version</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Pushbutton-switch-stimulation-using-the-special-edition-version/m-p/196095#M7244</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Special edition only limits the number of instruments you can add in a visualization tool window.&lt;/P&gt;&lt;P&gt;It does not limit the functionality&amp;nbsp;of the instruments.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I did try on a simple project&amp;nbsp;and I can toggle a bit on POTA through a Switch Instrument.&lt;/P&gt;&lt;P&gt;Did you initialize the port direction register appropriately to allow input on that bit?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As you did not specify which version of CodeWarrior you are using I assumed you are using CodeWarrior for MCU V6.2.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jul 2009 20:16:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Pushbutton-switch-stimulation-using-the-special-edition-version/m-p/196095#M7244</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2009-07-09T20:16:48Z</dc:date>
    </item>
  </channel>
</rss>