<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Re: Code Warrior for 8/ 16 bit</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Code-Warrior-for-8-16-bit/m-p/194483#M7125</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks it is much more clear to me now.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In order to create a project for an object library:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; - Create your project as usual using the wizard&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; -&amp;nbsp; Open the &lt;EM&gt;&lt;STRONG&gt;Target Settings&lt;/STRONG&gt;&lt;/EM&gt; dialog (Press ALT + F7)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; - In the &lt;STRONG&gt;&lt;EM&gt;Target&lt;/EM&gt;&lt;/STRONG&gt; -&amp;gt; &lt;EM&gt;&lt;STRONG&gt;Target Settings&lt;/STRONG&gt;&lt;/EM&gt; panel change Linker to &lt;EM&gt;&lt;STRONG&gt;Libmaker for HC12&lt;/STRONG&gt;&lt;/EM&gt; or &lt;STRONG&gt;&lt;EM&gt;Libmaker for HC08&lt;/EM&gt;&lt;/STRONG&gt; (depending on the processor you are targeting).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; - You will see a new panel &lt;STRONG&gt;&lt;EM&gt;Libmaker for HC12&lt;/EM&gt;&lt;/STRONG&gt; or &lt;STRONG&gt;&lt;EM&gt;Libmaker for HC08&lt;/EM&gt;&lt;/STRONG&gt; (according to the target), where you can adjust name of the library you want to create.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If your library is MCU independent, you can remove the MCU related .c and ,h file from your project. Just select the corresponding file names and click DELETE key.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Apr 2010 21:29:38 GMT</pubDate>
    <dc:creator>CrasyCat</dc:creator>
    <dc:date>2010-04-22T21:29:38Z</dc:date>
    <item>
      <title>Code Warrior for 8/ 16 bit</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Code-Warrior-for-8-16-bit/m-p/194480#M7122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;how to&amp;nbsp;generate the *.lib &amp;nbsp;file&amp;nbsp;from the original .c /.h file using specific setting done in the code warrior suite..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Apr 2010 16:39:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Code-Warrior-for-8-16-bit/m-p/194480#M7122</guid>
      <dc:creator>RohitSinghal</dc:creator>
      <dc:date>2010-04-22T16:39:07Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior for 8/ 16 bit</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Code-Warrior-for-8-16-bit/m-p/194481#M7123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Not sure I understand the question here.&lt;/P&gt;&lt;P&gt;Are you asking how you can rebuild the ANSI library after changing some compilation option?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If this is the question, there is a .mcp file in the {Install}\lib\hc08c or&amp;nbsp;&amp;nbsp;{Install}\lib\hc12c that can be loaded in CodeWarrior to rebuild the libraries.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Apr 2010 19:44:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Code-Warrior-for-8-16-bit/m-p/194481#M7123</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2010-04-22T19:44:58Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior for 8/ 16 bit</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Code-Warrior-for-8-16-bit/m-p/194482#M7124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;To make my question&amp;nbsp;more simple, In one of the project customer asked us to&amp;nbsp;develop of specific algo&amp;nbsp;related to their&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;application.&amp;nbsp; In order to&amp;nbsp;protect the algo&amp;nbsp;i want to covert this file in .lib format &amp;amp;&amp;nbsp;provide to customer with some known&amp;nbsp;API&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;defination&amp;nbsp;so that&amp;nbsp;further can&amp;nbsp;be used for&amp;nbsp;development purpose without disclosing the background code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope it will be much clear situation.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Apr 2010 20:01:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Code-Warrior-for-8-16-bit/m-p/194482#M7124</guid>
      <dc:creator>RohitSinghal</dc:creator>
      <dc:date>2010-04-22T20:01:17Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior for 8/ 16 bit</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Code-Warrior-for-8-16-bit/m-p/194483#M7125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks it is much more clear to me now.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In order to create a project for an object library:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; - Create your project as usual using the wizard&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; -&amp;nbsp; Open the &lt;EM&gt;&lt;STRONG&gt;Target Settings&lt;/STRONG&gt;&lt;/EM&gt; dialog (Press ALT + F7)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; - In the &lt;STRONG&gt;&lt;EM&gt;Target&lt;/EM&gt;&lt;/STRONG&gt; -&amp;gt; &lt;EM&gt;&lt;STRONG&gt;Target Settings&lt;/STRONG&gt;&lt;/EM&gt; panel change Linker to &lt;EM&gt;&lt;STRONG&gt;Libmaker for HC12&lt;/STRONG&gt;&lt;/EM&gt; or &lt;STRONG&gt;&lt;EM&gt;Libmaker for HC08&lt;/EM&gt;&lt;/STRONG&gt; (depending on the processor you are targeting).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; - You will see a new panel &lt;STRONG&gt;&lt;EM&gt;Libmaker for HC12&lt;/EM&gt;&lt;/STRONG&gt; or &lt;STRONG&gt;&lt;EM&gt;Libmaker for HC08&lt;/EM&gt;&lt;/STRONG&gt; (according to the target), where you can adjust name of the library you want to create.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If your library is MCU independent, you can remove the MCU related .c and ,h file from your project. Just select the corresponding file names and click DELETE key.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Apr 2010 21:29:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Code-Warrior-for-8-16-bit/m-p/194483#M7125</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2010-04-22T21:29:38Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior for 8/ 16 bit</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Code-Warrior-for-8-16-bit/m-p/194484#M7126</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your&amp;nbsp;wonderful support..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It works as i required to send the info.. to my customer..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Warm Regards,&lt;/P&gt;&lt;P&gt;Rohit&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Apr 2010 21:35:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Code-Warrior-for-8-16-bit/m-p/194484#M7126</guid>
      <dc:creator>RohitSinghal</dc:creator>
      <dc:date>2010-04-22T21:35:59Z</dc:date>
    </item>
  </channel>
</rss>