<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: Debuger code limit during evaluation intentional?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Debuger-code-limit-during-evaluation-intentional/m-p/193499#M7034</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The Special edition of CW for MCUs has a code limit of 64K. The evaluation version should not have a limit. It's sounds like something else might have been installed by accident or was left over from a previous installation. Did you install this over an old CW installation?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Apr 2010 19:23:34 GMT</pubDate>
    <dc:creator>J2MEJediMaster</dc:creator>
    <dc:date>2010-04-21T19:23:34Z</dc:date>
    <item>
      <title>Debuger code limit during evaluation intentional?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Debuger-code-limit-during-evaluation-intentional/m-p/193498#M7033</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I installed the CW 6.3 evaluation version to compile the MQX examples for the Tower system.&lt;/P&gt;&lt;P&gt;The compilation works fine and I can link and flash e.g. the 110k file for the "security webserver" demo without any problems.&lt;/P&gt;&lt;P&gt;However the debugger, after flashing the file, will immediately complain that it is running in demo mode and thus wont load source/symbol files any greater than 64k.&lt;/P&gt;&lt;P&gt;So, I can flash and run the programs but I can not step through them with the debugger. Kinda odd, is this intentional? I also noticed, in the license.dat file, there is a product code "HI409285" for the 30 day eval license, whereas the debugger is complaining about not finding a valid license for "HI409284" (notice the last digit).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;Sven&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Apr 2010 22:49:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Debuger-code-limit-during-evaluation-intentional/m-p/193498#M7033</guid>
      <dc:creator>Kopone</dc:creator>
      <dc:date>2010-04-20T22:49:22Z</dc:date>
    </item>
    <item>
      <title>Re: Debuger code limit during evaluation intentional?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Debuger-code-limit-during-evaluation-intentional/m-p/193499#M7034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The Special edition of CW for MCUs has a code limit of 64K. The evaluation version should not have a limit. It's sounds like something else might have been installed by accident or was left over from a previous installation. Did you install this over an old CW installation?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Apr 2010 19:23:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Debuger-code-limit-during-evaluation-intentional/m-p/193499#M7034</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2010-04-21T19:23:34Z</dc:date>
    </item>
    <item>
      <title>Re: Debuger code limit during evaluation intentional?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Debuger-code-limit-during-evaluation-intentional/m-p/193500#M7035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ah, yeah, I also got a (daily use) 6.2 SE installation sitting on my harddisk. The two seem to happily coexist, so I guess the debugger issue is a mere side-effect of this. I meanwhile requested a test period extension license and with that one the debugger works. Turns out we gotta upgrade to the 5225x for our current project, so thanks anyways (and blame on me I didnt mention the 6.2 installation right away &lt;IMG alt=":manhappy:" class="emoticon emoticon-manhappy" id="manhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_man-happy.gif" title="Man Happy" /&gt; )&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;Sven&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Apr 2010 20:10:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Debuger-code-limit-during-evaluation-intentional/m-p/193500#M7035</guid>
      <dc:creator>Kopone</dc:creator>
      <dc:date>2010-04-21T20:10:12Z</dc:date>
    </item>
  </channel>
</rss>