<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: Programming fuses in CW 10.2</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Programming-fuses-in-CW-10-2/m-p/192632#M6965</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;the easiest way to protect the flash is to have a S19 file (S-Record) which has the protection bytes in it programmed.&lt;/P&gt;&lt;P&gt;You might consider to merge two S19 files (one with the application, and one with just the protection bytes in it) using the burner utility (prog\burner.exe).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As for standalone flash programming: have a look at this post:&lt;/P&gt;&lt;P&gt;&lt;A href="https://mcuoneclipse.wordpress.com/2012/08/02/standalone-flash-programmer/" rel="nofollow" target="_blank"&gt;https://mcuoneclipse.wordpress.com/2012/08/02/standalone-flash-programmer/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;About doing protection with a CodeWarrior target task: that depends on the CPU you are using, but I know that CW MCU 10.3 (which comes out soon) has extended capabilities and supports more devices to protect/unprotect.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;BK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Aug 2012 02:45:47 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2012-08-30T02:45:47Z</dc:date>
    <item>
      <title>Programming fuses in CW 10.2</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Programming-fuses-in-CW-10-2/m-p/192631#M6964</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm not having much luck here.&amp;nbsp; I am using CW 10.2 and the PE Micro USB based programmer called the USB Multilink Interface.&amp;nbsp; It's worked fine for testing but now I want to flash units to leave the building and I want to protect the code against modification and from being read out of the device.&amp;nbsp; I can't find a way to do this and this programmer has no standalone app.&amp;nbsp; Maybe there is some third party app out there.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have searched this forum and found a good way to flash the main code into boards quickly and without having to rebuild every time by starting the debugger, but won't protect the flash.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can I do this?&amp;nbsp; Do I need to hand modify my S19 file to include the registers or is there an easier way?&amp;nbsp; If I did modify the .S19 file, would code warrior even send those protection settings anyway?&amp;nbsp; Do I have no choice but to buy a more expensive programmer?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Aug 2012 00:59:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Programming-fuses-in-CW-10-2/m-p/192631#M6964</guid>
      <dc:creator>MJWeston</dc:creator>
      <dc:date>2012-08-30T00:59:27Z</dc:date>
    </item>
    <item>
      <title>Re: Programming fuses in CW 10.2</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Programming-fuses-in-CW-10-2/m-p/192632#M6965</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;the easiest way to protect the flash is to have a S19 file (S-Record) which has the protection bytes in it programmed.&lt;/P&gt;&lt;P&gt;You might consider to merge two S19 files (one with the application, and one with just the protection bytes in it) using the burner utility (prog\burner.exe).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As for standalone flash programming: have a look at this post:&lt;/P&gt;&lt;P&gt;&lt;A href="https://mcuoneclipse.wordpress.com/2012/08/02/standalone-flash-programmer/" rel="nofollow" target="_blank"&gt;https://mcuoneclipse.wordpress.com/2012/08/02/standalone-flash-programmer/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;About doing protection with a CodeWarrior target task: that depends on the CPU you are using, but I know that CW MCU 10.3 (which comes out soon) has extended capabilities and supports more devices to protect/unprotect.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;BK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Aug 2012 02:45:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Programming-fuses-in-CW-10-2/m-p/192632#M6965</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2012-08-30T02:45:47Z</dc:date>
    </item>
    <item>
      <title>Re: Programming fuses in CW 10.2</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Programming-fuses-in-CW-10-2/m-p/192633#M6966</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks BlackNight.&amp;nbsp; I will see what I can figure out.&amp;nbsp; We may just pick up a Cyclone programmer and do it that way but at least there might be some options here.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Aug 2012 02:21:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Programming-fuses-in-CW-10-2/m-p/192633#M6966</guid>
      <dc:creator>MJWeston</dc:creator>
      <dc:date>2012-08-31T02:21:30Z</dc:date>
    </item>
  </channel>
</rss>