<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: vista update for codewarrior v4.5</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188463#M6659</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;dashz84,&lt;BR /&gt;&lt;BR /&gt;I assume you are using a purchased CodeWarrior Edition (Compiler update, Standard, Professional...). What you can do is to copy your original license file from the CodeWarrior for HC12 v4.5 directory (usually located here:"c:\Program Files\Freescale\CW for HC12 V4.5\license.dat" ) to the newly installed CodeWarior V4.7 home directory. Perhaps you could backup the v4.7 license.dat file (Special or Evaluation license) since it might be useful - e.g. you can rename it to license.bak.&lt;BR /&gt;&lt;BR /&gt;See the CrasyCat post in case you are using FREE Special edition.&lt;BR /&gt;&lt;BR /&gt;Stanish.&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Sep 2008 17:25:50 GMT</pubDate>
    <dc:creator>stanish</dc:creator>
    <dc:date>2008-09-29T17:25:50Z</dc:date>
    <item>
      <title>vista update for codewarrior v4.5</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188455#M6651</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;i'm using codewarrior dev. studio v4.5, and i'm running it on windows vista.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;during installation, while the program was trying to install the debugger, there was an error that read soemthing like " Failed to install the INF file, (C:\windows\inf\windrvr6.inf).....". I simply continued with the error anyway, because I was told that the error was due to code warrior's incompatibility to vista, a problem which is fixed by update v4.7.1.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I downloaded the update, however, the update asks for v4.7 which i do not have and cannot have.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;here are my questions&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1. Is codewarrior now compatible with vista or not?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2. if so, do i have the rigth update patch (i.e. v.4.7.1)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3. if the update patch is correct, how do use it on a v4.5?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks a bunch&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2008 04:40:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188455#M6651</guid>
      <dc:creator>dashz84</dc:creator>
      <dc:date>2008-09-26T04:40:19Z</dc:date>
    </item>
    <item>
      <title>Re: vista update for codewarrior v4.5</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188456#M6652</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;oh, by the way,&lt;BR /&gt;&lt;BR /&gt;this is for HCS12(X) microcontrollers&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2008 04:42:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188456#M6652</guid>
      <dc:creator>dashz84</dc:creator>
      <dc:date>2008-09-26T04:42:04Z</dc:date>
    </item>
    <item>
      <title>Re: vista update for codewarrior v4.5</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188457#M6653</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;Hello dashz84,&lt;BR /&gt;&lt;BR /&gt;1. As far as I know v4.5 may not running correctly under Windows Vista.&lt;BR /&gt;Recent release v4.7 should be compatible with Vista, see attached Vista release notes.&lt;BR /&gt;&lt;BR /&gt;2. Patch v4.7.1 doesn't cover Vista Compatibility but fixes several compiler/linker/debugger defects.&lt;BR /&gt;&lt;BR /&gt;3. I'm not aware of any patch for V4.5 that would cover Vista compatibility&lt;BR /&gt;&lt;BR /&gt;Note:&lt;BR /&gt;There is a way how to install CW V4.6 on Windows Vista by deselecting P&amp;amp;E drivers. See attached .pdf&lt;BR /&gt;I'm not sure whether it's applicable also to V4.5 since I didn't test it.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;Stanish&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/files/community_files/CW816COMM/Notes_CW_HC12_Vista1.txt" rel="nofollow" target="_self"&gt;Notes_CW_HC12_Vista1.txt&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/files/community_files/CW816COMM/CWHC12V46_Vista_Installation1.pdf" rel="nofollow" target="_self"&gt;CWHC12V46_Vista_Installation1.pdf&lt;/A&gt;&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by t.dowe on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-08-31&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;03:50 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2008 15:34:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188457#M6653</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2008-09-26T15:34:24Z</dc:date>
    </item>
    <item>
      <title>Re: vista update for codewarrior v4.5</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188458#M6654</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Stanish, thanks for the reply.&lt;BR /&gt;&lt;BR /&gt;my institution currently owns only a copy of codewarrior v4.5, to get v4.7, do I just need to upgrade it or do I have to have a new installation?&lt;BR /&gt;If I need to have a new installation, where and how do I obtain a copy of the installation CD?&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2008 21:39:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188458#M6654</guid>
      <dc:creator>dashz84</dc:creator>
      <dc:date>2008-09-26T21:39:42Z</dc:date>
    </item>
    <item>
      <title>Re: vista update for codewarrior v4.5</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188459#M6655</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;dashz84,&lt;BR /&gt;&lt;BR /&gt;You will need the new instalation. The CodeWarrior for HC12 v4.7 installer is available e.g. here:&lt;BR /&gt;&amp;nbsp;&lt;A href="https://www.freescale.com/webapp/Download?colCode=CWX-H12-PROED-EX&amp;amp;prodCode=CW-HCS12X&amp;amp;location=null&amp;amp;fpsp=1" rel="nofollow" target="_blank"&gt;https://www.freescale.com/webapp/Download?colCode=CWX-H12-PROED-EX&amp;amp;prodCode=CW-HCS12X&amp;amp;location=null&amp;amp;fpsp=1&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Just copy&amp;amp;paste the your license from V4.5 into CodeWarrior v4.7 home directory (e.g. "c:\Program Files\Freescale\CodeWarrior for HCS12 V4.7\license.dat"&amp;nbsp; )&lt;BR /&gt;&lt;BR /&gt;I'd recommend you also install the update (v4.7.1) since it fixes several defects. Here is the link:&lt;BR /&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-HCS12X&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab#" rel="nofollow" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-HCS12X&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab#&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Stanish&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2008 22:27:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188459#M6655</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2008-09-26T22:27:56Z</dc:date>
    </item>
    <item>
      <title>Re: vista update for codewarrior v4.5</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188460#M6656</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;thanks stanish,&lt;BR /&gt;&lt;BR /&gt;I will give that a try&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2008 22:49:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188460#M6656</guid>
      <dc:creator>dashz84</dc:creator>
      <dc:date>2008-09-26T22:49:31Z</dc:date>
    </item>
    <item>
      <title>Re: vista update for codewarrior v4.5</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188461#M6657</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi stanish,&lt;BR /&gt;&lt;BR /&gt;I double checked the installation CD box for codewarrior, and none of the 3 numbers on the back, LOT#, Date Code, and PN is the correct license key.&lt;BR /&gt;I also noticed that this is a Codewarrior dev. Studio Special Edition, do I have to email freescale for a license key or am I just missing something?&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2008 22:59:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188461#M6657</guid>
      <dc:creator>dashz84</dc:creator>
      <dc:date>2008-09-26T22:59:14Z</dc:date>
    </item>
    <item>
      <title>Re: vista update for codewarrior v4.5</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188462#M6658</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If you are installing a special edition for CodeWarrior HC12 V4.7, the special edition license file is part of&amp;nbsp;the installed layout.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The installation script will automatically install a special edition license in your CodeWarrior root installation directory.&lt;/DIV&gt;&lt;DIV&gt;There is no need to contact Freescale licensing to ask for a new license file.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;CrasyCat&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Sep 2008 16:22:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188462#M6658</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2008-09-29T16:22:42Z</dc:date>
    </item>
    <item>
      <title>Re: vista update for codewarrior v4.5</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188463#M6659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;dashz84,&lt;BR /&gt;&lt;BR /&gt;I assume you are using a purchased CodeWarrior Edition (Compiler update, Standard, Professional...). What you can do is to copy your original license file from the CodeWarrior for HC12 v4.5 directory (usually located here:"c:\Program Files\Freescale\CW for HC12 V4.5\license.dat" ) to the newly installed CodeWarior V4.7 home directory. Perhaps you could backup the v4.7 license.dat file (Special or Evaluation license) since it might be useful - e.g. you can rename it to license.bak.&lt;BR /&gt;&lt;BR /&gt;See the CrasyCat post in case you are using FREE Special edition.&lt;BR /&gt;&lt;BR /&gt;Stanish.&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Sep 2008 17:25:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188463#M6659</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2008-09-29T17:25:50Z</dc:date>
    </item>
    <item>
      <title>Re: vista update for codewarrior v4.5</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188464#M6660</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks for the replies guys, truly appreciate it!&lt;BR /&gt;&lt;BR /&gt;I have followed ur suggestions, and installed CW evaluation version 4.7, updated it with 4.7.1 patch.&lt;BR /&gt;&lt;BR /&gt;After starting the software with a new project made, I conected the programmer and the microcontroller, and under P&amp;amp;E multilink CyclonePro, I clicked on the Debug button. However, I received 2 errors.&lt;BR /&gt;Error 1: No file with extension prm found in project&lt;BR /&gt;Error 2: Link failed.&lt;BR /&gt;&lt;BR /&gt;I tried this a few times, always get the same error and can not enter the debugger. Indeed, I noticed that I do not have a required .prm file in the PRM folder, e.g (project1.prm, where project1 is the name of my new project)&lt;BR /&gt;&lt;BR /&gt;The weirdest thing though, I now restart CW4.5, and create a new project. Just like 4.7, there is no .prm file in the PRM folder. I try my luck with the Debugger in the P&amp;amp;E cyclonepro mode. The first time i click it, I get an error saying&lt;BR /&gt;Error starting external debugger. Processor Error Code 87 (0x57)&lt;BR /&gt;The parameter is incorrect.&lt;BR /&gt;However, I now see the project1.prm file under the PRM folder.&lt;BR /&gt;&lt;BR /&gt;I am able to run the new project (which was made in 4.5) in 4.7, and enter the debugger. Can you please expalin to me why I received the 2 erros in 4.7 when I tried to use the debugger? Also, will it affect me as i write more programs and debug it, if I make the .prm file in 4.5, and then use it in 4.7?&lt;BR /&gt;&lt;BR /&gt;Thanks verr much&lt;BR /&gt;&lt;BR /&gt;by the way, when I make the project, I selected Processor Expert, then PC-lint, then minimal startup, and none floating, and full chip+P&amp;amp;E simulation&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Sep 2008 23:25:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188464#M6660</guid>
      <dc:creator>dashz84</dc:creator>
      <dc:date>2008-09-29T23:25:17Z</dc:date>
    </item>
    <item>
      <title>Re: vista update for codewarrior v4.5</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188465#M6661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;It should create a prm file with CW 4.7 too, note though that with Processor expert the prm file is generated as part of the processor expert code generation, and not during the initial project creation. Therefore you only see the prm once you did build.&lt;BR /&gt;&lt;BR /&gt;I tried shortly with XP, and Processor Export did create the prm for me. Note that the prm file is located in the CODE folder on disk and in "Project Settings"/"Linker Files" in the Files views (and not in the prm folder).&lt;BR /&gt;&lt;BR /&gt;With 4.5, I think the error about not being able to start the external debugger is a known vista incompatibility which has been fixed in V4.7.&lt;BR /&gt;&lt;BR /&gt;Daniel&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Sep 2008 07:44:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/vista-update-for-codewarrior-v4-5/m-p/188465#M6661</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2008-09-30T07:44:11Z</dc:date>
    </item>
  </channel>
</rss>