<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックHello, I'm using Codewarrior for HCS 12 V4.6 with an Inda...</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Hello-I-m-using-Codewarrior-for-HCS-12-V4-6-with-an-Inda/m-p/188121#M6646</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;I'm using Codewarrior for HCS 12 V4.6 with an Indart One programmer/debugger, and I&lt;BR /&gt;can't find a solution to preserve a flash block data (1&amp;nbsp;block of 512 bytes) when I program&lt;BR /&gt;the MCU. This block is used to save informations (serial, date, ...) and these informations should not change on an application update.&lt;BR /&gt;Is it possible to specify a memory block into flash which it will not affected by code programmation ?&lt;/DIV&gt;&lt;DIV&gt;Thanks, best regards.&lt;/DIV&gt;&lt;DIV&gt;pm&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Sep 2008 00:15:24 GMT</pubDate>
    <dc:creator>pmag</dc:creator>
    <dc:date>2008-09-25T00:15:24Z</dc:date>
    <item>
      <title>Hello, I'm using Codewarrior for HCS 12 V4.6 with an Inda...</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Hello-I-m-using-Codewarrior-for-HCS-12-V4-6-with-an-Inda/m-p/188121#M6646</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;I'm using Codewarrior for HCS 12 V4.6 with an Indart One programmer/debugger, and I&lt;BR /&gt;can't find a solution to preserve a flash block data (1&amp;nbsp;block of 512 bytes) when I program&lt;BR /&gt;the MCU. This block is used to save informations (serial, date, ...) and these informations should not change on an application update.&lt;BR /&gt;Is it possible to specify a memory block into flash which it will not affected by code programmation ?&lt;/DIV&gt;&lt;DIV&gt;Thanks, best regards.&lt;/DIV&gt;&lt;DIV&gt;pm&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Sep 2008 00:15:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Hello-I-m-using-Codewarrior-for-HCS-12-V4-6-with-an-Inda/m-p/188121#M6646</guid>
      <dc:creator>pmag</dc:creator>
      <dc:date>2008-09-25T00:15:24Z</dc:date>
    </item>
    <item>
      <title>Re: Hello, I'm using Codewarrior for HCS 12 V4.6 with an Inda...</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Hello-I-m-using-Codewarrior-for-HCS-12-V4-6-with-an-Inda/m-p/188122#M6647</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hello pmag,&lt;BR /&gt;&lt;BR /&gt;You can specify memory modules that you don't want to erase automatically before programming.&lt;BR /&gt;Debugger menu -&amp;gt; File -&amp;gt; Configuration -&amp;gt; Load tab -&amp;gt; "Advanced..." button.&lt;BR /&gt;Unfortunately you can not specify individual sectors of Flash but pre-defined modules.&lt;BR /&gt;I'd suggest you to use EEPROM for saving this kind of information&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Stanish&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Sep 2008 16:22:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Hello-I-m-using-Codewarrior-for-HCS-12-V4-6-with-an-Inda/m-p/188122#M6647</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2008-09-25T16:22:29Z</dc:date>
    </item>
  </channel>
</rss>