<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックCW 10.2 - Standalone flash programmer inoperable</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-2-Standalone-flash-programmer-inoperable/m-p/186741#M6509</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I must be doing something wrong, since I can't imagine there's anything wrong with the tool...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to use the standalone flash programming feature in CW 10.2 for MCU to program a K70 Tower board using OSJTAG.&amp;nbsp; This is primarily to support a customer so they can do flash updates of their prototype in the field, without us having to reprogram their board for them.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, when I try to "Erase and Program", I immediately get a java.lang.NullPointerException.&amp;nbsp; I've tried it two different ways:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) Create a new bareboard project for Kinetis K70 120MHz, FN1M0, default options, lightning bolt / Flash File to Target, select internal flash target, select S19 file to program, click Erase and Program.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) Use existing MQX-based project, lightning bolt / Flash File to Target, select internal flash target, select S19 file to program, click Erase and Program.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Either way I try it, I get "An internal error occurred during: "Executing task K70FN1M0". java.lang.NullPointerException".&amp;nbsp; I need to be able to provide our customer with a means of programming an S19 image to one of his boards using the OSJTAG port on the Tower Kit board.&amp;nbsp; This appears to be the only way to do it, since Googling hasn't turned up a free standalone software programming tool.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, what am I doing wrong here?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Aug 2012 02:07:29 GMT</pubDate>
    <dc:creator>dmarks_ls</dc:creator>
    <dc:date>2012-08-08T02:07:29Z</dc:date>
    <item>
      <title>CW 10.2 - Standalone flash programmer inoperable</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-2-Standalone-flash-programmer-inoperable/m-p/186741#M6509</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I must be doing something wrong, since I can't imagine there's anything wrong with the tool...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to use the standalone flash programming feature in CW 10.2 for MCU to program a K70 Tower board using OSJTAG.&amp;nbsp; This is primarily to support a customer so they can do flash updates of their prototype in the field, without us having to reprogram their board for them.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, when I try to "Erase and Program", I immediately get a java.lang.NullPointerException.&amp;nbsp; I've tried it two different ways:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) Create a new bareboard project for Kinetis K70 120MHz, FN1M0, default options, lightning bolt / Flash File to Target, select internal flash target, select S19 file to program, click Erase and Program.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) Use existing MQX-based project, lightning bolt / Flash File to Target, select internal flash target, select S19 file to program, click Erase and Program.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Either way I try it, I get "An internal error occurred during: "Executing task K70FN1M0". java.lang.NullPointerException".&amp;nbsp; I need to be able to provide our customer with a means of programming an S19 image to one of his boards using the OSJTAG port on the Tower Kit board.&amp;nbsp; This appears to be the only way to do it, since Googling hasn't turned up a free standalone software programming tool.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, what am I doing wrong here?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Aug 2012 02:07:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-2-Standalone-flash-programmer-inoperable/m-p/186741#M6509</guid>
      <dc:creator>dmarks_ls</dc:creator>
      <dc:date>2012-08-08T02:07:29Z</dc:date>
    </item>
    <item>
      <title>Re: CW 10.2 - Standalone flash programmer inoperable</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-2-Standalone-flash-programmer-inoperable/m-p/186742#M6510</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Open Freescale support request&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Sep 2012 18:07:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-2-Standalone-flash-programmer-inoperable/m-p/186742#M6510</guid>
      <dc:creator>evgenik</dc:creator>
      <dc:date>2012-09-20T18:07:36Z</dc:date>
    </item>
  </channel>
</rss>