<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: Color coding dosen't work on one INCLUDE file</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Color-coding-dosen-t-work-on-one-INCLUDE-file/m-p/186202#M6473</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Which processor are you targeting?&lt;BR /&gt;Which extension do you use for the assembly include files?&lt;BR /&gt;Which version are you using (5.9 is the ide version, not the product version).&lt;BR /&gt;&lt;BR /&gt;In order to get target specific coloring, make sure you add the assembly include files to the project and to&lt;BR /&gt;map the extension to the right coloring setup.&lt;BR /&gt;Especially extensions like *.asm, *.s, *,inc, *.h, *.c are colored in a generic fashion unless the file is part of a project, in which case the project settings do usually cause it to be colored target dependent.&lt;BR /&gt;&lt;BR /&gt;Daniel&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Sep 2008 01:08:00 GMT</pubDate>
    <dc:creator>CompilerGuru</dc:creator>
    <dc:date>2008-09-17T01:08:00Z</dc:date>
    <item>
      <title>Color coding dosen't work on one INCLUDE file</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Color-coding-dosen-t-work-on-one-INCLUDE-file/m-p/186201#M6472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I'm having a problem with CodeWarrior version 5.90. The color coding is intermittent on one of my include files. The program is written in relocatable Assembly.&amp;nbsp;The code assembles without errors or warnings and the include file&amp;nbsp;appears in the listing file.&amp;nbsp;It also executes in the software simulator. If&amp;nbsp;I make changes to the include file in question, some times the color coding works, than stops working.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Any ideas?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Don O&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Sep 2008 00:46:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Color-coding-dosen-t-work-on-one-INCLUDE-file/m-p/186201#M6472</guid>
      <dc:creator>FreeRadical</dc:creator>
      <dc:date>2008-09-17T00:46:47Z</dc:date>
    </item>
    <item>
      <title>Re: Color coding dosen't work on one INCLUDE file</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Color-coding-dosen-t-work-on-one-INCLUDE-file/m-p/186202#M6473</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Which processor are you targeting?&lt;BR /&gt;Which extension do you use for the assembly include files?&lt;BR /&gt;Which version are you using (5.9 is the ide version, not the product version).&lt;BR /&gt;&lt;BR /&gt;In order to get target specific coloring, make sure you add the assembly include files to the project and to&lt;BR /&gt;map the extension to the right coloring setup.&lt;BR /&gt;Especially extensions like *.asm, *.s, *,inc, *.h, *.c are colored in a generic fashion unless the file is part of a project, in which case the project settings do usually cause it to be colored target dependent.&lt;BR /&gt;&lt;BR /&gt;Daniel&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Sep 2008 01:08:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Color-coding-dosen-t-work-on-one-INCLUDE-file/m-p/186202#M6473</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2008-09-17T01:08:00Z</dc:date>
    </item>
  </channel>
</rss>