<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 CW08 V5.0 HC08 chipset</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW08-V5-0-HC08-chipset/m-p/127967#M624</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi.&amp;nbsp; I'm still fairly new to using Codewarrior and I'm trying to use the "SetStopMode" function for the MC68HC908QY4 chip, but for some reason it's "greyed out".&amp;nbsp; I can't seem to activate this function and was wondering if there's anything special I need to set in order to be able to use this function.&amp;nbsp; Could it be the possibility that I'm currently using the Special Edition license and need to upgrade to Standard or Pro?&amp;nbsp; and if that's the case, then which version do I need?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks &lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif"&gt;&lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/A&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 04 Mar 2006 07:12:21 GMT</pubDate>
    <dc:creator>Jerry</dc:creator>
    <dc:date>2006-03-04T07:12:21Z</dc:date>
    <item>
      <title>CW08 V5.0 HC08 chipset</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW08-V5-0-HC08-chipset/m-p/127967#M624</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi.&amp;nbsp; I'm still fairly new to using Codewarrior and I'm trying to use the "SetStopMode" function for the MC68HC908QY4 chip, but for some reason it's "greyed out".&amp;nbsp; I can't seem to activate this function and was wondering if there's anything special I need to set in order to be able to use this function.&amp;nbsp; Could it be the possibility that I'm currently using the Special Edition license and need to upgrade to Standard or Pro?&amp;nbsp; and if that's the case, then which version do I need?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks &lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif"&gt;&lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/A&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Mar 2006 07:12:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW08-V5-0-HC08-chipset/m-p/127967#M624</guid>
      <dc:creator>Jerry</dc:creator>
      <dc:date>2006-03-04T07:12:21Z</dc:date>
    </item>
    <item>
      <title>Re: CW08 V5.0 HC08 chipset</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW08-V5-0-HC08-chipset/m-p/127968#M625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi, Jerry:&lt;BR /&gt;&lt;BR /&gt;The problem is that the MC68HC908QY4 only has a single stop-mode.&lt;BR /&gt;&lt;BR /&gt;All of the HC08 family processors have one stop mode, but with many variations, depending on how configure the peripherals. On the other hand, the HCS08 family has three stop modes. If you choose an HCS08 chip in CW, the stop-mode option should un-grey.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Mar 2006 09:31:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW08-V5-0-HC08-chipset/m-p/127968#M625</guid>
      <dc:creator>rocco</dc:creator>
      <dc:date>2006-03-04T09:31:38Z</dc:date>
    </item>
    <item>
      <title>Re: CW08 V5.0 HC08 chipset</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW08-V5-0-HC08-chipset/m-p/127969#M626</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Thanks for the reply roco, however, I actually have the 908QY4 chip and I'm using the SofTec InDart board for programming purposes.&amp;nbsp; This is the reason why I chose the chip at the beginning of Processor Expert in Codewarrior.&amp;nbsp; I realize that there is only 1 type of Stop mode in the QY4, however I can't seem to set any parameters that would allow me to use the "SetStopMode" function.&amp;nbsp; That's what made me wonder if it was the version of&amp;nbsp;software I was using.&amp;nbsp; Changing the chipset in software may&amp;nbsp;solve my problems with setting Stop mode, however, as I am limited to using this particular chip, does not quite solve my problem either.&amp;nbsp; Do you have any other suggestions for this particular chip?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thank you for taking the time to reply.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Mar 2006 00:37:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW08-V5-0-HC08-chipset/m-p/127969#M626</guid>
      <dc:creator>Jerry</dc:creator>
      <dc:date>2006-03-07T00:37:58Z</dc:date>
    </item>
    <item>
      <title>Re: CW08 V5.0 HC08 chipset</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW08-V5-0-HC08-chipset/m-p/127970#M627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;FONT face="Helv" size="2"&gt;&lt;FONT face="Helv" size="2"&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT face="Helv" size="2"&gt;&lt;FONT face="Helv" size="2"&gt;Hi,&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Helv" size="2"&gt;&lt;FONT face="Helv" size="2"&gt;To activation SetStopMode function it is necessary to enable STOP instruction. The "Clock settings - Low Power Mode settings - STOP instruction enabled" property should be set to "yes" value in CPU Inspector window - Properties page.&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Helv" size="2"&gt;&lt;FONT face="Helv" size="2"&gt;Regards, Processor Expert Support&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Mar 2006 02:00:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW08-V5-0-HC08-chipset/m-p/127970#M627</guid>
      <dc:creator>ProcessorExpert</dc:creator>
      <dc:date>2006-03-07T02:00:01Z</dc:date>
    </item>
    <item>
      <title>Re: CW08 V5.0 HC08 chipset</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW08-V5-0-HC08-chipset/m-p/127971#M628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;That's exactly what I was looking for.&amp;nbsp;&amp;nbsp; Thanks!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;IMG alt=":smileyvery-happy:" class="emoticon emoticon-smileyvery-happy" id="smileyvery-happy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-very-happy.gif" title="Smiley Very Happy" /&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Mar 2006 02:21:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW08-V5-0-HC08-chipset/m-p/127971#M628</guid>
      <dc:creator>Jerry</dc:creator>
      <dc:date>2006-03-07T02:21:27Z</dc:date>
    </item>
  </channel>
</rss>