<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Re: request enhancement for __SEG_END_ feature</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/request-enhancement-for-SEG-END-feature/m-p/179104#M5945</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please refer to following thread for instruction on how to request enhancement in the tool chain.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A __default_attr="77166" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/77166" jivemacro="thread" title="https://community.freescale.com/thread/77166"&gt;https://community.freescale.com/thread/77166&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The way SEG_END is implemented today was useful to a lot of customers. So I would not suggest&amp;nbsp; to change the way it works, but rather add a new command or functionality to the linker.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Jan 2011 18:49:10 GMT</pubDate>
    <dc:creator>CrasyCat</dc:creator>
    <dc:date>2011-01-26T18:49:10Z</dc:date>
    <item>
      <title>request enhancement for __SEG_END_ feature</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/request-enhancement-for-SEG-END-feature/m-p/179103#M5944</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the SEGMENTS section of the PRM file, named address ranges are defined for use in the PLACEMENT section. While it makes sense for __SEG_END_&amp;nbsp; to reflect used&amp;nbsp;range for the sections/segments defined in the PLACEMENT section, it would be more useful if __SEG_END_ reflected the defined range for segments defined in the SEGMENTS section.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Example:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;SEGMENTS&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; RAM = READ_WRITE 0xFD000'G TO 0xFFDFF'G;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; STACK = NO_INIT 0x3E00 TO 0x3FF;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ROM_LOW = READ_ONLY 0x7F4000 to 0x7F6BFF;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ROM_EOL = NO_INIT 0x7F6C00 TO 0x7F6FFF;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ROM_CAL = NO_INIT 0x7F7000 TO 0x7F7FFF;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ROM_MID = READ_ONLY 0x7F8000 TO 0x7FBFFF;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ROM_HI = READ_ONLY 0x7FC000 TO 0x7FFEFF;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; VECTORS = READ_ONLY 0x7FFF10 to 0x7FFFFF;&lt;/P&gt;&lt;P&gt;END&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;PLACEMENT&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DEFAULT_RAM INTO RAM;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SSTACK INTO STACK;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DEFAULT_ROM INTO ROM_LOW, ROM_MID, ROM_HI;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; INTVECT INTO VECTORS;&lt;/P&gt;&lt;P&gt;END&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It would be useful for the address of __SEG_END_ROM_EOL to be 0x7F7000.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jan 2011 06:22:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/request-enhancement-for-SEG-END-feature/m-p/179103#M5944</guid>
      <dc:creator>rlw</dc:creator>
      <dc:date>2011-01-26T06:22:14Z</dc:date>
    </item>
    <item>
      <title>Re: request enhancement for __SEG_END_ feature</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/request-enhancement-for-SEG-END-feature/m-p/179104#M5945</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please refer to following thread for instruction on how to request enhancement in the tool chain.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A __default_attr="77166" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/77166" jivemacro="thread" title="https://community.freescale.com/thread/77166"&gt;https://community.freescale.com/thread/77166&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The way SEG_END is implemented today was useful to a lot of customers. So I would not suggest&amp;nbsp; to change the way it works, but rather add a new command or functionality to the linker.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jan 2011 18:49:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/request-enhancement-for-SEG-END-feature/m-p/179104#M5945</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2011-01-26T18:49:10Z</dc:date>
    </item>
  </channel>
</rss>