<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: USBSPYDER08 Windows Vista Questions</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/USBSPYDER08-Windows-Vista-Questions/m-p/178312#M5876</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Thanks.&amp;nbsp; It worked like a charm.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I haven't written 4k of code yet but if the file license.dat contains this;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;#######################################################&lt;/P&gt;&lt;P&gt;# ( 843): HC08 V6.0 Special Edition&lt;/P&gt;&lt;P&gt;#######################################################&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Does that mean the special edition features are enabled?&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 Jan 2008 12:54:49 GMT</pubDate>
    <dc:creator>rick_l</dc:creator>
    <dc:date>2008-01-10T12:54:49Z</dc:date>
    <item>
      <title>USBSPYDER08 Windows Vista Questions</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/USBSPYDER08-Windows-Vista-Questions/m-p/178310#M5874</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;P&gt;hi... 1st post&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I bought a USBSPYDER08 to do some quick (more important CHEAP) microcontroller applications.&amp;nbsp; The computer near where this takes place runs Windows Vista.&amp;nbsp; CodeWarrior version 5.1 (?) that came on the CD with the part will not load.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I download CW_MCU_V6_1_SE will it work with the USBSPYDER08 ?&amp;nbsp; Is that the same (but&amp;nbsp;newer and compatable)&amp;nbsp;development system that came with the USBSPYDER08 ?&amp;nbsp; Will I be able to obtain the (free) special edition license for this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am clueless as to how USB works.&amp;nbsp; On the CD there is a program called usbspyder08_setup.exe from SofTek Microsystems.&amp;nbsp; Is this what puts the app on the PC to run the USB to CodeWarrior&amp;nbsp;interface?&amp;nbsp; Will it work with VIsta.&amp;nbsp; Do I run that after I install code warrior?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The USBSPYDER08 came populated with a MC9S08QG4CE.&amp;nbsp; If I read the data sheet correctly this part does not have a debug module (DBG).&amp;nbsp; Is that going to cause me additional problems.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sorry about so many questions.&amp;nbsp; Perhaps in my quest to get the most bang for the buck I made a poor choice.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2008 14:52:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/USBSPYDER08-Windows-Vista-Questions/m-p/178310#M5874</guid>
      <dc:creator>rick_l</dc:creator>
      <dc:date>2008-01-09T14:52:42Z</dc:date>
    </item>
    <item>
      <title>Re: USBSPYDER08 Windows Vista Questions</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/USBSPYDER08-Windows-Vista-Questions/m-p/178311#M5875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;BR /&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;rick-l wrote:&lt;BR /&gt;&lt;P&gt;hi... 1st post&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Welcome :-)&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;I bought a USBSPYDER08 to do some quick (more important CHEAP) microcontroller applications.&amp;nbsp; The computer near where this takes place runs Windows Vista.&amp;nbsp; CodeWarrior version 5.1 (?) that came on the CD with the part will not load.&lt;BR /&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;CW 5.1 does not support Vista, basically was released before Vista. Is that what you mean with "will not load"? With Vista, use CW for MCU 6.1.&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;If I download CW_MCU_V6_1_SE will it work with the USBSPYDER08 ?&amp;nbsp; Is that the same (but&amp;nbsp;newer and compatable)&amp;nbsp;development system that came with the USBSPYDER08 ?&amp;nbsp; Will I be able to obtain the (free) special edition license for this?&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;Yes, CW for MCU's 6.1 works with the spyder. The special license is automatically installed, I think (not 100% sure, just 90%).&lt;BR /&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;I am clueless as to how USB works.&amp;nbsp; On the CD there is a program called usbspyder08_setup.exe from SofTek Microsystems.&amp;nbsp; Is this what puts the app on the PC to run the USB to CodeWarrior&amp;nbsp;interface?&amp;nbsp; Will it work with VIsta.&amp;nbsp; Do I run that after I install code warrior?&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I guess you can run it, not sure if it does contain additional examples and stuff for the spyder.&lt;/P&gt;&lt;P&gt;As far as I remember, with HC08 V5.1 you had to install that in order to debug with the spyder. With 6.1, just installing 6.1 is enough to get you going. Create a new project for the SofTec connection.&lt;BR /&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The USBSPYDER08 came populated with a MC9S08QG4CE.&amp;nbsp; If I read the data sheet correctly this part does not have a debug module (DBG).&amp;nbsp; Is that going to cause me additional problems.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;As far as I know the GQ4 has a debug module. So no. Even without a debug modul (I don't think so), the S08 still has a single HW breakpoint.&lt;BR /&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Sorry about so many questions.&amp;nbsp; Perhaps in my quest to get the most bang for the buck I made a poor choice.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I like the spyder because its so small to carry around. But I'm usually not developing a target application, more try things with the development tools.&lt;BR /&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;BR /&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2008 17:51:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/USBSPYDER08-Windows-Vista-Questions/m-p/178311#M5875</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2008-01-09T17:51:32Z</dc:date>
    </item>
    <item>
      <title>Re: USBSPYDER08 Windows Vista Questions</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/USBSPYDER08-Windows-Vista-Questions/m-p/178312#M5876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Thanks.&amp;nbsp; It worked like a charm.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I haven't written 4k of code yet but if the file license.dat contains this;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;#######################################################&lt;/P&gt;&lt;P&gt;# ( 843): HC08 V6.0 Special Edition&lt;/P&gt;&lt;P&gt;#######################################################&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Does that mean the special edition features are enabled?&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jan 2008 12:54:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/USBSPYDER08-Windows-Vista-Questions/m-p/178312#M5876</guid>
      <dc:creator>rick_l</dc:creator>
      <dc:date>2008-01-10T12:54:49Z</dc:date>
    </item>
    <item>
      <title>Re: USBSPYDER08 Windows Vista Questions</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/USBSPYDER08-Windows-Vista-Questions/m-p/178313#M5877</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;yes. And ignore the 0, in 6.0. The license works for 6.1 too.&lt;BR /&gt;&lt;BR /&gt;Daniel&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jan 2008 17:21:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/USBSPYDER08-Windows-Vista-Questions/m-p/178313#M5877</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2008-01-10T17:21:49Z</dc:date>
    </item>
    <item>
      <title>Re: USBSPYDER08 Windows Vista Questions</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/USBSPYDER08-Windows-Vista-Questions/m-p/178314#M5878</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Excuse me, I use Vista too but I have another generic question on the Spyder key: can I use it to debug application based on other 8bits MCUs, let's say, the GZxx?&lt;BR /&gt;Thank you in advance.&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; Max&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Oct 2008 15:28:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/USBSPYDER08-Windows-Vista-Questions/m-p/178314#M5878</guid>
      <dc:creator>maxpayne</dc:creator>
      <dc:date>2008-10-12T15:28:23Z</dc:date>
    </item>
  </channel>
</rss>