<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using all 8K SRAM on NE64-CW4.5 in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/using-all-8K-SRAM-in-NE64-CW4-5/m-p/127647#M587</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks,CompilerGuru.&lt;BR /&gt;Works fine.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 24 Mar 2007 02:53:40 GMT</pubDate>
    <dc:creator>eddie</dc:creator>
    <dc:date>2007-03-24T02:53:40Z</dc:date>
    <item>
      <title>using all 8K SRAM in NE64-CW4.5</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/using-all-8K-SRAM-in-NE64-CW4-5/m-p/127645#M585</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Desperate to use all 8K of internal RAM of NE64.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Changed PRM file to specify RAM at 2000-3FFF.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Compiles okay but doesn't work.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I guess I somehow,somewhere need to change the RAM&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;mapping register(INITRM).How?Where?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Running out of RAM.Any help would be appreciated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Eddie&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Mar 2007 04:22:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/using-all-8K-SRAM-in-NE64-CW4-5/m-p/127645#M585</guid>
      <dc:creator>eddie</dc:creator>
      <dc:date>2007-03-23T04:22:33Z</dc:date>
    </item>
    <item>
      <title>Re: using all 8K SRAM in NE64-CW4.5</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/using-all-8K-SRAM-in-NE64-CW4-5/m-p/127646#M586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Search for INITRM in start12.c.&lt;BR /&gt;There is some code to map the RAM where you want it, but it is only enabled for the serial monitor. So enable the handling of INITRM in there.&lt;BR /&gt;INITRM has to be set in start12.c before Init is called.&lt;BR /&gt;&lt;BR /&gt;Daniel&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Mar 2007 05:32:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/using-all-8K-SRAM-in-NE64-CW4-5/m-p/127646#M586</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2007-03-23T05:32:52Z</dc:date>
    </item>
    <item>
      <title>Using all 8K SRAM on NE64-CW4.5</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/using-all-8K-SRAM-in-NE64-CW4-5/m-p/127647#M587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks,CompilerGuru.&lt;BR /&gt;Works fine.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Mar 2007 02:53:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/using-all-8K-SRAM-in-NE64-CW4-5/m-p/127647#M587</guid>
      <dc:creator>eddie</dc:creator>
      <dc:date>2007-03-24T02:53:40Z</dc:date>
    </item>
  </channel>
</rss>