<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Re: Producing a executable binary</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Producing-a-executable-binary/m-p/177489#M5814</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all.&lt;/P&gt;&lt;P&gt;I've been wanting to find a solution for this as well.&lt;/P&gt;&lt;P&gt;Having the load address &amp;amp; # bytes in the binary file is a bit of a headache.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A simple solution would be to prepend a bit of code to the binary which copies each section based on the load address &amp;amp; number of bytes, &lt;/P&gt;&lt;P&gt;however, I found another solution which is even easier.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Although I've not tried it yet, I did see a solution in another post, so thought I would relay it here.&lt;/P&gt;&lt;P&gt;There are a set of free tools from uTasker - one of which will convert the binary output from CodeWarrior to a flat binary suitable for executing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the link to the uTasker Forum:&amp;nbsp; &lt;A href="http://www.utasker.com/forum/index.php?topic=1445.0" title="http://www.utasker.com/forum/index.php?topic=1445.0"&gt;http://www.utasker.com/forum/index.php?topic=1445.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Under ' uTaskerConvert ' I see details of this function :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Verdana, arial, sans-serif; font-size: 12px; background-color: #e7eaef;"&gt;Added capability to convert Motorola binary to raw binary output. This is useful for CodeWarrior binary output&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Verdana, arial, sans-serif; font-size: 12px; background-color: #e7eaef;"&gt;which can otherwise not be used directly as a code image - after the conversion the content is in raw binary format&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Verdana, arial, sans-serif; font-size: 12px; background-color: #e7eaef;"&gt;and so suitable for general binary program use.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Verdana, arial, sans-serif; font-size: 12px; background-color: #e7eaef;"&gt;User "&lt;/SPAN&gt;&lt;TT class="bbc_tt" style="font-family: 'dejavu sans mono', monaco, 'lucida console', 'courier new', monospace; color: #000000; font-size: 12px; background-color: #e7eaef;"&gt;uTaskerConvert uTasker_BM.bin raw.bin -b&lt;/TT&gt;&lt;SPAN style="color: #000000; font-family: Verdana, arial, sans-serif; font-size: 12px; background-color: #e7eaef;"&gt;"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope that helps.&lt;/P&gt;&lt;P&gt;Ewan J. Wordsworth&lt;/P&gt;&lt;P&gt;Microbee Technology Pty Ltd.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/www.microbeetechnology.com.au" target="test_blank"&gt;www.microbeetechnology.com.au&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Aug 2014 23:24:49 GMT</pubDate>
    <dc:creator>ejwords</dc:creator>
    <dc:date>2014-08-06T23:24:49Z</dc:date>
    <item>
      <title>Producing a executable binary</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Producing-a-executable-binary/m-p/177486#M5811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Version of the compiler is 7.2 CPU type mcf52277&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since my last post I reduced the project to a header table (similar to vetors) and a simple single line of C code. Looking in the binary file produced, preceding the header there are two longs the first is the start address and the second in the size of the header. We want to make a executable binary and having these longs in the code will obviously cause issues. The S Record produced fails as well as it has the wanted code and then the two longs listed below at the same address. How do we produce a pure binary to run without the debugger?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We de-selected "Generate symbolic Info" but the output binary and S record still include these longs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Tony&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Feb 2010 20:37:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Producing-a-executable-binary/m-p/177486#M5811</guid>
      <dc:creator>tonytrm</dc:creator>
      <dc:date>2010-02-19T20:37:32Z</dc:date>
    </item>
    <item>
      <title>Re: Producing a executable binary</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Producing-a-executable-binary/m-p/177487#M5812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We also have a need for a pure binary file!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We were under the false impression that "Generate Binary Image" in CodeWarrior produced a pure binary image file. &amp;nbsp;But this binary file seems to be a binary version of the .s19 file which means we still have to parse it. &amp;nbsp;First 4 bytes are address, next 4 are number of data bytes, and then the data bytes follow. &amp;nbsp;This is repeated for each unique section.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Freescale - how can we get the tools to generate a pure binary image that can be directly downloaded and programmed in flash without having to go through the extra task of parsing it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Mar 2010 06:45:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Producing-a-executable-binary/m-p/177487#M5812</guid>
      <dc:creator>gmnelson</dc:creator>
      <dc:date>2010-03-16T06:45:36Z</dc:date>
    </item>
    <item>
      <title>Re: Producing a executable binary</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Producing-a-executable-binary/m-p/177488#M5813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How about creating an elf file then using objcopy to extract to a binary?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Mar 2010 16:16:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Producing-a-executable-binary/m-p/177488#M5813</guid>
      <dc:creator>martinw</dc:creator>
      <dc:date>2010-03-16T16:16:46Z</dc:date>
    </item>
    <item>
      <title>Re: Producing a executable binary</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Producing-a-executable-binary/m-p/177489#M5814</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all.&lt;/P&gt;&lt;P&gt;I've been wanting to find a solution for this as well.&lt;/P&gt;&lt;P&gt;Having the load address &amp;amp; # bytes in the binary file is a bit of a headache.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A simple solution would be to prepend a bit of code to the binary which copies each section based on the load address &amp;amp; number of bytes, &lt;/P&gt;&lt;P&gt;however, I found another solution which is even easier.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Although I've not tried it yet, I did see a solution in another post, so thought I would relay it here.&lt;/P&gt;&lt;P&gt;There are a set of free tools from uTasker - one of which will convert the binary output from CodeWarrior to a flat binary suitable for executing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the link to the uTasker Forum:&amp;nbsp; &lt;A href="http://www.utasker.com/forum/index.php?topic=1445.0" title="http://www.utasker.com/forum/index.php?topic=1445.0"&gt;http://www.utasker.com/forum/index.php?topic=1445.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Under ' uTaskerConvert ' I see details of this function :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Verdana, arial, sans-serif; font-size: 12px; background-color: #e7eaef;"&gt;Added capability to convert Motorola binary to raw binary output. This is useful for CodeWarrior binary output&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Verdana, arial, sans-serif; font-size: 12px; background-color: #e7eaef;"&gt;which can otherwise not be used directly as a code image - after the conversion the content is in raw binary format&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Verdana, arial, sans-serif; font-size: 12px; background-color: #e7eaef;"&gt;and so suitable for general binary program use.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Verdana, arial, sans-serif; font-size: 12px; background-color: #e7eaef;"&gt;User "&lt;/SPAN&gt;&lt;TT class="bbc_tt" style="font-family: 'dejavu sans mono', monaco, 'lucida console', 'courier new', monospace; color: #000000; font-size: 12px; background-color: #e7eaef;"&gt;uTaskerConvert uTasker_BM.bin raw.bin -b&lt;/TT&gt;&lt;SPAN style="color: #000000; font-family: Verdana, arial, sans-serif; font-size: 12px; background-color: #e7eaef;"&gt;"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope that helps.&lt;/P&gt;&lt;P&gt;Ewan J. Wordsworth&lt;/P&gt;&lt;P&gt;Microbee Technology Pty Ltd.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/www.microbeetechnology.com.au" target="test_blank"&gt;www.microbeetechnology.com.au&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Aug 2014 23:24:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Producing-a-executable-binary/m-p/177489#M5814</guid>
      <dc:creator>ejwords</dc:creator>
      <dc:date>2014-08-06T23:24:49Z</dc:date>
    </item>
    <item>
      <title>Re: Producing a executable binary</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Producing-a-executable-binary/m-p/177490#M5815</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I moved it to CodeWarrior for MCU to increase the possibility of being seen by those who may concern.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Aug 2014 01:31:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Producing-a-executable-binary/m-p/177490#M5815</guid>
      <dc:creator>lunminliang</dc:creator>
      <dc:date>2014-08-07T01:31:10Z</dc:date>
    </item>
    <item>
      <title>Re: Producing a executable binary</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Producing-a-executable-binary/m-p/177491#M5816</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;objcopy for sure should be usable to create a binary, either from the S19 file or from the .elf/.afx file.&lt;/P&gt;&lt;P&gt;I used it like in this post: &lt;A href="http://mcuoneclipse.com/2014/08/03/converting-s19-files-into-binary-files-with-gnu-objcopy/" title="http://mcuoneclipse.com/2014/08/03/converting-s19-files-into-binary-files-with-gnu-objcopy/"&gt;Converting S19 Files into Binary Files with GNU objcopy | MCU on Eclipse&lt;/A&gt;&lt;/P&gt;&lt;P&gt;You can use a post-build step to call objcopy:&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2013/10/29/s-record-manipulation-with-gnu-objcopy-and-burner-utility/" title="http://mcuoneclipse.com/2013/10/29/s-record-manipulation-with-gnu-objcopy-and-burner-utility/"&gt;http://mcuoneclipse.com/2013/10/29/s-record-manipulation-with-gnu-objcopy-and-burner-utility/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Aug 2014 05:31:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Producing-a-executable-binary/m-p/177491#M5816</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-08-07T05:31:06Z</dc:date>
    </item>
  </channel>
</rss>