<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: Setting CodeWarrior 10 Stack Size</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Setting-CodeWarrior-10-Stack-Size/m-p/176182#M5721</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Typically this is in the linker file. The syntax depends from toolchain (well linker) to another, so it is little bit different say for gcc compared to the Freescale compilers.&lt;/P&gt;&lt;P&gt;For Processor Expert enabled project: there is a setting in the CPU component properties &amp;gt; build tab for this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Nov 2012 18:57:08 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2012-11-14T18:57:08Z</dc:date>
    <item>
      <title>Setting CodeWarrior 10 Stack Size</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Setting-CodeWarrior-10-Stack-Size/m-p/176181#M5720</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How do I set the stack size in a project using CodeWarrior 10?&amp;nbsp; Other IDEs that I've used have a setting in the project options to do this, but there doesn't seem to be one for CW10.&amp;nbsp; Is there a file somewhere that needs to be modified?&amp;nbsp; Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Nov 2012 17:21:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Setting-CodeWarrior-10-Stack-Size/m-p/176181#M5720</guid>
      <dc:creator>jimfell</dc:creator>
      <dc:date>2012-11-14T17:21:08Z</dc:date>
    </item>
    <item>
      <title>Re: Setting CodeWarrior 10 Stack Size</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Setting-CodeWarrior-10-Stack-Size/m-p/176182#M5721</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Typically this is in the linker file. The syntax depends from toolchain (well linker) to another, so it is little bit different say for gcc compared to the Freescale compilers.&lt;/P&gt;&lt;P&gt;For Processor Expert enabled project: there is a setting in the CPU component properties &amp;gt; build tab for this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Nov 2012 18:57:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Setting-CodeWarrior-10-Stack-Size/m-p/176182#M5721</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2012-11-14T18:57:08Z</dc:date>
    </item>
    <item>
      <title>Re: Setting CodeWarrior 10 Stack Size</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Setting-CodeWarrior-10-Stack-Size/m-p/176183#M5722</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Nov 2012 23:13:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Setting-CodeWarrior-10-Stack-Size/m-p/176183#M5722</guid>
      <dc:creator>jimfell</dc:creator>
      <dc:date>2012-11-14T23:13:10Z</dc:date>
    </item>
  </channel>
</rss>