<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: External Clock</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/External-Clock/m-p/175268#M5631</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you also enter stop 2 mode?&amp;nbsp; If so, the external clock cannot be used for the RTI; only the internal 1kHz oscillator is available.&amp;nbsp; This must be explicitly enabled for it to&amp;nbsp;continue operating in stop mode.&amp;nbsp; However, the internal oscillator is not available in normal run mode, so the external clock must then&amp;nbsp;be used for the RTI.&amp;nbsp; This is one of the pecularities of the device.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you are&amp;nbsp;connecting a crystal as the external clock, the bit ICGC1_REFS must be set for the XTAL output pin to be available, for the crystal to oscillate.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Oct 2011 19:50:23 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2011-10-21T19:50:23Z</dc:date>
    <item>
      <title>External Clock</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/External-Clock/m-p/175267#M5630</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the KIT EVB 13213-SRB, I have a trouble for use the external clock, I select him to be source cpu clock to use the real time interrupt (RTI) with the external clock,(I just put a led to blink) but when the program is running doesn't happen nothing to the led.&lt;/P&gt;&lt;P&gt;I select in the RTI the external clock in the "clock settings" and put the value 32768 in the prescaler and enabled the interrupts&lt;/P&gt;&lt;P&gt;Could you help me?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Oct 2011 01:58:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/External-Clock/m-p/175267#M5630</guid>
      <dc:creator>cleriton</dc:creator>
      <dc:date>2011-10-20T01:58:01Z</dc:date>
    </item>
    <item>
      <title>Re: External Clock</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/External-Clock/m-p/175268#M5631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you also enter stop 2 mode?&amp;nbsp; If so, the external clock cannot be used for the RTI; only the internal 1kHz oscillator is available.&amp;nbsp; This must be explicitly enabled for it to&amp;nbsp;continue operating in stop mode.&amp;nbsp; However, the internal oscillator is not available in normal run mode, so the external clock must then&amp;nbsp;be used for the RTI.&amp;nbsp; This is one of the pecularities of the device.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you are&amp;nbsp;connecting a crystal as the external clock, the bit ICGC1_REFS must be set for the XTAL output pin to be available, for the crystal to oscillate.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Oct 2011 19:50:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/External-Clock/m-p/175268#M5631</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2011-10-21T19:50:23Z</dc:date>
    </item>
  </channel>
</rss>