<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: CW10 and PE USB Multilink on Win7 x64</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-and-PE-USB-Multilink-on-Win7-x64/m-p/173573#M5526</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you using P&amp;amp;E Microcomputer Systems' 64-bit drivers for the Multilink? They can be downloaded from the web site at &lt;A href="http://www.pemicro.com." rel="nofollow" target="_blank"&gt;www.pemicro.com.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Oct 2011 18:47:03 GMT</pubDate>
    <dc:creator>J2MEJediMaster</dc:creator>
    <dc:date>2011-10-12T18:47:03Z</dc:date>
    <item>
      <title>CW10 and PE USB Multilink on Win7 x64</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-and-PE-USB-Multilink-on-Win7-x64/m-p/173572#M5525</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using a PE micro USB Multilink Interface for development on win7x64, and a MC9S08QE8 device.&lt;/P&gt;&lt;P&gt;I can successfully debug, breakpoint etc.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My problem is in trying to program the device, using the USB Multilink Interface.&lt;/P&gt;&lt;P&gt;I have tried the Simple Flash tool CW10, but it fails, so I used the Flash Programmer and set up a programming task, and it failed too.&lt;/P&gt;&lt;P&gt;The failed results are shown below:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;fl::target -lc "MyAlarm_Using_USB_ML"&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;fl::target -b 0x0 0x0&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;fl::target -v off -l off -ie on -i "" -p MC9S08QE8&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;cmdwin::fl::device -d "MC9S08QE8_FLASH" -o "8kx16x1" -a 0xe000 0xffff&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;cmdwin::fl::erase all&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;Beginning Operation ...&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;-------------------------&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Initializing remote connection ...&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Performing target initialization ...&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Device MC9S08QE8_FLASH&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Detect frequence ...&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Frequence 0 Khz&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;Erasing .............&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Error:&amp;nbsp; Erase Command Failed.&amp;nbsp; Operation timeout. Protect violation error.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;An invalid preference was passed to the GDI protocol plugin(HC GDI Protocol Adapter&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Error: Device MC9S08QE8_FLASH&lt;/STRONG&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Has anybody successfully programmed a device with the PE micro USB Multilink Interface using CW 10?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Details:&lt;/P&gt;&lt;P&gt;CodeWarrior for MCU&lt;BR /&gt;Version: 10.1&lt;BR /&gt;Build Id:110204&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;PE Micro USB Multilink Interface&lt;/P&gt;&lt;P&gt;Rev C&lt;/P&gt;&lt;P&gt;USB HCS08/HCS12 MULTILINK detected - Flash Version 5.84&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Win 7 64 bit&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance. (tia)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Oct 2011 21:31:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-and-PE-USB-Multilink-on-Win7-x64/m-p/173572#M5525</guid>
      <dc:creator>chuckiethedrago</dc:creator>
      <dc:date>2011-10-11T21:31:08Z</dc:date>
    </item>
    <item>
      <title>Re: CW10 and PE USB Multilink on Win7 x64</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-and-PE-USB-Multilink-on-Win7-x64/m-p/173573#M5526</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you using P&amp;amp;E Microcomputer Systems' 64-bit drivers for the Multilink? They can be downloaded from the web site at &lt;A href="http://www.pemicro.com." rel="nofollow" target="_blank"&gt;www.pemicro.com.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Oct 2011 18:47:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-and-PE-USB-Multilink-on-Win7-x64/m-p/173573#M5526</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2011-10-12T18:47:03Z</dc:date>
    </item>
    <item>
      <title>Re: CW10 and PE USB Multilink on Win7 x64</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-and-PE-USB-Multilink-on-Win7-x64/m-p/173574#M5527</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes it has the correct drivers.&lt;/P&gt;&lt;P&gt;It works for debugging. So it does erase and program in debugging mode.&lt;/P&gt;&lt;P&gt;Using the "flash" function of CW10 is where it fails.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I see the problem as a CW -&amp;gt; PE interface, or PE settings problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Oct 2011 20:40:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-and-PE-USB-Multilink-on-Win7-x64/m-p/173574#M5527</guid>
      <dc:creator>chuckiethedrago</dc:creator>
      <dc:date>2011-10-12T20:40:38Z</dc:date>
    </item>
    <item>
      <title>Re: CW10 and PE USB Multilink on Win7 x64</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-and-PE-USB-Multilink-on-Win7-x64/m-p/173575#M5528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you're able to debug the program in RAM, I would think that the CodeWarrior &amp;lt;-&amp;gt; PEMicro interface is working. The flash may be secured accidentally. However, I am also puzzled over that 0 frequency setting. If you haven't already, it's time to file an on-line service request on this. Click &lt;A href="https://www.freescale.com/webapp/servicerequest.create_SR.framework" rel="nofollow" target="_self"&gt;here&lt;/A&gt; to do that.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Oct 2011 19:26:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-and-PE-USB-Multilink-on-Win7-x64/m-p/173575#M5528</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2011-10-14T19:26:49Z</dc:date>
    </item>
    <item>
      <title>Re: CW10 and PE USB Multilink on Win7 x64</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-and-PE-USB-Multilink-on-Win7-x64/m-p/173576#M5529</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Did you get this problem sorted out? If so, what was the solution? I am looking at getting a P&amp;amp;E device for communicating with my EVBQE128 board, on WIN 7 64-bit, seeing as how there is not a SofTec 64-bit USB driver that would support the usual USB comm link between that board and CW v10.1.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 05 Nov 2011 03:24:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW10-and-PE-USB-Multilink-on-Win7-x64/m-p/173576#M5529</guid>
      <dc:creator>buckeyeman</dc:creator>
      <dc:date>2011-11-05T03:24:44Z</dc:date>
    </item>
  </channel>
</rss>