<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problem connecting to MC9S08QG8 with USB-ML-12E using CW6.1 in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Problem-connecting-to-MC9S08QG8-with-USB-ML-12E-using-CW6-1/m-p/173531#M5524</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm stumped on this. It sounds like a hardware problem. The only advice I can give is that you try &lt;A href="http://www.pemicro.com/forums/index.php" rel="nofollow" target="_blank"&gt;P&amp;amp;E Micro's forums&lt;/A&gt; and see if they can help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Apr 2009 20:13:17 GMT</pubDate>
    <dc:creator>J2MEJediMaster</dc:creator>
    <dc:date>2009-04-21T20:13:17Z</dc:date>
    <item>
      <title>Problem connecting to MC9S08QG8 with USB-ML-12E using CW6.1</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Problem-connecting-to-MC9S08QG8-with-USB-ML-12E-using-CW6-1/m-p/173528#M5521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial, Helvetica, sans-serif'; font-size: 2;"&gt;Hi,&lt;BR /&gt;I am having great difficulty writing to flash of the MC9S08QG8 using USB-ML-12E, whenever I attempt to connect to do through real time debugger I keep on getting these two error messages&lt;BR /&gt;&lt;BR /&gt;1.Power Cycle Dialog&lt;BR /&gt;2.ERROR 34 during programming&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone know what &lt;SPAN style="font-family: 'Arial, Helvetica, sans-serif'; font-size: 2;"&gt;ERROR 34 is?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Apr 2009 10:25:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Problem-connecting-to-MC9S08QG8-with-USB-ML-12E-using-CW6-1/m-p/173528#M5521</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2009-04-20T10:25:35Z</dc:date>
    </item>
    <item>
      <title>Re: Problem connecting to MC9S08QG8 with USB-ML-12E using CW6.1</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Problem-connecting-to-MC9S08QG8-with-USB-ML-12E-using-CW6-1/m-p/173529#M5522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have you had any luck communicating with the board? When it's plugged in, do the LEDs on the board light up and stay on, or are they dark?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Apr 2009 19:13:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Problem-connecting-to-MC9S08QG8-with-USB-ML-12E-using-CW6-1/m-p/173529#M5522</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2009-04-20T19:13:53Z</dc:date>
    </item>
    <item>
      <title>Re: Problem connecting to MC9S08QG8 with USB-ML-12E using CW6.1</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Problem-connecting-to-MC9S08QG8-with-USB-ML-12E-using-CW6-1/m-p/173530#M5523</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom,&lt;/P&gt;&lt;P&gt;The blue LED lights up when connected to USB cable and the orange LED lights up when the QG8 is powered up using external power supply.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The set up used to work but then at certain stage I noticed that on the real-time debugger command window it was having trouble&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;"changing frequency down to approx 4 Mhz" to proceed any further.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am not sure if its the QG8 ICS on that particular chip that was causing this problem, it seemed to go away after i changed the chip.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, since then I have found that I was gradually being less able to write to flash per chip and eventually I am stuck at this point.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The only thing I can do is HOTSYNC the chip BUT I can not write to flash or rarely able to, and stuck at this 2 error message not able to go any further.&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by Learner on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-04-20&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;02:58 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Apr 2009 20:57:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Problem-connecting-to-MC9S08QG8-with-USB-ML-12E-using-CW6-1/m-p/173530#M5523</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2009-04-20T20:57:04Z</dc:date>
    </item>
    <item>
      <title>Re: Problem connecting to MC9S08QG8 with USB-ML-12E using CW6.1</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Problem-connecting-to-MC9S08QG8-with-USB-ML-12E-using-CW6-1/m-p/173531#M5524</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm stumped on this. It sounds like a hardware problem. The only advice I can give is that you try &lt;A href="http://www.pemicro.com/forums/index.php" rel="nofollow" target="_blank"&gt;P&amp;amp;E Micro's forums&lt;/A&gt; and see if they can help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Apr 2009 20:13:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Problem-connecting-to-MC9S08QG8-with-USB-ML-12E-using-CW6-1/m-p/173531#M5524</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2009-04-21T20:13:17Z</dc:date>
    </item>
  </channel>
</rss>