<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Configure Virtual SCI and output file from the command prompt in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Configure-Virtual-SCI-and-output-file-from-the-command-prompt/m-p/171418#M5301</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I&amp;nbsp;am targeting HC12. On top of the installed products dialog it stands "CodeWarrior Development Studio for the S12(X) Version 5.0, build 9061"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Dec 2010 23:51:51 GMT</pubDate>
    <dc:creator>Brynas</dc:creator>
    <dc:date>2010-12-22T23:51:51Z</dc:date>
    <item>
      <title>Configure Virtual SCI and output file from the command prompt</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Configure-Virtual-SCI-and-output-file-from-the-command-prompt/m-p/171416#M5299</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;I am currently working on a PERL script for automatically executing abs-files in the debugger for testing purposes. I got stuck on one thing that I haven't managed to find information about&amp;nbsp; how to do in the manual. Does anyone know how to configure the virtual SCI input / output ports and how to set the output file using commands (so that it can be scripted)?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Dec 2010 02:56:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Configure-Virtual-SCI-and-output-file-from-the-command-prompt/m-p/171416#M5299</guid>
      <dc:creator>Brynas</dc:creator>
      <dc:date>2010-12-22T02:56:09Z</dc:date>
    </item>
    <item>
      <title>Re: Configure Virtual SCI and output file from the command prompt</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Configure-Virtual-SCI-and-output-file-from-the-command-prompt/m-p/171417#M5300</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- Which CPU are you targeting (HC08, HC12, Coldfire, ..)&lt;BR /&gt;- Which version of CodeWarrior are you using?&lt;BR /&gt;&amp;nbsp; To retrieve that info:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - Start CodeWarrior&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - Select Help -&amp;gt; About Freescale CodeWarrior&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - Click on "Install Products"&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - CodeWarrior version used is displayed on top in the Installed Products dialog.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Dec 2010 17:06:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Configure-Virtual-SCI-and-output-file-from-the-command-prompt/m-p/171417#M5300</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2010-12-22T17:06:44Z</dc:date>
    </item>
    <item>
      <title>Re: Configure Virtual SCI and output file from the command prompt</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Configure-Virtual-SCI-and-output-file-from-the-command-prompt/m-p/171418#M5301</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I&amp;nbsp;am targeting HC12. On top of the installed products dialog it stands "CodeWarrior Development Studio for the S12(X) Version 5.0, build 9061"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Dec 2010 23:51:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Configure-Virtual-SCI-and-output-file-from-the-command-prompt/m-p/171418#M5301</guid>
      <dc:creator>Brynas</dc:creator>
      <dc:date>2010-12-22T23:51:51Z</dc:date>
    </item>
    <item>
      <title>Re: Configure Virtual SCI and output file from the command prompt</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Configure-Virtual-SCI-and-output-file-from-the-command-prompt/m-p/171419#M5302</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can find some documentation on how to redirect terminal output to a file in the Debugger_HC12.pdf manual.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Look at &lt;EM&gt;&lt;STRONG&gt;Book II HC(S)12(X) Debug Connections&lt;/STRONG&gt;&lt;/EM&gt; &amp;gt; &lt;EM&gt;&lt;STRONG&gt;HC(S)12(X) Full Chip Simulation&lt;/STRONG&gt;&lt;/EM&gt; &amp;gt; &lt;EM&gt;&lt;STRONG&gt;FCS Visualization Utilities&lt;/STRONG&gt;&lt;/EM&gt; &amp;gt; &lt;EM&gt;&lt;STRONG&gt;Terminal component&lt;/STRONG&gt;&lt;/EM&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is a section &lt;STRONG&gt;&lt;EM&gt;File Control Commands&lt;/EM&gt;&lt;/STRONG&gt; explaining how to use escape sequences to redirect stdout to a file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;All you need to do call TERM_Direct with appropriate set of parameters from your main application.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Dec 2010 18:29:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Configure-Virtual-SCI-and-output-file-from-the-command-prompt/m-p/171419#M5302</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2010-12-23T18:29:58Z</dc:date>
    </item>
  </channel>
</rss>