<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Re: Codewarrior with USB dongle on 64-bit Windows 7?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-with-USB-dongle-on-64-bit-Windows-7/m-p/170222#M5190</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry for the late reply, but here is what I did:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CW for HC(X)12 v.5.1: I rehosted the compiler to my disk-ID (instead of the USB-dongle) -&amp;gt; I can continue working on this single machine. Your advice to buy an USB_to_Ethernet-module is very clever, will allow me to use CW on several machines by taking the module along.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CW for HC08 v. 6.3: This version does not install on Win7, so I have installed CW10.2 instead. But since I use this compiler so seldom, I most probably will restart my computer to Win XP when needed (easier than to transfer the old projects from 6.3 to 10.2).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sten&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Aug 2012 18:49:18 GMT</pubDate>
    <dc:creator>StenS</dc:creator>
    <dc:date>2012-08-06T18:49:18Z</dc:date>
    <item>
      <title>Codewarrior with USB dongle on 64-bit Windows 7?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-with-USB-dongle-on-64-bit-Windows-7/m-p/170219#M5187</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am presently using CW for S12 v. 5.1 and for HCS08 v. 6.3 on&amp;nbsp;Win-XP. I have a CW_Pro_NL-licence with a USB dongle. Now I am getting a new computer with 64-bit Windows 7; and the question is, will my CodeWarriors still work? I have during the last years read a lot of comments here on the forum regarding Windows 7; but I haven't found any clear info if it is possible and how to do it in that case. On the CodeWarrior main page I also see this worrying info: "&lt;EM&gt;Please note: USB dongle license configuration not supported on 64 bit Windows 7"&lt;/EM&gt; .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can somebody give a clear reply; what steps must I follow to continue working with v. 5.1 and 6.3 on 64-bit Windows 7?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sten&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2012 14:04:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-with-USB-dongle-on-64-bit-Windows-7/m-p/170219#M5187</guid>
      <dc:creator>StenS</dc:creator>
      <dc:date>2012-06-07T14:04:57Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior with USB dongle on 64-bit Windows 7?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-with-USB-dongle-on-64-bit-Windows-7/m-p/170220#M5188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've the same issue. The dongle has been recongnzed with windows, the codewarrior do not see it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to find a workarround using the compatibility mode&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Jul 2012 14:43:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-with-USB-dongle-on-64-bit-Windows-7/m-p/170220#M5188</guid>
      <dc:creator>AROK</dc:creator>
      <dc:date>2012-07-14T14:43:49Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior with USB dongle on 64-bit Windows 7?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-with-USB-dongle-on-64-bit-Windows-7/m-p/170221#M5189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Like it says, the dongle option is NOT supported for Win 7 64-bit.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are work-arounds, but they involve changing your license type.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Option 1: Switch to a CodeWarrior floating license.&lt;/P&gt;&lt;P&gt;Pro: Gives same flexibility as dongle.&lt;/P&gt;&lt;P&gt;Con: You have to set up a license server, which usually creates headaches for the IT people because they have to unblock a specific IP port.&lt;/P&gt;&lt;P&gt;Con: If you can't get a network connection, you can't use CodeWarrior.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Option 2: Buy a USB-to-Ethernet interface module, and tie the CodeWarrior license to its MAC.&lt;/P&gt;&lt;P&gt;Pro: Gives same flexibility as a dongle, and you get Ethernet connectivity in the bargain.&lt;/P&gt;&lt;P&gt;Pro: Proven to work, and does not require a network connection-- just plug the module into the USB port.&lt;/P&gt;&lt;P&gt;Con: Have to buy the interface module, unless you are using one already.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jul 2012 21:11:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-with-USB-dongle-on-64-bit-Windows-7/m-p/170221#M5189</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2012-07-17T21:11:13Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior with USB dongle on 64-bit Windows 7?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-with-USB-dongle-on-64-bit-Windows-7/m-p/170222#M5190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry for the late reply, but here is what I did:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CW for HC(X)12 v.5.1: I rehosted the compiler to my disk-ID (instead of the USB-dongle) -&amp;gt; I can continue working on this single machine. Your advice to buy an USB_to_Ethernet-module is very clever, will allow me to use CW on several machines by taking the module along.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CW for HC08 v. 6.3: This version does not install on Win7, so I have installed CW10.2 instead. But since I use this compiler so seldom, I most probably will restart my computer to Win XP when needed (easier than to transfer the old projects from 6.3 to 10.2).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sten&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Aug 2012 18:49:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-with-USB-dongle-on-64-bit-Windows-7/m-p/170222#M5190</guid>
      <dc:creator>StenS</dc:creator>
      <dc:date>2012-08-06T18:49:18Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior with USB dongle on 64-bit Windows 7?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-with-USB-dongle-on-64-bit-Windows-7/m-p/170223#M5191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the update. Just be aware that if you have to reformat your hard drive (perhaps because of a system crash), the Disk ID changes, and you'l have to rehost your license. Since you've already done that once, doing it again should not be a problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Aug 2012 20:12:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-with-USB-dongle-on-64-bit-Windows-7/m-p/170223#M5191</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2012-08-06T20:12:56Z</dc:date>
    </item>
  </channel>
</rss>