<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Re: STOP MODE 3</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/STOP-MODE-3/m-p/169348#M5132</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, and welcome to the forum.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do you intend to wake up from STOP3 mode?&amp;nbsp; For other than an external reset, the alternatives would appear to be the RTI module, external interrupt pin, or the KBI module.&amp;nbsp; One of these methods will need to generate an interrupt to provide stop mode exit, and this will need to be enabled prior to entering stop mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Stop mode is entered by&amp;nbsp;incorporating the STOP instruction within the main loop, at the point where&amp;nbsp;you wish to&amp;nbsp;start this mode.&amp;nbsp; For a C program, you would use &lt;FONT face="courier new,courier"&gt;__asm stop;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;When the wake-up source becomes active, the associated ISR code would first be executed, and then&amp;nbsp;the main loop code will resume at the next instruction after the stop instruction.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;Regards,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;Mac&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 26 Sep 2011 05:05:01 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2011-09-26T05:05:01Z</dc:date>
    <item>
      <title>STOP MODE 3</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/STOP-MODE-3/m-p/169347#M5131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I need a help to enter in the stop mode 3 , I am using the kit EVK 13213-SRB, I selected the register and the stop mode tha i will use in the Device Inicilization, but, i don't know the program or code that enter in the stop mode.Could you help me?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Sep 2011 02:54:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/STOP-MODE-3/m-p/169347#M5131</guid>
      <dc:creator>cleriton</dc:creator>
      <dc:date>2011-09-24T02:54:38Z</dc:date>
    </item>
    <item>
      <title>Re: STOP MODE 3</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/STOP-MODE-3/m-p/169348#M5132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, and welcome to the forum.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do you intend to wake up from STOP3 mode?&amp;nbsp; For other than an external reset, the alternatives would appear to be the RTI module, external interrupt pin, or the KBI module.&amp;nbsp; One of these methods will need to generate an interrupt to provide stop mode exit, and this will need to be enabled prior to entering stop mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Stop mode is entered by&amp;nbsp;incorporating the STOP instruction within the main loop, at the point where&amp;nbsp;you wish to&amp;nbsp;start this mode.&amp;nbsp; For a C program, you would use &lt;FONT face="courier new,courier"&gt;__asm stop;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;When the wake-up source becomes active, the associated ISR code would first be executed, and then&amp;nbsp;the main loop code will resume at the next instruction after the stop instruction.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;Regards,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;Mac&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Sep 2011 05:05:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/STOP-MODE-3/m-p/169348#M5132</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2011-09-26T05:05:01Z</dc:date>
    </item>
    <item>
      <title>Re: STOP MODE 3</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/STOP-MODE-3/m-p/169349#M5133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank's for the help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Solved My problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks a lot.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Sep 2011 23:57:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/STOP-MODE-3/m-p/169349#M5133</guid>
      <dc:creator>cleriton</dc:creator>
      <dc:date>2011-09-26T23:57:45Z</dc:date>
    </item>
  </channel>
</rss>