<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックProgramming code with BDM</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Programming-code-with-BDM/m-p/168848#M5099</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With P&amp;amp;E BDM, when we download software into flash memory (HCS12 or S08) is there a way to keep un-erase some specific flash pages?&amp;nbsp; In our design, these pages are used for calibration parameters and we dont want to enter them each time we upgrade the device software.&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Sep 2011 00:32:44 GMT</pubDate>
    <dc:creator>lsi</dc:creator>
    <dc:date>2011-09-23T00:32:44Z</dc:date>
    <item>
      <title>Programming code with BDM</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Programming-code-with-BDM/m-p/168848#M5099</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With P&amp;amp;E BDM, when we download software into flash memory (HCS12 or S08) is there a way to keep un-erase some specific flash pages?&amp;nbsp; In our design, these pages are used for calibration parameters and we dont want to enter them each time we upgrade the device software.&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Sep 2011 00:32:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Programming-code-with-BDM/m-p/168848#M5099</guid>
      <dc:creator>lsi</dc:creator>
      <dc:date>2011-09-23T00:32:44Z</dc:date>
    </item>
    <item>
      <title>Re: Programming code with BDM</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Programming-code-with-BDM/m-p/168849#M5100</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On MCU's with more than one flash array or flash+EEPROM you can make debugger not erasing specific flash arrays or EEPROM. On others and in case you need to protect just one sector of flash use save-restore method using debugger *.cmd files:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A __default_attr="92804" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/92804" jivemacro="thread" title="https://community.freescale.com/thread/92804"&gt;https://community.freescale.com/thread/92804&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Sep 2011 01:20:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Programming-code-with-BDM/m-p/168849#M5100</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2011-09-23T01:20:49Z</dc:date>
    </item>
  </channel>
</rss>