<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic problem re-installing cw 10.1 in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/problem-re-installing-cw-10-1/m-p/168536#M5089</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I installed cw 10.1 and the patches but I could not get rid of one of the build error messages I had asking to install a CW patch. (Environment is win7 -64 targeting kinetis chips btw).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I uninstalled the cw eclipse environent, including the .eclipse user directory.&lt;/P&gt;&lt;P&gt;When I tried to re-install it went through the motions, but when i tried to run it it refused, just saying :"an error has occurred. se the logfile in c:\users\..\.metadata\.log&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;this file (attached) has a long sob story about things it could not resolve, among other complaints.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried again, attemting to remove any trace of the previous program to allow a completely clean install, but no luck.&lt;/P&gt;&lt;P&gt;my guess is there must be some junk left in the registry that is causing trouble.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any ideas how to get out of this mess and install the thing again?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Sep 2011 23:45:56 GMT</pubDate>
    <dc:creator>stav</dc:creator>
    <dc:date>2011-09-21T23:45:56Z</dc:date>
    <item>
      <title>problem re-installing cw 10.1</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/problem-re-installing-cw-10-1/m-p/168536#M5089</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I installed cw 10.1 and the patches but I could not get rid of one of the build error messages I had asking to install a CW patch. (Environment is win7 -64 targeting kinetis chips btw).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I uninstalled the cw eclipse environent, including the .eclipse user directory.&lt;/P&gt;&lt;P&gt;When I tried to re-install it went through the motions, but when i tried to run it it refused, just saying :"an error has occurred. se the logfile in c:\users\..\.metadata\.log&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;this file (attached) has a long sob story about things it could not resolve, among other complaints.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried again, attemting to remove any trace of the previous program to allow a completely clean install, but no luck.&lt;/P&gt;&lt;P&gt;my guess is there must be some junk left in the registry that is causing trouble.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any ideas how to get out of this mess and install the thing again?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2011 23:45:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/problem-re-installing-cw-10-1/m-p/168536#M5089</guid>
      <dc:creator>stav</dc:creator>
      <dc:date>2011-09-21T23:45:56Z</dc:date>
    </item>
    <item>
      <title>Re: problem re-installing cw 10.1 - solved</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/problem-re-installing-cw-10-1/m-p/168537#M5090</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok for the benefit of the next guy who has this problem, here is the solution:&lt;/P&gt;&lt;P&gt;on Win 7 if the program cannot write to a protected directory (eg programs\...), it will set up a ghost directory which it&lt;/P&gt;&lt;P&gt;will use instead uder the current user's name in the users directory under ...\virtualstore\etc .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It did not help that I had admin rights. This was messing up the re-install, until I erased it manually. The uninstall does not handle it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2011 14:59:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/problem-re-installing-cw-10-1/m-p/168537#M5090</guid>
      <dc:creator>stav</dc:creator>
      <dc:date>2011-09-22T14:59:43Z</dc:date>
    </item>
  </channel>
</rss>