<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: Failed to resume target process., Download using 3rd party component...</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Failed-to-resume-target-process-Download-using-3rd-party/m-p/167933#M5029</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My fault.&amp;nbsp; I had two isr's assigned to the same interrupt vector.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I suppose the build doesn't catch that error and left the "3rd party component" -- whatever that is -- with an impossible task. Is that it?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 May 2012 21:31:42 GMT</pubDate>
    <dc:creator>cab</dc:creator>
    <dc:date>2012-05-31T21:31:42Z</dc:date>
    <item>
      <title>Failed to resume target process., Download using 3rd party component...</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Failed-to-resume-target-process-Download-using-3rd-party/m-p/167930#M5026</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CW10.2 MC9S08LG32 Win7x64&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Fresh install of CW10.2.&amp;nbsp; New project using bareboard and adding source files.&amp;nbsp; After build I used Run-&amp;gt;Debug Configurations and got this message:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Problem Occurred&lt;BR /&gt;'Launching MASTER_MC9S08LG32_PnE U-Multilink' has&lt;BR /&gt;encountered a problem...&lt;BR /&gt;&lt;BR /&gt;Failed to resume target Process., Download using 3rd&lt;BR /&gt;party component..&lt;BR /&gt;[&amp;lt;&amp;lt;Details]&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;And the details just repeat the error message.&amp;nbsp; I cannot fathom how to address this error--CW was freshly installed, I did nothing but create a bareboard project, Build, and then Run-&amp;gt;DebugConfiguration-&amp;gt;[MASTER_MC9S08LG32_PnE U-Multilink]-&amp;gt;Debug.&amp;nbsp; It started the process for awhile, then the error message.&amp;nbsp; This has occurred before, just prior to my fresh install, and I thought the fresh install would fix it as it has fixed my many Java NullPointerExceptions, as documented in my longish NullPointerException post.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am stumped how to recover--is the 3rd-party component on the internet somewhere--supposed to be on my windows system? Do I have a system which CW10.2 does not work on? I saw no error messages when I installed CW for the nth time--it does not appear that re-installing is going to work.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If anybody has a suggestion, it would be much appreciated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-Cab-&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 May 2012 08:16:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Failed-to-resume-target-process-Download-using-3rd-party/m-p/167930#M5026</guid>
      <dc:creator>cab</dc:creator>
      <dc:date>2012-05-31T08:16:45Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to resume target process., Download using 3rd party component...</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Failed-to-resume-target-process-Download-using-3rd-party/m-p/167931#M5027</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well, I have two projects in workspace500 -- MASTER and SLAVE.&amp;nbsp; The SLAVE project downloaded okay, but the MASTER did not when I went back to it.&amp;nbsp; These were both built from bareboard and they are almost alike--one is the master and the other the slave on an IIC bus.&amp;nbsp; I will try to see if I can spot some feature that might explain things--I just wanted to get this reply out in case it helps anyone interested.&lt;/P&gt;&lt;P&gt;-Cab-&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 May 2012 08:29:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Failed-to-resume-target-process-Download-using-3rd-party/m-p/167931#M5027</guid>
      <dc:creator>cab</dc:creator>
      <dc:date>2012-05-31T08:29:35Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to resume target process., Download using 3rd party component...</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Failed-to-resume-target-process-Download-using-3rd-party/m-p/167932#M5028</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So I tried downloading the MASTER code into the SLAVE processor--that must be it, something wrong with the MASTER hardware--but no, the MASTER program won't download anywhere--I got the original "Failed to resume target process."&lt;/P&gt;&lt;P&gt;- Alas, but at least I didn't break the customer hardware.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 May 2012 08:37:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Failed-to-resume-target-process-Download-using-3rd-party/m-p/167932#M5028</guid>
      <dc:creator>cab</dc:creator>
      <dc:date>2012-05-31T08:37:36Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to resume target process., Download using 3rd party component...</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Failed-to-resume-target-process-Download-using-3rd-party/m-p/167933#M5029</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My fault.&amp;nbsp; I had two isr's assigned to the same interrupt vector.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I suppose the build doesn't catch that error and left the "3rd party component" -- whatever that is -- with an impossible task. Is that it?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 May 2012 21:31:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Failed-to-resume-target-process-Download-using-3rd-party/m-p/167933#M5029</guid>
      <dc:creator>cab</dc:creator>
      <dc:date>2012-05-31T21:31:42Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to resume target process., Download using 3rd party component...</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Failed-to-resume-target-process-Download-using-3rd-party/m-p/167934#M5030</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;the "3rd party component" is the P&amp;amp;E library (3rd Party of Freescale).&lt;/P&gt;&lt;P&gt;Looks you were running into this problem:&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.wordpress.com/2012/03/30/problem-occurred-flash-programming-with-overlapping-memory/" rel="nofollow" target="_blank"&gt;http://mcuoneclipse.wordpress.com/2012/03/30/problem-occurred-flash-programming-with-overlapping-memory/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I really wish there would be a better error message.&lt;/P&gt;&lt;P&gt;But as you had assigned two interrupt vectors for the same memory location, this was causing an overlap. My guess and thinking.&lt;/P&gt;&lt;P&gt;Sorry, I did not think about this the first time.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 May 2012 22:21:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Failed-to-resume-target-process-Download-using-3rd-party/m-p/167934#M5030</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2012-05-31T22:21:16Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to resume target process., Download using 3rd party component...</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Failed-to-resume-target-process-Download-using-3rd-party/m-p/167935#M5031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ahh, I had those warnings disabled as well.&amp;nbsp; Very useful post,.&amp;nbsp; Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 May 2012 23:01:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Failed-to-resume-target-process-Download-using-3rd-party/m-p/167935#M5031</guid>
      <dc:creator>cab</dc:creator>
      <dc:date>2012-05-31T23:01:35Z</dc:date>
    </item>
  </channel>
</rss>