<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Full Chip simulator problem for MCF51JE256 in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Full-Chip-simulator-problem-for-MCF51JE256/m-p/164277#M4698</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes. The service pack allows to compile the code, providing include files and libraries for JE256. Without this service pack is impossible to compile code for JE256/128.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, apparently﻿&amp;nbsp;full chip simulator is not supported.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Sep 2011 20:47:41 GMT</pubDate>
    <dc:creator>gustavod</dc:creator>
    <dc:date>2011-09-02T20:47:41Z</dc:date>
    <item>
      <title>Full Chip simulator problem for MCF51JE256</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Full-Chip-simulator-problem-for-MCF51JE256/m-p/164275#M4696</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using CodeWarrior 6.3 with MCF51JE256 microcontroller.&lt;/P&gt;&lt;P&gt;I'm able to compile my project, but when i try to do the full chip simulator there is no JE microcontroller into derivatives options.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a workaround for that?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Gustavo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2011 19:26:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Full-Chip-simulator-problem-for-MCF51JE256/m-p/164275#M4696</guid>
      <dc:creator>gustavod</dc:creator>
      <dc:date>2011-09-02T19:26:16Z</dc:date>
    </item>
    <item>
      <title>Re: Full Chip simulator problem for MCF51JE256</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Full-Chip-simulator-problem-for-MCF51JE256/m-p/164276#M4697</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you have JE256 service pack installed? CW 6.3. updates:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_UPDATES_MCU_63" rel="nofollow" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_UPDATES_MCU_63&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2011 20:36:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Full-Chip-simulator-problem-for-MCF51JE256/m-p/164276#M4697</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2011-09-02T20:36:56Z</dc:date>
    </item>
    <item>
      <title>Re: Full Chip simulator problem for MCF51JE256</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Full-Chip-simulator-problem-for-MCF51JE256/m-p/164277#M4698</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes. The service pack allows to compile the code, providing include files and libraries for JE256. Without this service pack is impossible to compile code for JE256/128.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, apparently﻿&amp;nbsp;full chip simulator is not supported.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2011 20:47:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Full-Chip-simulator-problem-for-MCF51JE256/m-p/164277#M4698</guid>
      <dc:creator>gustavod</dc:creator>
      <dc:date>2011-09-02T20:47:41Z</dc:date>
    </item>
  </channel>
</rss>