<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Re: HC12 V3.1 Intermittent Communication With BDM Multilink</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-V3-1-Intermittent-Communication-With-BDM-Multilink/m-p/163799#M4662</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hunh... I never thought to check the Power Settings.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I'm running Windows XP Pro, but checking the Power Options under the control panel, I don't see anything that I can identify that might fix this, if it's the problem.&amp;nbsp; Is there some other tool I can use to check this out?&amp;nbsp; I'm afraid I don't know where this is actually controlled.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;-Laura&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 Jun 2008 22:29:27 GMT</pubDate>
    <dc:creator>slaybalj</dc:creator>
    <dc:date>2008-06-16T22:29:27Z</dc:date>
    <item>
      <title>HC12 V3.1 Intermittent Communication With BDM Multilink</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-V3-1-Intermittent-Communication-With-BDM-Multilink/m-p/163791#M4654</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I'm trying to set up a new installation of CW HC12 V3.1, but I'm having problems getting the BDM USB Multilink to work.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Sometimes when I run the debugger, it cannot find the BDM.&amp;nbsp; When this happens and I open the ICD-12 &amp;gt; Connect&amp;nbsp; dialog box from the debugger menu bar, it will not display the USB interface at all.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Sometimes when I run the debugger, it will find the USB BDM just fine, but&amp;nbsp;at about 80%, it'll lose connection and stop.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;This last time I also got a windows generated error message when it failed.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The only information I can get from my coworkers for installation is as follows:&lt;/DIV&gt;&lt;DIV&gt;1) 2 updates must be downloaded and installed to work, as well as the P&amp;amp;E BDM driver.&lt;/DIV&gt;&lt;DIV&gt;2) Installing more than just those two updates will cause the program to fail and need to be uninstalled.&lt;/DIV&gt;&lt;DIV&gt;3) Running the updates in the wrong order will cause the program to fail and need to be uninstalled.&lt;/DIV&gt;&lt;DIV&gt;4) They can't remember which updates were necessary or what order they need to be installed in.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Does anybody have any information on this?&amp;nbsp; I can't help but think some of what they're telling me is wrong.&amp;nbsp; But still, if anyone can provide suggestions, I could use some.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;-slaybalj&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jun 2008 04:04:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-V3-1-Intermittent-Communication-With-BDM-Multilink/m-p/163791#M4654</guid>
      <dc:creator>slaybalj</dc:creator>
      <dc:date>2008-06-12T04:04:00Z</dc:date>
    </item>
    <item>
      <title>Re: HC12 V3.1 Intermittent Communication With BDM Multilink</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-V3-1-Intermittent-Communication-With-BDM-Multilink/m-p/163792#M4655</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I'm using the same version and P&amp;amp;E Cyclone Pro which should be identical to the Multilink. To get the debugger working I have to install a strange file "icd12.tgt" I once received from Freescale support...&lt;BR /&gt;&lt;BR /&gt;Still, CW3.1 doesn't set up the P&amp;amp;E drivers properly or something, because I have to run a P&amp;amp;E program and then close it before I can even use the debugger with P&amp;amp;E equipment. I don't have this problem with newer CW versions though, so it seems to be some flaws in CW3.1.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jun 2008 13:36:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-V3-1-Intermittent-Communication-With-BDM-Multilink/m-p/163792#M4655</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2008-06-12T13:36:16Z</dc:date>
    </item>
    <item>
      <title>Re: HC12 V3.1 Intermittent Communication With BDM Multilink</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-V3-1-Intermittent-Communication-With-BDM-Multilink/m-p/163793#M4656</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If you intend to use the USB Multilink cable, I would suggest you to switch to the latest release V4.7.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;You have support for USB multilink cable out of the box there.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;CrasyCat&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jun 2008 18:38:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-V3-1-Intermittent-Communication-With-BDM-Multilink/m-p/163793#M4656</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2008-06-12T18:38:05Z</dc:date>
    </item>
    <item>
      <title>Re: HC12 V3.1 Intermittent Communication With BDM Multilink</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-V3-1-Intermittent-Communication-With-BDM-Multilink/m-p/163794#M4657</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Crasy,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I wish I could.&amp;nbsp; But this is for a project that's already been developed under 3.1, and noone wants to try to do a compiler upgrade at this point.&amp;nbsp; We also have a full license for 3.1 and not for 4.7.&amp;nbsp;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Unfortunately, noone remembers how to make it work.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Laura&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jun 2008 19:50:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-V3-1-Intermittent-Communication-With-BDM-Multilink/m-p/163794#M4657</guid>
      <dc:creator>slaybalj</dc:creator>
      <dc:date>2008-06-12T19:50:55Z</dc:date>
    </item>
    <item>
      <title>Re: HC12 V3.1 Intermittent Communication With BDM Multilink</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-V3-1-Intermittent-Communication-With-BDM-Multilink/m-p/163795#M4658</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Looking into our Web page there is a service pack available, that you can install on top of V3.1&lt;/DIV&gt;&lt;DIV&gt;to add support for USB 2.0 multilink.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; - Go to &lt;A href="http://www.freescale.com" rel="nofollow" target="_blank"&gt;www.freescale.com&lt;/A&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; - Click on Downloads&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; - Click on "Updates &amp;amp; Patches"&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; - Click on "CodeWarrior for HCS12(X)"&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; - Click on "Updates for CodeWarrior for HCS12 v3.1 and earlier"&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; - Download and install "CodeWarrior for HC12 v3.1 - USB 2.0 Service Pack"&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I am not sure if there are dependency to other service packs. Please read carefully the release notes&lt;/DIV&gt;&lt;DIV&gt;coming with this install.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;CrasyCat&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jun 2008 16:50:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-V3-1-Intermittent-Communication-With-BDM-Multilink/m-p/163795#M4658</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2008-06-13T16:50:44Z</dc:date>
    </item>
    <item>
      <title>Re: HC12 V3.1 Intermittent Communication With BDM Multilink</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-V3-1-Intermittent-Communication-With-BDM-Multilink/m-p/163796#M4659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Crasy,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Yes,&amp;nbsp; I have installed that update after installing 3.1.&amp;nbsp; It allows me to usually see the BDM Multilink on the connect window.&amp;nbsp; However, when attempting to run the debugger, it will almost invariably hang at 80% when programming the chip.&amp;nbsp; It will not do this under 4.7 while using the same board and BDM.&amp;nbsp; For these steps I'm attempting a plain old vanilla project created with the project wizard and no changes made to program.&amp;nbsp; All the program does is go into an infinite loop and performs no action.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;When it hangs, the only message that shows up in the debugger window is 'Mcu invalidated'.&amp;nbsp; No other comments at all.&amp;nbsp; If I google search on that message, I get a few other forums for people having trouble, however none of the suggestions seem to point towards a solution for me.&amp;nbsp; I've wondered if it's some sort of timing issue, since the autoset clock is different from what I get when I manually compute the timing calculation (15, vs 14).&amp;nbsp; However, I cannot communicate at all when I manually set the timing to 14.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I qualified the above statements with a 'usually' and an 'almost always' because sometimes when I start the debugger, the BDM doesn't appear at all, even when the blue and yellow lights are on.&amp;nbsp; If it doesn't appear at all, I can usually get it to appear by opening the 'Connect' dialog box&amp;nbsp; and manually selecting it or repeatedly trying to open the debugger and going to the 'Connect' dialog box.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Finally, just last morning, I got a setup that appeared to work.&amp;nbsp; But that install process has been unrepeatable.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If it helps any, I've been trying to install some permutation of:&lt;/DIV&gt;&lt;DIV&gt;CW 3.1&lt;/DIV&gt;&lt;DIV&gt;Patch C128&lt;/DIV&gt;&lt;DIV&gt;Patch E256&lt;/DIV&gt;&lt;DIV&gt;USB 2.0 Patch&lt;/DIV&gt;&lt;DIV&gt;P&amp;amp;E BDM Multilink Drivers.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Additionally, CW3.1 offers to install a different BDM driver (Noral ?).&amp;nbsp; I've tried installing with and without this.&amp;nbsp; I have no idea whether&amp;nbsp;it works in conjunction with the P&amp;amp;E driver, just gets in the way, or is irrelevent.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;-slaybalj&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jun 2008 19:46:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-V3-1-Intermittent-Communication-With-BDM-Multilink/m-p/163796#M4659</guid>
      <dc:creator>slaybalj</dc:creator>
      <dc:date>2008-06-13T19:46:44Z</dc:date>
    </item>
    <item>
      <title>Re: HC12 V3.1 Intermittent Communication With BDM Multilink</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-V3-1-Intermittent-Communication-With-BDM-Multilink/m-p/163797#M4660</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I've had the same issue with the USB version of BDM with CW 3.x I found that it was the power management in the PC that was the problem.&lt;BR /&gt;&lt;BR /&gt;I suspect that the power management wasn't correctly tracking the activity of the USB connection and shutting down the USB port.&lt;BR /&gt;&lt;BR /&gt;Once I did that, I had no problem with my laptop (Win2K) using the BDM MultiLink or a desktop running WinXP. Haven't run it with Vista yet. I got all my tools over on Vista with the exception of CW, and I don't think that's gonna happen any time soon.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jun 2008 00:13:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-V3-1-Intermittent-Communication-With-BDM-Multilink/m-p/163797#M4660</guid>
      <dc:creator>mke_et</dc:creator>
      <dc:date>2008-06-16T00:13:52Z</dc:date>
    </item>
    <item>
      <title>Re: HC12 V3.1 Intermittent Communication With BDM Multilink</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-V3-1-Intermittent-Communication-With-BDM-Multilink/m-p/163798#M4661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;CodeWarrior for HC12 V4.7 does run on Windows Vista.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Please read "{INSTALLATION DIRECTORY}\Release_Notes\HC12\Notes_CW_HC12_Vista.txt" for information on limitation when running on Vista.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;CrasyCat&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jun 2008 18:40:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-V3-1-Intermittent-Communication-With-BDM-Multilink/m-p/163798#M4661</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2008-06-16T18:40:27Z</dc:date>
    </item>
    <item>
      <title>Re: HC12 V3.1 Intermittent Communication With BDM Multilink</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-V3-1-Intermittent-Communication-With-BDM-Multilink/m-p/163799#M4662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hunh... I never thought to check the Power Settings.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I'm running Windows XP Pro, but checking the Power Options under the control panel, I don't see anything that I can identify that might fix this, if it's the problem.&amp;nbsp; Is there some other tool I can use to check this out?&amp;nbsp; I'm afraid I don't know where this is actually controlled.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;-Laura&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jun 2008 22:29:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-V3-1-Intermittent-Communication-With-BDM-Multilink/m-p/163799#M4662</guid>
      <dc:creator>slaybalj</dc:creator>
      <dc:date>2008-06-16T22:29:27Z</dc:date>
    </item>
    <item>
      <title>Re: HC12 V3.1 Intermittent Communication With BDM Multilink</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-V3-1-Intermittent-Communication-With-BDM-Multilink/m-p/163800#M4663</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;It's been a long time ago that I fixed my setup. I turned off all power management to fix the problem then started playing forward.&lt;BR /&gt;&lt;BR /&gt;There was another thread where an individual suggested going right to the hardware devices and finding the USB rot hub and telling that to not turn off power.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jun 2008 00:23:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-V3-1-Intermittent-Communication-With-BDM-Multilink/m-p/163800#M4663</guid>
      <dc:creator>mke_et</dc:creator>
      <dc:date>2008-06-23T00:23:02Z</dc:date>
    </item>
  </channel>
</rss>