<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: Software analysis/trace for HCS08</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Software-analysis-trace-for-HCS08/m-p/154840#M3900</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Erich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That would be Linux (Mageia 32-bit), CW10.2. I'll check my cwide-env file later this evening.&lt;/P&gt;&lt;P&gt;I just checked it on WinXP, CW10.2, and was able to run one analysis.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Oct 2012 21:04:22 GMT</pubDate>
    <dc:creator>bob_walker</dc:creator>
    <dc:date>2012-10-29T21:04:22Z</dc:date>
    <item>
      <title>Software analysis/trace for HCS08</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Software-analysis-trace-for-HCS08/m-p/154838#M3898</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For some reason, the P&amp;amp;E debugger won't download when I enable trace/software analysis. I get a "An internal error occurred during...." error message. At startup, I'm always greeted with "There is a mismatch between the System environment and the workbench environment, which may result in Software Analysis malfunctioning." I suspect that this is the case. Has anyone seen this one before? Any solution? Any idea where to look?&lt;/P&gt;&lt;P&gt;Perhaps and environment variable is whacked?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Oct 2012 20:17:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Software-analysis-trace-for-HCS08/m-p/154838#M3898</guid>
      <dc:creator>bob_walker</dc:creator>
      <dc:date>2012-10-26T20:17:52Z</dc:date>
    </item>
    <item>
      <title>Re: Software analysis/trace for HCS08</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Software-analysis-trace-for-HCS08/m-p/154839#M3899</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Windows or Linux host? Which version (10.2 or 10.3)?&lt;/P&gt;&lt;P&gt;Have you just installed a service pack or an update? I have seen such a thing if I do a 'restart' of Eclipse instead of closing it and then start a fresh one.&lt;/P&gt;&lt;P&gt;Not sure, but it could be related to the LD_LIBRARY_PATH (or similar). Could you check/post the content of your cwide-env file (located in the eclipse folder) and check if all the paths exist on your system?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Oct 2012 09:32:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Software-analysis-trace-for-HCS08/m-p/154839#M3899</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2012-10-29T09:32:24Z</dc:date>
    </item>
    <item>
      <title>Re: Software analysis/trace for HCS08</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Software-analysis-trace-for-HCS08/m-p/154840#M3900</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Erich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That would be Linux (Mageia 32-bit), CW10.2. I'll check my cwide-env file later this evening.&lt;/P&gt;&lt;P&gt;I just checked it on WinXP, CW10.2, and was able to run one analysis.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Oct 2012 21:04:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Software-analysis-trace-for-HCS08/m-p/154840#M3900</guid>
      <dc:creator>bob_walker</dc:creator>
      <dc:date>2012-10-29T21:04:22Z</dc:date>
    </item>
  </channel>
</rss>