<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: HCS12(X) V4.7 Install problem with error 1722 in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HCS12-X-V4-7-Install-problem-with-error-1722/m-p/154145#M3860</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you running the 64-bit version of XP? If so, you may want to look at this &lt;A href="http://forums.freescale.com/freescale/board/message?board.id=CWCOMM&amp;amp;thread.id=4561&amp;amp;page=5" target="_self"&gt;thread&lt;/A&gt;. Although it's about Vista, the trouble is the same in that it was the 64-bit version that was causing problems for the CodeWarrior installer. That solution might apply here.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Nov 2009 21:12:59 GMT</pubDate>
    <dc:creator>J2MEJediMaster</dc:creator>
    <dc:date>2009-11-13T21:12:59Z</dc:date>
    <item>
      <title>HCS12(X) V4.7 Install problem with error 1722</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HCS12-X-V4-7-Install-problem-with-error-1722/m-p/154144#M3859</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, have seen problems on VISTA with this error message but I'm on XPSP2&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Trying to install CWHCS12X_v4.7.exe gives the following message when progress bar reaches the end:&lt;/P&gt;&lt;P&gt;"Error 1722. There is aproblem with this Windows Installer package. A program run as part of the setupdid not finish as expected"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anyone come across this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Nov 2009 19:43:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HCS12-X-V4-7-Install-problem-with-error-1722/m-p/154144#M3859</guid>
      <dc:creator>daveybadlad</dc:creator>
      <dc:date>2009-11-13T19:43:48Z</dc:date>
    </item>
    <item>
      <title>Re: HCS12(X) V4.7 Install problem with error 1722</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HCS12-X-V4-7-Install-problem-with-error-1722/m-p/154145#M3860</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you running the 64-bit version of XP? If so, you may want to look at this &lt;A href="http://forums.freescale.com/freescale/board/message?board.id=CWCOMM&amp;amp;thread.id=4561&amp;amp;page=5" target="_self"&gt;thread&lt;/A&gt;. Although it's about Vista, the trouble is the same in that it was the 64-bit version that was causing problems for the CodeWarrior installer. That solution might apply here.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Nov 2009 21:12:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HCS12-X-V4-7-Install-problem-with-error-1722/m-p/154145#M3860</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2009-11-13T21:12:59Z</dc:date>
    </item>
    <item>
      <title>Re: HCS12(X) V4.7 Install problem with error 1722</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HCS12-X-V4-7-Install-problem-with-error-1722/m-p/154146#M3861</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found the problem!! :smileyhappy:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;P&amp;amp;E micro (and other codewarrior versions) install windrvr6.sys.&amp;nbsp; If this driver is loaded already, the installer fails when executing wdreg_gui.exe -inf "C:\Program Files\Freescale\CodeWarrior for HCS12 V4.7\Drivers\windrvr6.inf" install&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;SOLUTION:&lt;/P&gt;&lt;P&gt;Uninstall the windrvr6 driver and remove files so that the installer can re-install them&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It may also have been possible to disable the P&amp;amp;E micro feature in a custom install??&lt;/P&gt;&lt;P&gt;I'm up and running now anyway! :smileyhappy:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Nov 2009 21:35:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HCS12-X-V4-7-Install-problem-with-error-1722/m-p/154146#M3861</guid>
      <dc:creator>daveybadlad</dc:creator>
      <dc:date>2009-11-13T21:35:29Z</dc:date>
    </item>
  </channel>
</rss>