<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Library Inclusion in CW 10 Application Project</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Library-Inclusion-in-CW-10-Application-Project/m-p/152653#M3745</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a CodeWarrior 10 application project that references multiple compiled libraries.&amp;nbsp; One of these libraries references yet another library.&amp;nbsp; All of the library projects build without any problems.&amp;nbsp; However, when I try to build my application project, it gets numerous link errors for undefined symbols, all of which are located in that one sub-library.&amp;nbsp; I thought that when building a library that references another library, that referenced library gets pulled into the library being built.&amp;nbsp; Is that not the case with CodeWarrior 10?&amp;nbsp; Is there a way to get CodeWarrior 10 to include referenced libraries in the final output when building a library project?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Oct 2012 19:42:26 GMT</pubDate>
    <dc:creator>jimfell</dc:creator>
    <dc:date>2012-10-25T19:42:26Z</dc:date>
    <item>
      <title>Library Inclusion in CW 10 Application Project</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Library-Inclusion-in-CW-10-Application-Project/m-p/152653#M3745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a CodeWarrior 10 application project that references multiple compiled libraries.&amp;nbsp; One of these libraries references yet another library.&amp;nbsp; All of the library projects build without any problems.&amp;nbsp; However, when I try to build my application project, it gets numerous link errors for undefined symbols, all of which are located in that one sub-library.&amp;nbsp; I thought that when building a library that references another library, that referenced library gets pulled into the library being built.&amp;nbsp; Is that not the case with CodeWarrior 10?&amp;nbsp; Is there a way to get CodeWarrior 10 to include referenced libraries in the final output when building a library project?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Oct 2012 19:42:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Library-Inclusion-in-CW-10-Application-Project/m-p/152653#M3745</guid>
      <dc:creator>jimfell</dc:creator>
      <dc:date>2012-10-25T19:42:26Z</dc:date>
    </item>
    <item>
      <title>Re: Library Inclusion in CW 10 Application Project</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Library-Inclusion-in-CW-10-Application-Project/m-p/152654#M3746</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Which MCU are you targeting&amp;nbsp; (HCS08, Coldfire, Kinetis, ...)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Oct 2012 07:42:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Library-Inclusion-in-CW-10-Application-Project/m-p/152654#M3746</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2012-10-26T07:42:11Z</dc:date>
    </item>
    <item>
      <title>Re: Library Inclusion in CW 10 Application Project</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Library-Inclusion-in-CW-10-Application-Project/m-p/152655#M3747</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi CrasyCat.&amp;nbsp; We're using ColdFire V1.&amp;nbsp; However, I think that I've been able to resolve this particular issue.&amp;nbsp; The sub-library was missing a source file, which had the function definitions in question, when it was built.&amp;nbsp; It didn't complain when being built as a library because the function prototypes in the header file were declared as external.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Oct 2012 13:07:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Library-Inclusion-in-CW-10-Application-Project/m-p/152655#M3747</guid>
      <dc:creator>jimfell</dc:creator>
      <dc:date>2012-10-26T13:07:54Z</dc:date>
    </item>
  </channel>
</rss>